Here’s the page we think you wanted. See search results instead:

 

Sprechen Sie mit einem Experten

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 39

Sort:
Can I use a normal USB cable for datalogging with the U1250A Series Handheld Digital Multimeters?
No, you cannot use a normal USB cable for datalogging with the U1250A Series Handheld Digital Multimeters…..

FAQ 2013-11-17

Are there any calibration options available for the U1251A/U1252A Handheld Digital Multimeter?
Yes, there are a variety of calibration options available for the U1251A and U1252A Handheld Digital Multimeter…

FAQ 2013-11-17

Can HyperTerminal be used with the U1251A/U1252A Handheld Digital Multimeter?
No, HyperTerminal cannot be used with the U1251A and U1252A Digital Multimeter….

FAQ 2013-11-17

Can I use the test probe leads marked with CAT III 1000V rating come together with the U1241A/U1242A/U1251A/U1252A/U1253A handheld Multimeter…
The test lead kit which currently marked with CAT III 1000V rating can be used with the multimeter at CAT IV 600V measurement environment...

FAQ 2013-11-17

Can I measure temperature with the U1251A/U1252A Handheld Digital Multimeter?
Yes, you can measure temperature with the U1251A and U1252A Handheld Digital Multimeter…

FAQ 2013-11-17

Can I measure duty cycle or pulse width with the U1251A/U1252A Handheld Digital Multimeter?
Yes, you can measure duty cycle or pulse width with the U1251A and U1252A Handheld Digital Multimeter.

FAQ 2013-11-17

Can I change the amplitude level for the squarewave output function?
No, you cannot change the amplitude level …

FAQ 2013-11-17

Do the U1251A and U1252A Digital Multimeters come with connectivity cables?
No, the U1251A and U1252A Digital Multimeters do not come with connectivity cables. The cable is an optional accessory…..

FAQ 2013-11-17

Can I export the interval logging data saved in the internal memory of my U1253A Handheld Multimeter?
Yes, you can export the interval logging data saved by upgrade your U1253A Firmware revision to V1.20…..

FAQ 2013-11-17

What are the conditions that will cause the U1270 series handheld multimeter to display Incorrect DC Voltage values at DC measurement mode when signal
The error value may occur if the Filter is not enabled...

FAQ 2013-11-10

Can event (trigger) logged data be transferred to the GUI DATA LOGGER?
No, data can only be transferred for manual logged data and interval logged data.

FAQ 2011-05-05

Does Keysight U1271A/U1272A Handheld Digital Multimeter comes with a power adapter?
No, U1271A/U1272A is powered by four 1.5V AAA alkaline batteries.

FAQ 2011-05-05

Under the unit function’s ACV and DCV, the display rate of U1271/2A indicates 7 times per second, can GUI DATA LOGGER capture all 7 readings?
No, the GUI DATA LOGGER is running on different acquisition method than the unit’s display rate, therefore the fastest update rate is 1 sample per second.

FAQ 2011-05-05

Why am I getting a reading instead of zero when using U1252A/U1253A frequency counter measurement function although no measurement was done…
After the probes are connected to the U1252A/U1253A, the measured value will be automatically zeroed.

FAQ 2010-08-09

Can I measure coil resistance with the U1241B/U1242B Handheld Digital Multimeter (DMM)?
Yes, you can measure coil resistance with the U1241B/U1242B Handheld Digital Multimeter (DMM)

FAQ 2010-08-08

Can I measure AC voltage with the U1241B/U1242B Handheld Digital Multimeter (DMM) if there is a DC offset?
Yes, you can measure AC voltage with the U1241B/U1242B Handheld Digital Multimeter (DMM), even if there is a DC offset

FAQ 2010-08-08

Can I control the beeper sound volume for the audible continuity measurement?
No, you can't….

FAQ 2010-07-18

What is the different between Frequency Function and Frequency Counter Function at U1252B/U1253B Series handheld Digital Multimeter?
The Frequency function measures up to 600kHz 1000V … Frequency Counter function measures upto 20 MHz at <30Vpp…

FAQ 2010-05-10

Can I perform measurement with my U1252A/U1253A Handheld Multimeter while charging the unit?
No, U1252A/U1253A Handheld Multimeter does not allow to perform measurement while charging…

FAQ 2010-05-05

How to check the condition of the fuses in U1253A/U1253B before you use it?
To test the fuses inside the U1253A/U1253B OLED display DMM, just follow the instructions as follows…

FAQ 2010-03-22

Can I program to control U1401B?
No...

FAQ 2010-03-22

What should I consider when charging my U1252B/U1253B Handheld Digital Multimeter with the DC power adaptor?
Please ensure the following precautions is observed during the charging process ...

FAQ 2010-02-23

Can I use a normal USB cable for datalogging with the U1250B Series Handheld Digital Multimeters?
No, you cannot use a normal USB cable for datalogging with the U1250B Series Handheld Digital Multimeters…..

FAQ 2010-02-21

How long can the batteries of the U1241B or U1242B Handheld Digital Multimeter last?
The batteries that are supplied with the U1241B or U1242B Handheld Digital Multimeter can last for more than 200 hours under normal use.

FAQ 2010-02-21

Why is the battery life of the U1253B Handheld Digital Multimeter (DMM) typically shorter than the battery life of the U1251B/U1252B?
The battery life of the U1253B Handheld Digital Multimeter (DMM) is typically shorter because its display brightness is set to the highest….

FAQ 2010-02-21

1 2 Next