Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discutez avec un expert

Support technique

Mesure Electronique

Support by Product Model Number:

Affiner la liste

retirer tout le raffinement

Par industrie/technologie

Par type de contenu

Par catégorie de produit

Par autre catégorie

251-275 sur 977

Tri:
Keysight Technologies Begins Operations
Keysight Technologies, Inc. announces the electronic measurement business of Agilent Technologies has begun operating under the Keysight name.

Dossier de presse 2014-08-01

No-Cost, Six-Month Availability of Modelithics COMPLETE Library for Genesys 2014
Extensive Model Library Enables Exceptional Accuracy with Genesys RF Simulation Software.

Dossier de presse 2014-07-28

Industry's most accurate test solution for USB 3.1 receivers – press release
Using the USB 3.1 receiver test set, design and test engineers in the semiconductor and computer industry can now accurately characterize and verify USB 3.1 receiver ports in ASICs and chipsets.

Dossier de presse 2014-07-09

Introduces Industry's Most Accurate Test Solution for USB 3.1 Receivers
Achieve accurate receiver characterization with the J-BERT high-performance BERT

Dossier de presse 2014-07-09

ADS DDR4 Compliance Test Bench for Solving the Simulation-Measurement Correlation Challenge
The solution is ideal for semiconductor companies developing DDR controller IP; those developing DRAM chips and DIMMs; and OEMs integrating the controller and DIMM into a system using PCB technology.

Dossier de presse 2014-06-30

New ADS DDR4 Compliance Test Bench for Solving the Simulation-Measurement Correlation Challenge
Agilent introduces Advanced Design System DDR4 Compliance Test Bench, which enables a complete workflow for DDR4 engineers from simulation of a candidate design through measurement of the finished prototype. The solution is ideal for semiconductor companies developing DDR controller IP; those developing DRAM chips and DIMMs; and OEMs integrating the controller and DIMM into a system using PCB technology.

Dossier de presse 2014-06-30

Agilent Technologies Introduces Family of Basic AC Power Sources for Reliable Testing
A new family of basic AC power sources that deliver reliable power for design and manufacturing. The new Agilent AC6800 Series includes four models from 500 VA to 4000 VA output power, all with the quality and capability required for basic testing.

Dossier de presse 2014-06-24

Advanced Modeling Solutions for Nanoscale 3D FinFETs and High-Frequency/High-Power GaN HEMTs
Agilent announces several innovations for the 2014 release of its industry-leading suite of device modeling and characterization software tools. The suite is comprised of IC-CAP, MBP, and MQA.

Dossier de presse 2014-06-18

Agilent Technologies Introduces Advanced Open FPGA Design Flow and Real-Time Measurement Solution
EEsof EDA W1462 SystemVue FPGA Architect now supports on-board FPGA design and simulation with the Agilent M9703A AXIe wideband digital receiver/digitizer. The new modeling and simulation capability reduces development time for research and design validation teams working on early system prototyping and development of advanced multichannel applications.

Dossier de presse 2014-06-17

Agilent Technologies Introduces Advanced Open FPGA Design Flow and Real-Time Measurement Solution
Agilent announces that the Agilent EEsof EDA W1462 SystemVue FPGA Architect now supports on-board FPGA design and simulation with the Agilent M9703A AXIe wideband digital receiver/digitizer.

Dossier de presse 2014-06-17

Agilent Technologies Announces Portfolio of DOCSIS 3.1 Test Solutions
Agilent announces a portfolio of Data Over Cable Service Interface Specification (DOCSIS) hardware and software test solutions for generating and analyzing signals up to a bandwidth of 192 MHz. The test solutions are used by R&D engineers to test transmitters, receivers and components against the requirements set forth in the DOCSIS 3.1 specification.

Dossier de presse 2014-06-12

Agilent Technologies and Cascade Microtech Announce Alliance to Streamline Wafer-Level Measurements
Agilent Technologies and Cascade Microtech announce a strategic alliance to provide fully configured and validated RF measurement solutions that streamline wafer-level semiconductor measurements while delivering guaranteed configuration, installation and support.

Dossier de presse 2014-06-03

TowerJazz Releases Enhanced RF SOI CMOS and High Speed SiGe PDKs for use with ADS
TowerJazz, the global specialty foundry leader, announces the availability of enhanced RF SOI CMOS and high speed SiGe process design kits (PDKs) for its 0.18µm process technology. These kits were developed for use with Advanced Design System (ADS) software.

Dossier de presse 2014-06-03

Agilent Technologies Introduces Advanced 4G Design and Validation Support
Agilent announces that the Agilent EEsof EDA W1918 LTE-Advanced baseband verification library has added support for key 4G technologies, such as Adaptive Modulation and Coding (AMC) and Coordinated Multi-Point (CoMP).

Dossier de presse 2014-06-02

Certification of HDMI 2.0 6G Test Solution for HDMI 2.0 Compliance Test - press release
2.0 6G test solution provides the widest coverage for HDMI physical layer compliance test. Certification was achieved using the collaborative framework of Simplay Labs Authorized Test Centers, the world's leading HD testing service provider, with locations in Sunnyvale, California; Beijing, Shanghai and Shenzhen, China; and Seoul, Korea.

Dossier de presse 2014-05-30

Genesys 2014 Delivers Breakthrough Modulated RF Analysis for Circuit, System Design
Keysight announces the latest release of Genesys 2014.

Dossier de presse 2014-05-27

New Modeling, Verification Platform for Radar, Electronic Warfare
Moving Scenarios, Beamforming Accelerate Radar System Design and Validation.

Dossier de presse 2014-05-21

Agilent Technologies to Attend IMS with Leading-Edge RF/Microwave Design and Measurement Solutions
Agilent announces it will attend the IEEE MTT-S International Microwave Symposium 2014 (Booth 1133), June 1-6, in Tampa, Fla. The company will demonstrate over 20 of its newest design and measurement solutions.

Dossier de presse 2014-05-21

Agilent Technologies Announces 4x4 True MIMO Evolution on EXM Wireless Test Set

Dossier de presse 2014-05-21

Automatic Fixture Removal Option Enables Industry's Fastest, Easiest Non-Coaxial Device Measurement

Dossier de presse 2014-05-20

Agilent Technologies Introduces Modeling, Verification Platform for Radar, Electronic Warfare
Agilent announces that the W1905 radar model library has been enhanced to simulate moving 3-D radar scenarios as well as phased-array adaptive beamforming.

Dossier de presse 2014-05-19

Advanced Design System Selected by GIT Japan for Front-to-Back MMIC and Silicon RFIC Implementation
GIT Japan Inc., a provider of advanced interface technologies between people and information, and a competence center for ultrawideband (UWB) chipset and module development, has selected the ADS platform for complete GaAs/GaN- and silicon-based RFIC/MMIC implementations.

Dossier de presse 2014-05-08

Agilent's UXM Wireless Test Set Accelerates Marvell's LTE-Advanced Category 7 Chipset Development
Agilent and Marvell worked in concert to achieve sustained bidirectional 300 Mbps downlink/100 Mbps uplink data throughput using 3GPP release 10 downlink and uplink carrier aggregation.

Dossier de presse 2014-05-06

Agilent Technologies Acquires Electrothermal Analysis Technology from Gradient Design Automation
Agilent announces its acquisition of electrothermal analysis technology from Gradient Design Automation, the maker of HeatWave electrothermal analysis software.

Dossier de presse 2014-04-30

Certification of HDMI 2.0 Test Solution
Certification of HDMI 2.0 Test Solution for HDMI 2.0 Compliance Test, With Widest Coverage of Test Items

Dossier de presse 2014-04-17

Précédente ... 11 12 13 14 15 16 17 18 19 20 ... Page suivante