Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 724

Sort:
Can the B01 bundle for the M9703B digitizer support 1 GHz of bandwidth?
No, the AXIe carrier board in the B01 bundle contains different assemblies than the standard M9703B board. Click on the link for additional information.

FAQ 2017-08-01

What is the time out limit of response time (2.4) in M8020A Interactive link training?
The LTSSM (Link Training and Status State Machine) implements the timeouts as specified in the PCIe specification. Click on the question for additional information.

FAQ 2017-06-28

If we use external clocks for both the Pattern Generator and Error Detector parts, can we run them at different data rates?
It would be more straight-forward to provide the PG (TX) with a 10 GHz clock (for 10 Gb/s data) and then use the 1:4 demux and provide the ED (RX) with a 2.5 GHz clock (measuring 2.5 Gb/s data). Click on the question for additional information.

FAQ 2017-06-28

Is there a PDF version available of the user guide for the M9210A? There are issues with the .chm file that is available.
No, there is not a PDF version available for the M9210A user manual. To read the .chm file, it must be downloaded and copied on the local C drive before opening.

FAQ 2017-06-28

Does the Maury Microwave MT7553B03 50 GHz Noise Receiver Module lower the effective noise figure of the N5245A beyond that of option 029?
Yes, the NF of the 50 GHz PNA-X is about 10 dB for most of its range while the typical NF from the MT7553B03 is 6 dB.

FAQ 2017-06-28

What is the raw jitter tolerance for the N4960A/N4952A?
There is no CDR in the N4960A, so by itself, the JTOL plot will be a flat line somewhere below 1 UI. An external CDR can be used. Click on the question for additional information.

FAQ 2017-06-28

How do I create a Mono FM Signal using N5182B MXG ARB?
You can configure N7611B Signal Studio Broadcast Radio to play a mono/FM signal.

FAQ 2017-06-28

I am using an electronic load to draw current into my DUT, but when I draw current the voltage drops. Why is this happening?
A voltage drop will appear across this impedance as current flows through it in accordance with Ohm’s Law. Click on the question for additional information.

FAQ 2017-06-28

Does the noise figure application on the PNA-X (option 029) provide a full noise-parameter system (tuners and software)?
No, we don’t provide a full noise-parameter system. Click on the question for additional information.

FAQ 2017-06-28

For my UXA Signal Analyzer, what applications support option H1G (1 GHz Analysis Bandwidth) and what additional functionality does it provide?
Option H1G also includes the B2X digitizer. Therefore, option H1G is supported by all applications that support B2X up to at least 255 MHz bandwidth. Option H1G additionally provides 1 GHz analysis bandwidth for some other measurement applications.

FAQ 2017-06-28

Is option RTS necessary for streaming with bandwidths greater than 40 MHz?
Option RTS is necessary for streaming bandwidths greater than 40 MHz. Either real-time option, RT1 or RT2, is required. Even though these options are license key enabled, they require the analyzer to have B85, B1X, B2X, or B5X.

FAQ 2017-06-28

How many carriers can the MXG support in Carrier Aggregation mode?
One MXG can support one instance of the Carrier Aggregation mode. One instance of the Carrier Aggregation mode supports 5 component carriers.

FAQ 2017-06-28

Is Option RTS a license key or hardware upgrade?
Option RTS is a hardware and license key upgrade. Therefore, this upgrade requires the analyzer to be returned to Keysight.

FAQ 2017-06-28

Why is Option DP2 or B40 recommended on the spectrum analyzer (EXA, MXA, PXA) with the EMI Measurement Application(N6141A)?
Time Domain Scan (TDS), Monitor Spectrum, and Amplitude Probability Distribution (APD) all require 2 GB of Capture memory (option DP2). Option B40 includes DP2, so having either option B40 or DP2 will work equally as well for N6141A.

FAQ 2017-06-28

Is it possible to develop specific macros for E5061B to support TRL cal or the unknown thru method under a 9-term calibration method?
Yes, it is possible to perform a user developed 8-term calibration, like TRL, using an external program for the E5061B. Click on the question for additional information.

FAQ 2017-06-28

Can a CalPod system be used with the N1500A software?
No, the CalPod and N1500A Software are not compatible.

FAQ 2017-06-28

Does M9393A work without M9300? If so, when using the M9393A with 100MHz reference on a pulse generator, what is the external reference input voltage?
When replacing the M9300 with a pulse generator, self-test and alignments may pass. Click on the question for additional information.

FAQ 2017-06-28

What is the difference of software options between M9485A and PNA/ENA series VNA?
There is no difference for option 007/009/010. There are some differences for options 025, 028, 086 and 551.

FAQ 2017-05-25

Which power meter is recommended for system power calibration?
U2000 Series USB Average Power Sensors or U8480 Series USB Thermocouple Power Sensors are recommended.

FAQ 2017-05-25

Can I use multiple M9485A with one controller?
Yes, but there are some limitations. Please refer to below.

FAQ 2017-05-25

FieldFox Manuals, Firmware, Software and Product Support
Manuals, firmware upgrade, software trials & upgrade and support page for FieldFox analyzers

FAQ 2017-02-02

Is There a GPS Receiver for FieldFox?
GPS capability has been added to FieldFox starting from firmware revision A.05.33.

FAQ 2017-01-23

Can the U4431A MIPI M-PHY protocol analyzer be controlled from an external PC via the AXIe mainframe's USB port?
Yes, the USB connected chassis option (M9502A-U20/M9505A-U20) is a viable connection strategy when using the U4431A M-PHY Protocol Analyzer instrument.

FAQ 2016-07-08

What termination model (Balanced vs. Unbalanced) should I use for my M8000 BERT?
For M8000 (M8041A/51A/61A/62A) BERT data outputs, a Termination Model must be selected in the Amplifier section of the Parameters window, Balanced or Unbalanced.

FAQ 2016-07-08

What is the phase noise sensitivity of the E5052B with E5053A and 11970 Mixers?
Please refer to this document.

FAQ 2016-03-29

1 2 3 4 5 6 7 8 9 10 ... Next