이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

데이터 수집 - DAQ

모델 번호 입력:

1-25 / 32

정렬방식:
Can I do voltage measurement using the U2802A rather than temperature measurement?
Yes, you can do voltage measurement easily by using the Keysight Measurement Manager (AMM)...

FAQ 2013-11-17

How can I input 28V digital signal to U2651A/U2652A when it support digital input voltage < 24V?
You can connect a voltage divider in front of the digital input to reduce the voltage to <24V

FAQ 2010-10-07

NI LabVIEW가 내 82357A USB/GPIB 인터페이스와 통신할 수 있도록 하려면 어떻게 해야 합니까?
IO Libraries Suite를 설치하고 82357A를 구성하십시오. NI-VISA를 설치할 경우에는 구성 단계가 다를 수도 있습니다.

FAQ 2010-08-27

If I set Channel 1 of U2300A/U2500A with voltage range of 5V, I get a reading of 4.99968 when nothing is connected to the DAQ.
If you don't have anything connected to the DAQ and you do an acquisition out of it, the result…

FAQ 2010-08-09

Why do we see unused port in U2300A/U2500A with similar waveform and frequency but with lower amplitude to its adjacent or close by used port?
It is recommended to ground all the AI connection that is not being used. If you have multiples of AI channels to be used, one good way is to have…

FAQ 2010-08-09

What is the clock rate for Digital Inputs(DI) and Digital Outputs(DO) of U23xxA and U25xxA USB Data Acquisition?
The DAQ DIO is not meant to measure DI with clock rate precision or to control frequency of digital output

FAQ 2010-07-18

34970A: RTD 온도 측정시 어떤 온도 계수(Temperature Coefficient)를 지원 합니까?
.

FAQ 2010-05-16

Is there any special setting that I need to do in Keysight VEE before using the U2300A or U2500A DAQ with it?
Yes. In fact it is the most important thing you need to set before using the DAQ with Keysight VEE. As most instruments uses MSB byte ordering, DAQ...

FAQ 2009-12-15

Can strain gauges be measured with the Keysight 34970A?
The 34970A can measure strain gauges using 4-wire ohms measurements and return the strain value using the math formula Mx+B.

FAQ 2009-11-18

What is the main difference between the digital output (DO) of the U2100A, U2600A, U2300A and U2500A?
The DO port of U2100A and U2600A requires external power supply to be pumped into the port...

FAQ 2009-10-20

34970A: 어떻게 구성해야 34901A와 34902A에서 공통접지일 때의 전압 값을 읽어올 수 있을까요?
.

FAQ 2009-10-04

How do I know what is the best sampling rate to use for my measurement?
Typically if you follow Nyquist theory, your sampling rate should be 2x the highest frequency of the incoming signal that you are measuring. However, we recommend that you use 5x...

FAQ 2009-09-29

RTD는 종종 3개의 리드와 함께 제공되는 이유는 무엇이며 어떻게 측정합니까?
이 구성을 통해 사용자는 리드 저항에 맞게 보정할 수 있습니다.

FAQ 2009-09-28

Why do I receive an error message below ?
Generally, if you are sampling at 60kSa/s and above, you should use high sampling mode to acquire data. This is just a rough guideline. If you encountered this message even when....

FAQ 2009-08-06

How can I remotely connect to all my USB DAQ devices, Digital IOs, and card cage?
Please make sure that your remote PC (which is connected to all your USB instruments) is connected to the same network as yourself. However, your remote PC cannot be connected...

FAQ 2009-08-06

Can both Analog Input and Analog Output function at the same time?
Yes, both Analog Input and Analog Output can function at the same time. However,….

FAQ 2009-02-04

34970A를 사용하여 열전쌍 측정을 수행할 때 100V 이상의 동상 모드 전압을 제거할 수 있습니까?
예, 300V 피크 이하의 경우 내부 DMM의 적분 시간을 파워 라인 사이클의 값 1 이상으로 설정하여 제거할 수 있습니다.

FAQ 2007-01-10

34901A 카드 및 T타입 열전쌍을 사용하여 스위치 온도를 측정했습니다. 이 스위치에서 몇 볼트(V)의 AC 전압 및 60Hz가 표시됩니다. 온도 결과는 완전히 틀리며 빠르고 크게 변합니다. AC 전압이 약 50Hz 또는 다른 주파수인 경우 온도가 정확합니다. ...
AC 신호로 열전쌍 측정을 수행할 경우 판독값에서 노이즈를 예상해야 합니다. 공통 모드 노이즈 제거를 적용하여 이 노이즈를 줄일 수 있습니다.

FAQ 2007-01-09

34970A: What is Burden Voltage?
Connecting the internal DMM in series with a test circuit to measure a current, a measurement error is introduced.

FAQ 2006-08-29

Can I configure the 34970A for 4-wire resistance, 4-ohms, and/or 4-wire scan?
Yes, the 34970A can be configured for 4 wire resistance, 4 wire RTD or 4 wire external scanning.

FAQ 2006-08-29

How do I make a measurement from the front panel with the Keysight 34970A?
This FAQ describes how to setup for a measurement from the front panel using the thermocouple shipped with the 34970A and a 34901A/34902A/34908A module card.

FAQ 2006-02-02

34901A, 34902A , 34908A 모듈에서 전압 측정시 플로팅 상태로 측정할 수 있습니까?

FAQ 2005-09-20

키사이트 34970A로 열전쌍 측정을 수행할 때 어떤 온도 참조 접점을 선택할 수 있습니까?
내부, 외부 및 고정 참조를 사용할 수 있습니다.

FAQ 2005-05-26

34970A: How can I improve the stability of flowmeter measurements?
Stability improvements can be made by eliminating unwanted noise.

FAQ 2004-03-29

34970A: How can the measurement speed be maximized?
Several setups can be made to the 34970A to increase your measurement speed.

FAQ 2003-12-11

1 2 다음