Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 218

Sort:
For my UXA Signal Analyzer, what applications support option H1G (1 GHz Analysis Bandwidth) and what additional functionality does it provide?
Option H1G also includes the B2X digitizer. Therefore, option H1G is supported by all applications that support B2X up to at least 255 MHz bandwidth. Option H1G additionally provides 1 GHz analysis bandwidth for some other measurement applications.

FAQ 2017-06-28

Why is Option DP2 or B40 recommended on the spectrum analyzer (EXA, MXA, PXA) with the EMI Measurement Application(N6141A)?
Time Domain Scan (TDS), Monitor Spectrum, and Amplitude Probability Distribution (APD) all require 2 GB of Capture memory (option DP2). Option B40 includes DP2, so having either option B40 or DP2 will work equally as well for N6141A.

FAQ 2017-06-28

When using the DIQ application, what happens when I set the internal receiver to measure beyond the frequency range of my instrument?
Data for frequencies beyond the instrument hardware limitations is extrapolated from the hardware’s maximum and minimum limits. Click on the question for additional information.

FAQ 2017-06-28

What is the difference between the Integrated true-mode stimulus application (opt 460) and the Differential and I/Q devices application (opt 089)?
The Integrated TMSA and the DIQ both simplify measurements of differential (balanced) devices. The two applications however, are used for different measurements. Click on the question for additional information.

FAQ 2017-06-28

FieldFox Manuals, Firmware, Software and Product Support
Manuals, firmware upgrade, software trials & upgrade and support page for FieldFox analyzers

FAQ 2017-02-02

What termination model (Balanced vs. Unbalanced) should I use for my M8000 BERT?
For M8000 (M8041A/51A/61A/62A) BERT data outputs, a Termination Model must be selected in the Amplifier section of the Parameters window, Balanced or Unbalanced.

FAQ 2016-07-08

Can I use the Fixture Simulator functions with the 2-port ENA?
Yes, but the function is limited...

FAQ 2015-01-09

Is there a summary of available cable test methods when using the FieldFox Hand Held portable analyzers?
Yes. Please refer to the FieldFox Hand Held Cable Test details and methods below.

FAQ 2014-08-11

When automating markers on the ENA is it possible to programmatically query the indicated inductance or capacitance on a Smith Chart?
The inductance / capacitance information cannot be directly queried via the automation interfaces. The inductance (positive reactance, top half of the Smith Chart) or capacitance (negative reactance, lower half of the Smith Chart) is not available as an automation query.

FAQ 2014-08-11

Why does my FieldFox spectrum analyzer preamplifier increase the noise floor when engaged?
The FieldFox spectrum analyzer preamplifier selection will normally reduce the displayed noise floor when activated. However, if the FieldFox RF attenuation AUTO selection is set to ON then the preamp may not reduce the noise floor.

FAQ 2014-03-03

What is 802.11af, and does Keysight have a solution for testing 802.11af devices?
Learn more about Keysight's 802.11af solutions…

FAQ 2014-02-28

Can I do voltage measurement using the U2802A rather than temperature measurement?
Yes, you can do voltage measurement easily by using the Keysight Measurement Manager (AMM)...

FAQ 2013-11-17

Can I measure temperature with the U1251A/U1252A Handheld Digital Multimeter?
Yes, you can measure temperature with the U1251A and U1252A Handheld Digital Multimeter…

FAQ 2013-11-17

Can I set a measurement interval on the U1251A and U1252A Handheld Digital Multimeters?
Yes, you can set a measurement interval on the U1251A and U1252A Handheld Digital Multimeters….

FAQ 2013-11-17

I am looking at a 160 MHz OFDM signal at 5 GHz on my MXA or PXA signal analyzer. Why can’t I see the whole signal?
The instrument preselector is limiting the bandwidth of the MXA or PXA input.

FAQ 2013-08-07

On the PNA Vector Network Analyzer Family Is it possible to save a Touchstone (SnP) file with unwrapped phase?
Yes. The PNA Family of Vector Network Analyzers can save Touchstone (SnP) files with the phase information as unwrapped phase. To achieve unwrapped phase in a Touchstone file save perform the following...

FAQ 2013-07-29

Where can I find information or example programs using the API for Signal Studio?
The Signal Studio for pulse building help file has information and example programs under the API control chapter.

FAQ 2013-05-16

Does the ENA 6 series have the swept sweep mode in the frequency sweep?
No. The E5061A/62A and E5061B have only stepped sweep mode in the frequency sweep.

FAQ 2013-04-25

Uncertainty Calculators. What is the Accuracy of My Measurements?
Whether you are a novice or experienced user of Keysight test equipment, you may sometimes need more details to answer the question “How accurate are these measurements?” Learn more important details and download the following uncertainty calculators.

FAQ 2013-02-28

Vector Network Analyzer Uncertainty Calculator, What is the Accuracy of My Measurements?
No matter whether you are an experienced or novice user of vector automatic network analyzers, you may have asked "How accurate are these measurements?"

FAQ 2013-01-13

Are there any step-by-step measurement examples for ENA 7 series?
Yes. There are some measurement examples in ENA help file...

FAQ 2012-12-28

What is the best configuration for wideband I/Q modulation?
An E8267D Option 016 or an N8212A Option 016 signal generator with an M8190A arbitrary waveform generator

FAQ 2012-12-28

How many measurements do I need to make and how long is the predistortion data good?
The number of measurements needed depends on the number of parameters that are changed. The calibration (measurement data) could be valid for two days or longer.

FAQ 2012-12-28

How much time/frequency error is introduced by the Custom Profile or Custom I/Q resampling?
After using the formula to calculate the number of resampled data points, work backwards to determine the error.

FAQ 2012-12-28

Why can’t I view a help file downloaded from the Keysight website?
After downloading the file to your PC, open it from the location it was saved and a security warning appears. To view the help system, clear the checkmark from the "Always ask before opening this file" check box.

FAQ 2012-12-28

1 2 3 4 5 6 7 8 9 Next