이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-11 / 11

정렬방식:
무료 체험판은 어디에서 확인할 수 있습니까?
제품군별로 가용한 무료 체험판을 확인하십시오.

FAQ 2014-08-14

Why do I need to pay installation/calibration charges for N4010A license-only upgrades?
The N4010A has several license-only upgrade paths, most of which enhance the base technology options that are already enabled in the unit. Click on the question above for a fuller description.

FAQ 2013-02-06

I lost my E5500 Phase Noise System license key. How do I obtain a permanent replacement license key?
In order to obtain a permanent replacement phase noise system license key the phase detector test set (70420A or N5500A) serial number is required.

FAQ 2012-12-20

34970A와 34980A의 DL Pro license는 별도입니까?
별개입니다.

FAQ 2010-10-21

GMA N4017A 소프트웨어 라이센스는 어떻게 설치하는가?
http:///find/softwarelicense에서 N4017A 권한 인증을 회복하려면 소프트웨어를 N4010A 테스트 세트로 제한할 것인지 PC로 제한할 것인지 결정해야 합니다.

FAQ 2010-09-27

Can I mix 34980As and 34970As in the same configuration?
You can have a combination of one 34980A and one or two 34970As in a configuration.

FAQ 2010-05-05

N5532A 센서 모듈의 주파수 범위는 어떻게 됩니까?
100kHz~4.2GHz, 10MHz~18GHz, 30MHz~26.5GHz 및 30MHz~50GHz.

FAQ 2010-04-13

Fault Detective: Why does my annual license file expire on a date that is not one year from the day I redeemed my license file?
The expiration date for an annual license file is one year plus two weeks from the date of the order.

FAQ 2010-02-25

Fault Detective: Why does my perpetual license file expire on January 31st?
A perpetual license requires a yearly renewal of the license file, at no cost.

FAQ 2010-02-25

How can I update the MWA software on my ENA to the latest revision?
The latest revision of the MWA can be downloaded from Keysight web page.

FAQ 2009-07-15

How can I identify if the MWA software is installed on my ENA?
The registered key code of the MWA is stored in the ENA directory.

FAQ 2009-07-15