By Topic

By Type of Content

By Product Category

1-7 of 7

Sort:
What is the accuracy of ENA time domain measurements?
The TDR/TDT measurement uncertainty is provided in the following table.

FAQ 2014-02-01

Is 4-port calibration using the 2-port ECal module supported on ENA Option TDR?
No.

FAQ 2012-02-02

When I perform both the calibration with frequency offset off and the scalar-mixer calibration with frequency offset on, which one is valid?
If the frequency offset function is turned on, the scalar mixer calibration data is used.

FAQ 2011-10-17

Can the ENA perform Vector Mixer Calibration (VMC) with Fixed RF or Fixed IF measurement?
No. It is not possible to perform Fixed RF measurements (RF: Fixed, LO and IF: Swept) with VMC.

FAQ 2011-10-17

Can I measure a dual conversion mixer on the ENA?
If the LO frequencies are fixed, dual conversion mixers can be measured with option 008 (Frequency-Offset Mode).

FAQ 2011-10-17

Is it possible to make a vector measurement of a balanced-mixer using ENA?
Yes.

FAQ 2009-06-08

With the Vector Mixer Calibration (VMC) technique, is it possible to characterize mixers below the lowest operating frequency of the ENA?
Yes.

FAQ 2009-02-23