Here’s the page we think you wanted. See search results instead:

 

Parla con un Esperto

Technical Support

Electronic Measurement

Support by Product Model Number:

1-4 of 4

Sort:
How can I read the calibration date for an E363xA or an E364xA power supply?
The calibration message containing the factory calibration date can be retrieved by using the "CALibration:STRing" command. After the calibration is completed, the date can be changed with the " CALibration:STRing " command.

FAQ 2010-09-08

How long is the calibration time interval?
Keysight recommends 1 year as the calibration interval for all E3600 series power supplies.

FAQ 2008-09-23

66xxA: Re-Calibration Date
There are no components used in Power Products which have a specific shelf life. Therefore, the calibration period of this instrument begins on the date that the product is first put into service by the customer. The recommended calibration interv...

FAQ 2008-09-22

66xxA: Calibration Certificates
Criteria have been established to determine which products get or do not get a calibration from the factory. A product with a product number does not automatically qualify for a calibration certificate.

FAQ 2008-09-22