이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

상세 분류

상세분류 제거

주제별

분야별 검색결과

제품 카테고리별

1-25 / 75

정렬방식:
What is the performance test procedure of 4349A?
See the documentation.

FAQ 2014-09-03

PDF PDF 3.71 MB
교정 키트 토크 렌치를 위한 인증(및 재인증) 프로세스는 무엇입니까?

FAQ 2014-03-24

Are rules execution sequences arrange able? If yes, how to do it?
Yes, expand the Device Navigation tree of the particular device types, select one of the rule, click "Up" or "Down" key to move the rule to your desired location. For example: Moving "Agilent_fi" rule to before "Agilent_Swap_S&I" of the resistor devices.

FAQ 2013-10-16

Replacement of Control XTP, Module Control Card
Frequently Asked Questions about XTPA Module Control Card

FAQ 2013-06-11

Sample “testplan” for Utility card & FR3070A
Sample “testplan” for Utility card & FR3070A from manufacturing site

FAQ 2013-02-18

What you need to know about Advanced DGN Reporting?
Frequently Asked Questions about Advanced DGN Reporting.

FAQ 2012-11-28

How to debug the 3 differences that are encountered on the new hybrid pin cards (P/N: E4000-66562 and E4000-66563)?
Follow the guideline to debug your test when you start using the new bybrid pin cards: • E4000-66562 for 6MPs (standard hybrid pin card) • E4000-66563 for 12MPs (advanced hybrid pin card)

FAQ 2012-11-12

Why must my N4010A instrument firmware be A.05.06.02 (or newer)?
This is the minimum firmware revision for a hardware change that was introduced during October 2012

FAQ 2012-10-30

Sample DLL for i3070 External DLL Feature
External DLL (dynamic- link library) call feature expands i3070 platform capability for additional functional test / application in a flexible way. Here is a DLL example of data management, updating the test status to a database.

FAQ 2012-10-18

XVision fails to install on some laptops
Before installing XVision /ICT software, please follow the steps below:

FAQ 2012-09-25

3.5mm 암 PSC(precision slotless connector)에 사용할 수 있는 커넥터 수리 키트가 있습니까?
예. 수리 키트의 부품 번호는 85052-60049입니다.

FAQ 2012-05-04

Why must my N4010A instrument firmware be A.05.04.01 (or newer)?
This is the minimum firmware revision for a hardware change that was introduced during December 2011.

FAQ 2012-02-24

How can I turn on the Services for NFS on Windows® 7 ICT controller?
Both the Windows 7 Ultimate and Windows Enterprise Edition contain the client for the Network File System (NFS) and Subsystem for UNIX-based Applications (SUA).

FAQ 2011-11-01

How can I turn on the SUA and its UNIX utility package on Windows® 7 ICT controller?
It is recommended that you DO NOT enable or install SUA. This is an optional feature and utility that is not needed for mapping NFS share.

FAQ 2011-11-01

How can I access my i3070/3070 ICT board directories residing on Linux/UNIX controller, if I am running my ICT controller on Windows® 7?
Services for Network File System (NFS) and Subsystem for UNIX-based Applications (SUA) are the software packages provided by Microsoft® to enable the UNIX subsystem and other parts of the UNIX environment to be integrated onto the Windows environment.

FAQ 2011-11-01

What are the known conflicts between MKS NutCracker and Interix and the recommended workaround solutions?
There are three known key issues which you need to look out for:

FAQ 2011-11-01

How can I set up File Security and board directories with NFS share?
Once you have enabled “Client for NFS”, you can mount any NFS share on your network. There are a few ways to set up NFS share file security.

FAQ 2011-11-01

How to access board directories resided on the Linux/Unix server using SAMBA/Common Internet File System (CIFS), if ICT controller is on Windows® 7?
SAMBA is a utility which allows you to share your files between Linux/UNIX and Windows®. By mounting the SAMBA share on your Linux/UNIX server, you can access the board files across the operating systems.

FAQ 2011-11-01

Why i can't find other languages help file setting in U160X A/B series HH oscilloscope?
In order to access to other language, please go to respective product support page in www.Keysight.com. Go to Driver & Software page, select Firmware Update.

FAQ 2011-09-12

Eight commonly asked questions about the Medalist i3070 Series 5
The i3070 Series 5 sports various innovative hardware and software features to bring you much wider test coverage and superb throughput for cost savings and faster time to profit. Check out these key features.

FAQ 2011-08-08

"RunAllAIC"가 무엇인가요?
unpowered analog 테스트의 결과 입니다.

FAQ 2011-04-26

What is an example of a routine in the testplan for flash programming using the Utility Card?
an example of a routine in the testplan for flash programming using the Utility Card

FAQ 2011-01-04

Why does my E6651A fail Source Modulated Power Level Accuracy in TME?
This may be due to a compatibility issue between the E6651A firmware version and TME.

FAQ 2010-10-14

Why would my N4010A report a "memory lost" error?
This type of error may be reported by the N4010A if it is power-cycled whilst running an internal calibration routine.

FAQ 2010-09-08

What replacement parts and accessories are available for the 113xA-series InfiniiMax probes?
The best place to find this information is in the most recent revision of the InfiniiMax Active Probes User´s Quick Start Guide.

FAQ 2010-06-07

1 2 3 다음