By Topic

By Type of Content

1-25 of 517

Sort:
FieldFox Manuals, Firmware, Software and Product Support
Manuals, firmware upgrade, software trials & upgrade and support page for FieldFox analyzers

FAQ 2017-02-02

In VSA software, how can I export data from the coordinate transformed data that is displayed on the trace?
This can be done by copying/pasting data, or via the API.

FAQ 2016-07-08

In 89601B Digital Demodulation, how can we perform Pi/4 QPSK?
QPSK can be used for Pi/4 QPSK modulation analysis, but the demodulated bits will not be valid.

FAQ 2016-07-08

Can the U4431A MIPI M-PHY protocol analyzer be controlled from an external PC via the AXIe mainframe's USB port?
Yes, the USB connected chassis option (M9502A-U20/M9505A-U20) is a viable connection strategy when using the U4431A M-PHY Protocol Analyzer instrument.

FAQ 2016-07-08

In 89601B for APSK demodulation, how does the LDPC parameter affect measurements?
LPDC adds bit encoding.

FAQ 2016-07-08

Why isn’t the unit being discovered by VSA software hosted inside the instrument itself?
Check to see if Keysight Technologies is returned from the analyzer as part of the *IDN query.

FAQ 2016-07-08

In 89601B, I want to know if the setting is finished. Is there a .NET equivalent of *OPC?
No, there is no equivalent *OPC command since this is typically not required. The command "Measurements.WaitForMeasurementDone" can wait for the end of the measurement.

FAQ 2016-07-08

In 89601B Vector Mode, what is the maximum Main Time length achieved?
Main Time is limited to 524288 samples.

FAQ 2016-07-08

Which PNA / ENA remote interfaces support use of the Keysight cXL code translator?
On the PNA and ENA vector network analyzers, the Keysight cXL code translator is supported and operational only via the GPIB interface.

FAQ 2016-01-27

Does FieldFox support data-based cal kits?
FAQ for FieldFox support of Cal Kits

FAQ 2015-09-09

When automating markers on the ENA is it possible to programmatically query the indicated inductance or capacitance on a Smith Chart?
The inductance / capacitance information cannot be directly queried via the automation interfaces. The inductance (positive reactance, top half of the Smith Chart) or capacitance (negative reactance, lower half of the Smith Chart) is not available as an automation query.

FAQ 2014-08-11

How can I get correct Log Frequency Scale Trace Data Using IntuiLink or BenchVue with my ESA Series Spectrum Analyzer?
Save the trace as a .csv file

FAQ 2014-03-13

How can I save my log plot data to a CSV file type when using the option 226 Phase Noise personality on the PSA or ESA?
In the Phase Noise personality, the log plot data can only be saved as a binary file with the .lpt extension.

FAQ 2014-01-31

On the Keysight NFA Series of Noise Figure Analyzers, is it possible to query the RF attenuator range while in the auto range mode?
The command to query the Keysight NFA RF attenuator while in the auto ranging mode is: DIAG:BLU:RF:RANG?

FAQ 2014-01-31

Is there a sample program for acquiring Noise Figure and Gain Data from the NFA Series of Noise Figure Analyzers?
Yes

FAQ 2014-01-31

Can I save the image of Meter or Logger mode to the internal memory of my U1602A/U1604A Handheld Oscilloscope?
No, you cannot save your Meter or Logger data to the internal memory nor the USB Flash Memory (for option-001) of your U1602A/U1604A....

FAQ 2013-11-17

Can I export the data saved in the U1602A/U1604A Handheld Oscilloscope's internal memory to my PC?
No, you cannot export the data saved in the U1602A/U1604A Handheld Oscilloscope's internal memory to your PC....

FAQ 2013-11-17

Can HyperTerminal be used with the 34405A Digital Multimeter?
No, HyperTerminal cannot be used with the 34405A Digital Multimeter….

FAQ 2013-11-17

Can I use a normal USB cable for datalogging with the U1250A Series Handheld Digital Multimeters?
No, you cannot use a normal USB cable for datalogging with the U1250A Series Handheld Digital Multimeters…..

FAQ 2013-11-17

Does Keysight VEE 9.0 support Windows 7?
Yes. A Keysight VEE patch is currently in development and is tentatively scheduled for release on 2nd quarter of 2010.

FAQ 2013-11-17

Can HyperTerminal be used with the U1251A/U1252A Handheld Digital Multimeter?
No, HyperTerminal cannot be used with the U1251A and U1252A Digital Multimeter….

FAQ 2013-11-17

Which currently available power meters are compatible with the 8753E network analyzer?
In order to work with the 8753E network analyzer, your power meter must emulate either the 436A, 437B, 438A E4418A or the E4419A power meter. Keysight is no longer selling those power meters. However, the E4418B (formerly named the EPM-441A) and E4...

FAQ 2013-11-17

How do I get the N5162A, N5182A, N5172B, N5182B default waveform files from Keysight and download them into the instrument memory?
The arbitrary waveform files are stored in the non-volatile memory of the N5182A/N5162A MXG when they ship out of the factory. In case these waveform files are accidentally deleted, a user can retrieve them through either of the following methods...

FAQ 2013-08-14

How do I use the Service Request method (SRQ) to determine if the X-Series, ESA and PSA Signal Analyzers measurement is complete or has an error me...
Click here for information on the Service Request query to determine when a measurement is complete.

FAQ 2013-06-25

How do I remotely program my spectrum or vector signal analyzer?
Instructions, examples, and references for remotely programming your spectrum analyzer

FAQ 2013-05-16

1 2 3 4 5 6 7 8 9 10 ... Next