이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-25 / 49

정렬방식:
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2017-08-30

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

Where do I find E6651A Mobile WiMAX™ Test Set Software and Firmware
Links to N64xxA and E665xA software and the neccessary firmware.

FAQ 2014-10-28

How do I update the operating system in an N9038A MXE EMI receiver from Windows XP to Windows 7?
PC4 (Dual-Core High Performance Processor) 및 W7X (Window 7 OS) Option을 구매하시면 Window 7으로 upgrade 가능합니다.

FAQ 2014-08-25

What are the Factory Upgrade options for the N8241A and N8242A?
List of options for N8241A and N8242A factory upgrades.

FAQ 2014-05-01

Can I upgrade my 86100A, 86100B or 86100C mainframe to obtain an 86100D?
The 86100D has major hardware differences that make an upgrade uneconomical. Keysight regularly offers trade-in and other incentive programs for DCA mainframes. Contact your local representative for details about the current trade-in program available for your unit.

FAQ 2013-11-27

E8257D 업그레이드 표
E8257D PSG 아날로그 신호 발생기 업그레이드 표

FAQ 2013-08-20

After purchasing an N9094AK upgrade, must the instrument be sent to a Keysight Service Center to be upgraded?
No. The N9094AK upgrades can easily be installed by the user...

FAQ 2013-04-25

How can I get 8960 Lab Application Annual Contract Subscription Release Downloads?
Get the latest downloads here

FAQ 2013-02-28

HTML HTML
Why do I need to pay installation/calibration charges for N4010A license-only upgrades?
The N4010A has several license-only upgrade paths, most of which enhance the base technology options that are already enabled in the unit. Click on the question above for a fuller description.

FAQ 2013-02-06

Why are some of the features shown in the Framescope user manual not available in software version 7.0.5?
Users might encounter different features when using Framescope software version 7.0.5 versus what is stated in the documentation.

FAQ 2012-11-28

Why must my N4010A instrument firmware be A.05.06.02 (or newer)?
This is the minimum firmware revision for a hardware change that was introduced during October 2012

FAQ 2012-10-30

IO Libraries Suite: 고객이 제공한 Suite 14 이상에서 이전 버전을 사용할 수 있습니까?
키사이트 계측기를 한 대 갖고 있는 고객이라면 버전과는 상관 없이 IO Libraries Suite 라이센스 한 개를 사용할 수 있는 법적 권리가 있습니다.

FAQ 2012-10-08

IO Libraries Suite 15 라이센스는 어떻게 구할 수 있나요?
키사이트는 약 150가지 키사이트 계측기 모델, GPIB 및 I/O 컨버터 제품, T&M Toolkit 및 VEE Pro 소프트웨어 개발 복사본과 함께 IO Libraries Suite를 무료로 제공해 드리고 있습니다.

FAQ 2012-10-08

Why must my N4010A instrument firmware be A.05.04.01 (or newer)?
This is the minimum firmware revision for a hardware change that was introduced during December 2011.

FAQ 2012-02-24

이전에 구매한 스코프/로직애널라이저의 소프트웨어 라이선스를 다시 설치할 수 있나요?
주문번호와 certificate 번호가 필요합니다.

FAQ 2011-10-23

Why i can't find other languages help file setting in U160X A/B series HH oscilloscope?
In order to access to other language, please go to respective product support page in www.Keysight.com. Go to Driver & Software page, select Firmware Update.

FAQ 2011-09-12

Why are my N4010A DEVM test results different with firmware revision A.05.03.15?
Revision A.05.03.15 was a short-lived release that used a modified measurement algorithm. Please upgrade to revision A.05.03.16, which uses the correct measurement algorithm.

FAQ 2011-02-18

IO Libraries Suite: What is new with Keysight IO Libraries Suite 14.0?
Keysight IO Libraries Suite provides a new and improved set of tools for establishing, verifying, and troubleshooting instrument-to-PC connections.

FAQ 2010-10-30

Why does my E6651A fail Source Modulated Power Level Accuracy in TME?
This may be due to a compatibility issue between the E6651A firmware version and TME.

FAQ 2010-10-14

IO Libraries Suite: What are the differences between Keysight IO Libraries Suite versions 14.0 and 14.1?
The major enhancement that has been added to version 14.1 is compatibility with National Instruments NI-488.2 API or I/O Library.

FAQ 2010-09-08

IO Libraries Suite: What has changed in version 14.2?
Version 14.2 includes defect fixes and makes two changes to improve the compatibility of Keysight 488 with third-party software.

FAQ 2010-09-08

IO Libraries Suite: What pieces of software do I need to install for the IO Libraries to work?
View the data sheet for the full list of requirements.

FAQ 2010-09-08

IO Libraries Suite: Is an IO Libraries Suite license transferable?
An IO Libraries Suite license can travel with the Keysight instrument, Keysight hardware I/O product or Keysight software…

FAQ 2010-09-08

1 2 다음