Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contact an Expert

Suporte técnico

Medição Eletrônica

Support by Product Model Number:

Refine the List

remove all refinements

By Topic

Mercado/Tecnologia

By Type of Content

Categoria de Produto

51-75 de 302

Sort:
What is the Max DC Input Voltage Before the Battery Charger Shuts Down?
21-22 Volts.

FAQ 2011-08-29

What are the rackmount accessories for an X-Series Signal Analyzer?
There are many different rackmount accessories that are compatible with the X-Series...

FAQ 2011-08-17

Can I use the electrical Infiniimax probes (1130A/31A/32A/34A) with the 86100 DCA modules?
Yes, the N1022A probe adapter allows the Infiniimax probes (1130A/31A/32A/34A) to be used with the 86100 DCA modules.

FAQ 2011-07-25

Why is the "E-230 data corrupt or stale" error message occasionally displayed on the E4980A while saving a measurement data in the USB memory stick...
It is caused when the procedure for saving a data is not performed correctly or when the USB memory stick is not compatible with the E4980A.

FAQ 2011-07-24

What is a recommended USB memory device for the E4980A and the E4981A?
4 GB USB Memory (Keysight PN 1819-0637) is recommended.

FAQ 2011-07-11

Which high impedance / differential probe can be used with the E5052A/B Signal Source Analyzer?
The 54006A 6 GHz Passive Divider Probe Kit, the 41800A Active Probe, U1818A/B Active Differential Probe, the 1134A InfiniimMax 7 GHz Probe, can be used with the E5052A/B Signal Source Analyzer.

FAQ 2011-06-13

How should a DC blocking capacitor be inserted between the 42941A probe and a DUT when a live DC voltage exists on the device?
It is recommended to insert a SMA DC blocking adapter between the furnished pin probe and 3.5-mm connector at the tip of the 42941A.

FAQ 2011-06-07

Can the 42941A probe be substituted for discontinued 41941A/B probe?
No, the 42941A cannot be substituted for the discontinued 41941A/B and doesn’t have compatibility with old 4194A analyzer.

FAQ 2011-06-07

Can the 16338A be used with LCR meters such as the 4263B and the E4980A?
No, the 16338A Test Lead Set doesn’t have compatibility with LCR meters. The 16338A can be used with the 4338A/B only.

FAQ 2011-06-07

How can the E4980A or the 4263B measure internal impedance of batteries?
Insert DC blocking capacitors between the measurement terminals and a battery DUT. The 16065C can substitute for the DC blocking capacitors.

FAQ 2011-06-07

Why is permeability measurement result unstable when a low permeability magnetic material or a thin magnetic material is measured with the 16454A?
It is because the impedance of the magnetic material inserted into the 16454A is too low for the impedance analyzer to measure it accurately.

FAQ 2011-06-07

Can the 42941A probe be used with any RF test fixture adapter?
No, the 42941A does not have any test fixture adapter available for connecting the probe to an RF component test fixture.

FAQ 2011-06-07

What is the possible cause of the difference when the permittivity measured with the 16453A is different from the value previously obtained?
Most likely cause of the measurement discrepancy or drift is insufficient electrode pressure due to improper pressure adjustment.

FAQ 2011-06-07

What is the interface cable or adapter required to control external GPIB equipment by using VBA macro function of the E4991A?
The 10833A/B/C/D, 82357A or 82357B is required depending on the OS version of the E4991A.

FAQ 2011-06-07

How do I change the power-line voltage setting of 34401A and what is the corresponding power-line fuse to be used?
The line voltage has been set to the proper value for your country when the multimeter is shipped from the factory...

FAQ 2011-06-05

What additional items are required to utilize the E4991A option 007 Temperature Characteristic Test Kit?
For newly purchased E4991As a Keysight 82357B USB-GPIB card is required as well as a GPIB interface on the temperature chamber. The recommended temperature chamber is an ESPEC model SU-261 temperature chamber.

FAQ 2011-05-31

Can I use the test fixture with B2900A?
Yes. The N1295A device/component test fixture is available for B2900A up to 42V.

FAQ 2011-05-18

What waveguide flanges do the M1970V and M1970W band external mixers have?
The waveguide flanges for the M1970V and M1970W (V & W Band) waveguide harmonic mixers are the same as the current legacy 11970V and 11970W mixers. The V band mixer uses the WR15 and WR10 is in the W band mixer.

FAQ 2011-04-26

What is the dielectric constant and material composition of the Keysight 33391C Microwave Insulator Bead Assembly?
The insulator bead is Noryl® modified Polyphenylene Oxide (PPO). The dielectric constant is 2.63-2.68.

FAQ 2011-04-21

Is there an external battery pack for the X-Series (PXA/MXA/EXA/CXA) Signal Analyzer?
Not at initial release.

FAQ 2011-03-24

Do I need a keyboard and mouse to operate the X-Series Signal Analyzers?
No. However, since this is a Windows-based instrument, it is easier to navigate various windows using a mouse.

FAQ 2011-03-24

How can I get the accessories (cables and adaptors) for measurement setup of the ENA & the E5092A?
All accessories are included in the option of the E5092A.

FAQ 2011-01-20

34970A: How do I add a DMM to a 34970A that does not have one installed?
Order the customer installable retrofit kit 34970-80100.

FAQ 2010-10-12

I lost some of the small parts of the N1021B probe kit. Can I get them without buying a whole kit?
The following items will be available from www.keysight.com ...

FAQ 2010-09-19

Which MXG signal generator parts are customer-replaceable?
See the Replaceable Parts chapter of N5161A/62A and N5181A/82A/83A MXG Signal Generators Service Guide

FAQ 2010-09-19

Voltar 1 2 3 4 5 6 7 8 9 10 ... Avançar