Contact an Expert

Technical Support

Spectrum Analyzers (Signal Analyzers)

Find by Product Model Number: Examples: 34401A, E4440A

226-250 of 838

Sort:
How do I remotely read the summary table for a demodulated Wireless LAN signal from the 89601A VSA software using Microsoft Excel?
Open the Excel file provided, select "Enable Macros" and follow procedure documented inside spreadsheet.

FAQ 2012-05-29

Does the E7495A/B Base Station Test Set allow simultaneous operation of the CW and complex source in Spectrum Analyzer mode, Channel Analyzer mode,...
Yes. This support was added for A.02.10 firmware in January 2004.

FAQ 2012-05-29

How can I upgrade my PSA Series Spectrum Analyzer to add Gated Sweep (Time gating)?
A hardware retrofit will be required before gated sweep can be used in PSA's purchased before September 2003 (Serial Prefix less than US4336 or MY4336 ). Firmware Release A.04.12 or greater is also needed.

FAQ 2012-05-28

What are the measurement intervals for the W-CDMA, cdma2000, and 1xEV-DO QPSK EVM measurements for E4406A and the PSA Series? Is the 12.2k Reverse ...
Click on this FAQ to get detailed information on the measurement interval ranges.

FAQ 2012-05-28

How do I remotely program my E4406A VSA Series Analyzer to transfer binary block data in Visual Basic 6?
Click here for information on transfering binary block trace data.

FAQ 2012-05-28

How do I optimize my cdmaOne ACPR measurement for the third offset (2.75 MHz offset, 1 MHz bandwidth) in the E4406A and PSA Series cdmaOne personal...
By changing the default number of FFTs segments to 5 and upgrading to the 14 bit digital IF (E4406A only) you can substantially improve your results.

FAQ 2012-05-28

Can I get a temporary license key for my PSA Series, ESA Series, or EMC Series Analyzer?
No. At this time, we do not have temporary licenses. License keys for these instruments are generated based on the serial number, model number, and Host ID.

FAQ 2012-05-28

What cdmaOne (Option BAC) radio standards and band classes are supported by the E4406A and PSA Series for the ACP and Spur Close measurements?
Radio standards IS-95A, J-STD-008, IS-97D and IS-98D are supported. The following Band Classes are supported to comply with IS-97D and IS-98D requirements: Band Class 0 (800MHz), Band Class 1 (1900MHz), Band Class 3 (JTACS), Band Class 4 (Korean ...

FAQ 2012-05-28

How do I upgrade the E4406A VSA Series 321.4 MHz IF Output Option 300?
This option can be upgraded at your local Keysight Service Center. (Click on this FAQ for more information)

FAQ 2012-05-28

How do I remotely transfer screen images from my ESA/PSA Series Spectrum Analyzer using Visual Basic 6?
Click here for information on transfering screen images.

FAQ 2012-05-28

For my ESA/PSA/EMC Series Spectrum Analyzer or E4406A VSA Series Analyzer how do I serial poll to determine when an auto-alignment is complete usin...
Click here for information on performing an alignment and using serial polling to determine when it is complete.

FAQ 2012-05-28

How do I upgrade the E4406A VSA Series Base Band I/Q Inputs Option B7C?
This option can be upgraded at your local Keysight Service Center. (Click on this FAQ for more information)

FAQ 2012-05-28

How do I perform WCDMA Power Control measurements on the E4406A or PSA Series Spectrum Analyzers?
Reverse link power control measurements can be made using the W-CDMA (Option BAF) power control measurement. Power control analysis on the downlink can be done in the Code Domain Power measurement using the Symbol Power vs. Time view.

FAQ 2012-05-28

How do I upgrade the E4406A VSA Series Firmware and Measurement Personalities?
The E4406A firmware and measurement personalites can be upgraded via the LAN or crossover cable. (Click on this FAQ for more information)

FAQ 2012-05-28

What file formats does the 89601A VSA software support for signal waveforms?
Recorded data from the following files can be interpreted by the 89600: ASCII (.txt and .csv), Binary (89600 SDF .sdf, .dat), Binary (E3238 .cap), Binary (N5510A .bin), MATLAB 7 (or earlier, .mat)

FAQ 2012-05-28

Does the E4406A or PSA Series Spectrum Analyzer provide GSM trigger to time zero (T0) timing in order to test Enhanced Observed Time Difference Tec...
Yes, the EDGE / GSM measurement personalities for the E4406A and PSA Series provide precise nanosecond timing between an external trigger and the training sequency T0 transition point. (click here for more details).

FAQ 2012-05-28

How many options can be loaded into my E4406A with A.06.03 firmware at one time?
With a 48 MB flash memory board, you can fit up to seven measurement personalities. To determine what will fit, add up the memory sizes of the personalities that you want. If the total is less than 19,225 kB then they will fit.

FAQ 2012-05-28

How do I upgrade the E4406A VSA Series iDEN Measurement Personality Option HN1?
This option can be upgraded via the LAN or crossover cable. (Click on this FAQ for more information)

FAQ 2012-05-28

Does the E4406A or PSA Series support GPRS measurements?
Both the E4406A and PSA Series support GPRS measurements. For the E4406A, option BAH (GSM) or option 202 (EDGE with GSM) are required. For the PSA, option 202 (GSM with EDGE) and option B7J (Digital Demodulation hardware) are required.

FAQ 2012-05-28

How do I remotely transfer screen images from my E4406A VSA Series Analyzer using Visual Basic 6?
Click here for information on transfering screen images.

FAQ 2012-05-28

Does my E4406A VSA Series Analyzer have a 14-bit digital IF or a 12-bit digital IF?
All Instruments with serial numbers that start with MY or that have serial numbers later than US41513009 were shipped with 14 bit digital IFs. You can also determine which digital IF assembly you have under the system key.

FAQ 2012-05-28

What transit case do I order for my E4406A VSA Series Analyzer?
The dimensions of the E4406A are 426 mm x 177 mm x 452 mm (16 3/4 in x 7 in x 17 7/8 in) without the removable feet. There are two System II Cabinet Style Transit Cases that Keysight sells that best fit the E4406A. (Click here for more info)

FAQ 2012-05-28

For the PSA Series and E4406A VSA Series 1xEV-DO measurement personality, why did the Modulation Accuracy (Composite Rho) measurement change names ...
In the cdma2000 standard, Rho is a common parameter name used to express modulation quality. However, 3GPP2 uses the term Waveform Quality in the 1xEV-DO conformance tests, and the 1xEV-DO measurement personality was updated to use the same termi...

FAQ 2012-05-28

Where can I find detailed specifications for the E4406A, PSA Series, ESA Series Spectrum Analyzers?
We publish both an abbreviated Data Sheet and complete Specifications Guide for these analyzers. You can find the complete specifications guide by looking under Manuals, Guides, and Notifications at the bottom of each product web page.

FAQ 2012-05-28

Do the E4406A, PSA Series and 89600 VSA Software report Peak Code Domain Error for W-CDMA and cdma2000?
Yes. The screen capture below shows a W-CDMA Modulation Accuracy measurement on the E4406A and PSA Series, and Peak Code Domain Error is reported in the results table.

FAQ 2012-05-26

Previous 1 2 3 4 5 6 7 8 9 10 ... Next