이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

상세 분류

클래스별

산업/기술

분야별 검색결과

제품 카테고리별

26-50 / 3424

정렬방식:
Get Segmented Memory Time Tags and Measurement Results, VISA COM library, VBA
This sample program assumes the oscilloscope has been set to capture N segments. The program lists the segment number and the relative time stamp of that segment. A Delay measurement is made between channels 1 and 2 within each segment and the measurement value from each segment is listed.

프로그램 예제 2017-04-28

ZIP ZIP 33.08 KB
Get Waveform Data, VISA COM library, VBA
This sample program gets waveform data from the oscilloscope.

프로그램 예제 2017-04-28

ZIP ZIP 1.01 MB
Get *IDN? Query Results, VISA COM library, C#
This sample program sends a *IDN? SCPI query to an instrument to get its identification string. The result is displayed on a MS Windows Console.

프로그램 예제 2017-04-28

ZIP ZIP 41.79 KB
Get Waveform Data (Brute Force), VISA library, Python
This script shows how to pull the waveform data from the analog channels for already acquired data and save it to a computer. It shows how to determine which channels are on and have data, how much data, get the data into an array, scale data for each channel, and save/recall it to/from disk in both csv and Python Numpy formats.

프로그램 예제 2017-04-28

ZIP ZIP 13.62 KB
Acquisition Synchronization, Two Simple Methods, MATLAB
This script shows how to properly initialize a Keysight InfiniiVision or InfiniiVision X-Series oscilloscope and synchronize an acquisition using the blocking :DIGitize command.

프로그램 예제 2017-04-28

ZIP ZIP 328.53 KB
N8836A PAM-4 Test Application Software and 30-Day Trial License
Keysight N8836A PAM-4 test application software for Infiniium Z-Series and 90000 Q-Series oscilloscopes.
이전 버전

계측기 펌웨어/소프트웨어 현재 버전: 03.00 | 2017-04-28

Get *IDN? Query, Screen Image, and Waveform Data Results, VISA COM library, VBA
This sample program performs three different tasks: 1) sends a *IDN? query to the instrument and reads back the ID string, 2) captures and saves a screen image from the oscilloscope, and 3) gets the oscilloscope's waveform data from channels 1 and 2.

프로그램 예제 2017-04-28

ZIP ZIP 1.30 MB
Get Waveform Data (Elegant), VISA library, Python
This script shows how to pull the waveform data from the analog channels for already acquired data and save it to a computer. It shows how to determine which channels are on and have data, how much data, get the data into an array, scale data for each channel, and save/recall it to/from disk in both csv and Python Numpy formats.

프로그램 예제 2017-04-28

ZIP ZIP 13.93 KB
Acquisition Synchronization, Two Simple Methods, VISA library, Python
This script shows the two best synchronization methods for all InfiniiVision and InfiniiVision X-Series oscilloscopes. Benefits and drawbacks of each method are described.

프로그램 예제 2017-04-28

ZIP ZIP 338.73 KB
Load Arbitrary Waveform Data into WaveGen, VISA library, Python
This example shows several methods for getting arbitrary waveform data into the waveform generator of a Keysight InfiniiVision X-Series oscilloscope. The oscilloscope must have the WaveGen license and support arbitrary waveforms.

프로그램 예제 2017-04-28

ZIP ZIP 6.08 KB
E5080A Network Analyzer Firmware Update
이전 버전

계측기 펌웨어/소프트웨어 현재 버전: A.12.55.02 | 2017-04-28

Get InfiniiVision Oscilloscope Screen Image, LabVIEW
This sample program captures and saves a screen image from the InfiniiVilsion oscilloscope.

프로그램 예제 2017-04-28

ZIP ZIP 48.93 KB
Save and Recall Setups, VISA library, Python
This script shows how to query the oscilloscope setup, save it to disk, recall it form disk, and use it to set up the oscilloscope again. This is also shown using the *LRN? query and with just trigger setups.

프로그램 예제 2017-04-28

ZIP ZIP 4.39 KB
MQA 소프트웨어
MQA를 사용하려면 먼저 라이센스를 구입한 후 다운로드해야 합니다.
이전 버전

컴퓨터 소프트웨어 현재 버전: 2017 | 2017-04-28

Get Screen Image, VISA library, Python (2.7)
This script shows how to save a screen image from an InfiniiVision oscilloscope to a PC.

프로그램 예제 2017-04-28

ZIP ZIP 3.27 KB
Get Waveform Data, LabVIEW
This sample program gets waveform data from the oscilloscope.

프로그램 예제 2017-04-28

ZIP ZIP 69.15 KB
N1085A PAM-4 Test Application Software and 30-Day Trial License
Keysight N1085A PAM-4 test application software for 86100D DCA-X oscilloscopes.
이전 버전

계측기 펌웨어/소프트웨어 현재 버전: 03.00 | 2017-04-28

Save Multiple Waveforms to a Binary File with Averaging, VEE
This sample program saves multiple waveforms to a binary file with averaging.

프로그램 예제 2017-04-28

ZIP ZIP 4.06 KB
Get Lister Data, VISA library, Python 3.5
This script is a reference and starting point for automating Lister data capture over USB.

프로그램 예제 2017-04-28

ZIP ZIP 4.21 KB
MBP 소프트웨어
MBP를 사용하려면 먼저 라이센스를 구입한 후 다운로드해야 합니다.
이전 버전

컴퓨터 소프트웨어 현재 버전: 2017 | 2017-04-28

Get InfiniiVision X-Series Oscilloscope Screen Image, LabVIEW
This sample program captures and saves a screen image from the InfiniiVilsion X-Series oscilloscope.

프로그램 예제 2017-04-28

ZIP ZIP 65.53 KB
Infiniium Series Oscilloscopes IVI and MATLAB Instrument Drivers
Supported models: 8000, 9000, 80000, 90000, 548xx, X, S, V, and Z Series
이전 버전

드라이버 현재 버전: 1.5.1.0 | 2017-04-26

키사이트 계측기 제어 번들 다운로드
IO Libraries Suite 17.2, Command Expert 1.5, BenchVue 3.0
이전 버전

컴퓨터 소프트웨어 현재 버전: 4.2017 | 2017-04-26

Keysight Instrument Control Bundle .iso Download
IO Libraries Suite 2017, Command Expert 2017, BenchVue 2017
이전 버전

컴퓨터 소프트웨어 현재 버전: 4.2017 | 2017-04-26

PXIe Vector Network Analyzer Firmware Update
이전 버전

계측기 펌웨어/소프트웨어 현재 버전: A.12.55.03 | 2017-04-25

이전 1 2 3 4 5 6 7 8 9 10 ... 다음