Here’s the page we think you wanted. See search results instead:

 

Sprechen Sie mit einem Experten

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 8072

Sort:
Solving your IoT Wireless Testing Challenges from NB-IoT to NFC
From design verification to manufacturing to conformance testing, simplify your IoT wireless testing with cross-platform measurement algorithms and one-button standard compliance measurement software.

FAQ 2017-07-20

Get to Market Faster with a Technology Refresh
Maximize test asset value while lowing cost, securing the right technology, and getting to market on time

FAQ 2017-07-13

What are the Keysight equivalent model numbers for Centellax BERT products and test accessories?
Click on the question for full details of the equivalent model numbers.

FAQ 2017-07-13

Where can I find online communities of Keysight EDA users?
Find us on LinkedIn, Keysight Forums, YouTube, YouKu, Facebook, Twitter, and Google+

FAQ 2017-07-12

Is calibration included in the 86100DU-WN7 Windows 7 upgrade?
86100DU-WN7 is a return to service center upgrade and does include calibration, in addition to a certificate of calibration and data.

FAQ 2017-06-28

How do I display the mixer conversion loss of M1970 Series or M1971 Series Harmonic Mixer on an X-Series Signal Analyzer?
There is no way to display the conversion loss values from these mixers on screen. There is a hard copy of the conversion loss data supplied with each mixer that can be referenced.

FAQ 2017-06-28

How do I send the UXM Error Logs to Keysight?
You can use the UXM’s Export Logs function to send the UXM platform log files to the Keysight support team. Click on the question for additional information.

FAQ 2017-06-28

I want to use multiple 2-port M9371A PXIe VNAs in my system. Is option 551 necessary?
If the modules are used as independent 2-port VNAs, no; however, option 551 is necessary to perform true, calibrated, multiport measurements. Click on the question for additional information.

FAQ 2017-06-28

For signals requiring wider bandwidth, how can Keysight’s LTE Signal Studio waveform creation products be used to increase carrier spacing?
Set the FFT length to 8192 and a sample rate of 800 MHz. Subcarrier spacing = sampleRate/FFT size

FAQ 2017-06-28

What is the time out limit of response time (2.4) in M8020A Interactive link training?
The LTSSM (Link Training and Status State Machine) implements the timeouts as specified in the PCIe specification. Click on the question for additional information.

FAQ 2017-06-28

Is it possible to develop specific macros for E5061B to support TRL cal or the unknown thru method under a 9-term calibration method?
Yes, it is possible to perform a user developed 8-term calibration, like TRL, using an external program for the E5061B. Click on the question for additional information.

FAQ 2017-06-28

Can the PNA-X support SSLT or SSST calibration techniques?
Yes; however, the Cal Kit must be defined properly to work. The Cal can be modified via Advanced Modify Cal Kit for Definitions under the Calibration menu.

FAQ 2017-06-28

How do I create a Mono FM Signal using N5182B MXG ARB?
You can configure N7611B Signal Studio Broadcast Radio to play a mono/FM signal.

FAQ 2017-06-28

Can Keysight’s PXIe VNAs be used with Non-Keysight PXI Chassis?
Yes, the M937xA can be successfully installed in a non-Keysight PXI chassis. Click on the question for additional information.

FAQ 2017-06-28

Is there a PDF version available of the user guide for the M9210A? There are issues with the .chm file that is available.
No, there is not a PDF version available for the M9210A user manual. To read the .chm file, it must be downloaded and copied on the local C drive before opening.

FAQ 2017-06-28

Is Option RTS a license key or hardware upgrade?
Option RTS is a hardware and license key upgrade. Therefore, this upgrade requires the analyzer to be returned to Keysight.

FAQ 2017-06-28

Does M9393A work without M9300? If so, when using the M9393A with 100MHz reference on a pulse generator, what is the external reference input voltage?
When replacing the M9300 with a pulse generator, self-test and alignments may pass. Click on the question for additional information.

FAQ 2017-06-28

If we use external clocks for both the Pattern Generator and Error Detector parts, can we run them at different data rates?
It would be more straight-forward to provide the PG (TX) with a 10 GHz clock (for 10 Gb/s data) and then use the 1:4 demux and provide the ED (RX) with a 2.5 GHz clock (measuring 2.5 Gb/s data). Click on the question for additional information.

FAQ 2017-06-28

I am using an electronic load to draw current into my DUT, but when I draw current the voltage drops. Why is this happening?
A voltage drop will appear across this impedance as current flows through it in accordance with Ohm’s Law. Click on the question for additional information.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

Can a CalPod system be used with the N1500A software?
No, the CalPod and N1500A Software are not compatible.

FAQ 2017-06-28

Is there a software application for the E5062A to calculate K factor?
No, there is not a software application to calculate K factor for the E5062A.

FAQ 2017-06-28

Where are the SDS’s (safety datasheets) for products located?
Product-related SDS (MSDS's) for all Keysight products are available from our customer facing Regulatory Compliance web page. If a product review on this website produces no SDS (MSDS) results, then this means there is no hazardous material associated with the product. For example, N9010A is not on the list.

FAQ 2017-06-28

Can antivirus programs run on the Windows based PNA-X?
Yes, antivirus programs can run on any Windows based machine.

FAQ 2017-06-28

1 2 3 4 5 6 7 8 9 10 ... Next