이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

데이터 수집 하드웨어 및 시스템 전환

모델 번호 입력:

1-25 / 83

정렬방식:
Is E5810B remote USB interface supported in NI MAX environment?
No. E5810B remote USB interface is not supportable in NI MAX environment. The E5810B remote USB interface only detectable in Keysight IO libraries Suite.

FAQ 2014-12-10

Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

Why are USB modular instruments (U2700 Series) and USB DAQ modules (U2300, U2500, U2600 Series) not detectable by the E5810B?
Establish the connection between the USB modular Instrument and the PC directly, and then disconnect the device from the PC (while it’s still powered-on), and connect to E5810B.

FAQ 2014-04-17

shielded wire를 34970A 플러그인 모듈에 어떻게 연결하나요?
이 질문에 두가지 답변이 있습니다. 1. 플라스틱 코팅으로 된 shielded wire를 사용하는 것이 가장 최선입니다. 측정면의 LO에 shield의 한쪽 끝에 연결합니다. 접지 loop error를 발생시키기 때문에 LO shield의 끝을 연결하지 않도록 해야합니다. 2. 다른 방법은 34970A의 뒤 패널의 스크루 샤시 접지(GPIB 인터페이스 콘넥터 근처에 위치)에 wire를 접지 연결하는 것입니다.

FAQ 2014-01-06

PC와 Keysight 34970A사이에 RS-232연결을 위해 어떤 COM포트를 사용하나요?
34970A RS-232포트는 당신의 PC의 어떤 RS-232포트와도 연결 할수 있습니다. Benchlink Datalogger는 PC가 COM1부터 COM4로 표시된 어떤 포트와 사용할 수 있도록 정상적으로 구성되어 있습니다. PC에 설치된 포트를 사용하여야하며 어떤 다른 프로그램을(PDA 소프트웨어 같은)사용하지 않아야 합니다.

FAQ 2014-01-06

What is the maximum total length of the RJ45 control cable for connecting multiple 34945EXTs?
The maximum total length of the RJ45 control cables is 140 feet.

FAQ 2013-05-06

What can I do if the Keysight USB Modular Instrument driver installations failed to complete installation on a Windows 7 environment?
If you encountered the event mentioned above, follow the installation best practices steps below.

FAQ 2012-07-25

What can I do if I fail to establish hardware connection after successfully installing Keysight USB modular instrument driver on a Win7 environment?
If you encountered the event mentioned above, follow the installation best practices steps below.

FAQ 2012-07-25

How many Keysight 34970A data acquisition units can be connected to a single PC at a time?
Only one Keysight 34970A can be connected for each RS-232 port on the PC. A GP-IB cable can be used to connect up to 15 units if the GP-IB cable is being referenced by the VEE software. The Benchlink Data Logger 3 software can support up to 4 units...

FAQ 2012-01-25

The Keysight 8761B SPDT Coaxial Switches are not listed in the "Keysight 34945A, L4445A and L4490A/L4491A Configuration Guide". Why?
Due to the 8761B’s internal design the RF path selection is achieved via DC polarity reversal across the coil control terminals. The Keysight 34945A, L4445A and L4490A/L4491A Control Units do not provide a polarity reversal mode. Thus the 8761B cannot be controlled by the 34945A, L4445A and L4490A/L4491A Control Units.

FAQ 2012-01-16

The Benchlink Data Logger Software is unable to see my 34970A even though it is connected, how do I correct this?

FAQ 2011-12-20

BenchLink DataLogger 3에서 "MDAC installation failed" 오류 메시지가 나타나는 이유는 무엇입니까?
MDAC(Microsoft Data Access Components)가 손상된 것일 수 있으며 복구가 필요합니다.

FAQ 2011-12-20

Can the same type modules be paired together to open/close corresponding switches at the same time?
Yes, here are a couple of examples: The N2280A (Quad 1x2) can be configured as two wire 1x2s using the "card pair" command. The N2281A (Dual 1x4) can be configured as 2x4s using the "card pair" command.

FAQ 2011-07-27

34970A: How do I add a DMM to a 34970A that does not have one installed?
Order the customer installable retrofit kit 34970-80100.

FAQ 2010-10-12

How can I input 28V digital signal to U2651A/U2652A when it support digital input voltage < 24V?
You can connect a voltage divider in front of the digital input to reduce the voltage to <24V

FAQ 2010-10-07

34980A 메인프레임의 일련 번호는 어디에 있습니까?
일련 번호는 34980A 후면 패널의 LAN 및 USB 커넥터 왼쪽에 있습니다.

FAQ 2010-09-15

Where can I get the drivers for the U2300A Series USB Data Acquisition (DAQ) devices?
The drivers for the U2300A Series Data Acquisition (DAQ) devices are available on the Keysight website….

FAQ 2010-09-08

A Windows® Logo warning message appears during the U2300A Series driver installation. What does this mean?
The Windows® Logo warning message appears if the U2300A Series driver does not have Microsoft® Windows® Logo certification...

FAQ 2010-09-08

NI GPIB 카드와 키사이트 GPIB 카드 및 컨버터는 같은 시스템에서 작동 가능 합니까? 같이 작동하기 위해서는 어떤 구성이 필요한가요?
예. 원하는 셋업에 따라 VISA나 Keysight 488 설정을 구성해야 할 수도 있습니다.

FAQ 2010-09-08

Matlab throw this error with U2300A/U2500A "??? Error using ==> daqhwinfo at 115 Failure to find requested data acquisition device: agilentu2500....
Please check whether your Matlab adaptor is installed at the following path:.....

FAQ 2010-08-09

If I set Channel 1 of U2300A/U2500A with voltage range of 5V, I get a reading of 4.99968 when nothing is connected to the DAQ.
If you don't have anything connected to the DAQ and you do an acquisition out of it, the result…

FAQ 2010-08-09

Why is my acquired data for U2300A and U2500A shifted? eg. Column 2 data is in column 1, column 3 data is in column 2, and so on.
Install DAQ hardware driver version 1.05 and above.

FAQ 2010-08-09

What is the clock rate for Digital Inputs(DI) and Digital Outputs(DO) of U23xxA and U25xxA USB Data Acquisition?
The DAQ DIO is not meant to measure DI with clock rate precision or to control frequency of digital output

FAQ 2010-07-18

I get error from the example "C:\Program Files\Keysight\RF Switch Driver\Examples\VS.NET\CSharp\Example1".
The temporary solution to this is to load the U2931A .dll file that was not loaded with the...

FAQ 2010-07-18

Transferring Data and Configurations to a new version or to a new computer
Moving between computers with same version or moving configurations and data to a new version on the same computer...

FAQ 2010-05-07

1 2 3 4 다음