Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

126-146 of 146

Sort:
Can I configure the 34970A for 4-wire resistance, 4-ohms, and/or 4-wire scan?
Yes, the 34970A can be configured for 4 wire resistance, 4 wire RTD or 4 wire external scanning.

FAQ 2006-08-29

How can I download/upload configuration to/from the 34970A?
Follow the procedures below to download and upload configuration to and from 34970A.

FAQ 2006-02-28

What is the difference between the 'latch' mode and 'track' mode on the Keysight 34970A's alarm output lines?
Configure the behavior of the alarm output lines to trigger external control system or hardware...

FAQ 2006-02-02

When I press the front panel [Measure] key, only two functions are available: 'SCANNED' and '4W SCAN'. Why?
The internal DMM is either disabled or it is not installed...

FAQ 2006-02-02

How long can I scan with the 34970A?
Limiting this question to the 34970A being used as a standalone datalogger, the answer is a function of the 50000 internal reading memory. If we scan one channel at the maximum scan interval of 100 hours, the memory will fill in 5 million hours.

FAQ 2006-01-18

Is there a way to control the digital to analog converter output of the Keysight 34907A Multi-function module with the BenchLink Data Logger 3 softw...
Yes. The BenchLink Data Logger 3 Software can be used to set a discrete value DAC output of the 34970A. However, the output cannot be included in the scan list.

FAQ 2006-01-18

Is there a way to show values on the axes of the strip chart in BenchLink Data Logger 3?
Yes! In the Quick Graph tab, choose Preferences and select "Show X-Axis Labels" then select "Apply" or "OK".

FAQ 2006-01-18

34970A: Why is the 34903A Circuit Diagram/Board Marked Normally Open (NO) and Normally Closed (NC)?
The NO and NC designation provide a reference for the channel OPEN and CLOSE commands.

FAQ 2005-05-09

34970A: Can I Operate the 34970A from a DC Source?
You can use an inverter capable of providing the correct power.

FAQ 2005-05-09

In the Keysight 34970A and its plug-in modules, what type of memory is used? How much memory is available? How do I clear the memory?
Everything you need to know about the memory used in the 34970A and its modules. Declassify your 34970A.

FAQ 2005-05-09

34970A: What is the default output of the digital port in the 34907A multifunction module?
The default level on the digital output port is 5 Vdc.

FAQ 2004-03-30

34970A: Can the voltage measurement float on the 34901A, 34902A or 34908A modules?
If the instruments specification is not exceeded, you can float a measurement.

FAQ 2004-02-02

34970A: Do the 34901A and the 34902A have a common ground?
No. The 34901A and 34902A provide isolated inputs to the internal DMM.

FAQ 2004-02-02

34970A: Can I disable the digital multimeter in the 34970A so that it can be used for switching only?
Yes it can, either using a remote command or using the front panel.

FAQ 2004-02-02

34970A: Can thermocouple measurements be set up on any channel of the 34901A/02A/08A?
Thermocouple measurements can be set up on the 34901A, 34902A, 34908A module cards.

FAQ 2003-12-05

34970A: How can I turn off the 34970A's beeping noise?
There is no way to disable the beep sound in the 34970A.

FAQ 2003-12-02

34970A: Where do I hook up my external DMM?
External instruments must be connected via a module card.

FAQ 2003-12-02

34970A: What is the "thermocouple check" feature of the Keysight 34970A?
The "thermocouple check" is a feature in the 34970A that checks for the presence of a good thermocouple connected to a specified channel on a 34901A, 34902A and 34908A module.

FAQ 2003-12-02

34970A: Is there a recommended way to connect to "Earth Ground" on the 34970A?
Earth ground is connected to the 34970A through the "third" wire on the power cord.

FAQ 2003-12-01

34970A: What is wrong with Channels 07 and 11 in my 34901A Module?
There is an extra screw terminal at both ends of the connector strip.

FAQ 2003-11-24

34970A: Can I Assign Multiple Alarms to the Same Channel on the Keysight 34970A Modules?
You cannot assign alarm limits on a specific channel to more than one alarm number.

FAQ 2003-11-20

Previous 1 2 3 4 5 6