이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

데이터 수집 하드웨어 및 시스템 전환

모델 번호 입력:

226-250 / 407

정렬방식:
How many U2781A modular chassis can be connected via USB at the same time?
USB has a limit of 127 device connections. Theoretically, about 18 chassis can be connected at a time.

FAQ 2008-09-24

What are the maximum sampling rates for the U2531A, U2541A and U2542A Data Acquisition (DAQ) devices?
The maximum sampling rates for the U2531A, U2541A and U2542A Data Acquisition (DAQ) devices are:….

FAQ 2008-09-24

Which thermocouple types are compatible with the U2802A Thermocouple input device?
Eight standard thermocouple types defined in the NIST ITS-90 Thermocouple Database are compatible with the U2802A input device….

FAQ 2008-09-24

What programming platforms are compatible with the U2300A Series Data Acquisition (DAQ) devices?
Keysight VEE, LabView, Microsoft Visual Studio and C++ are compatible with the U2300A Series Data Acquisition (DAQ) devices.

FAQ 2008-09-24

Can the U2300A/U2500A Series Data Acquisition (DAQ) devices that are used with three modular chassis be synchronized?
Yes, the U2300A and U2500A Series Data Acquisition (DAQ) devices that are used with three modular chassis can be synchronized….

FAQ 2008-09-24

Is calibration required for the U2651A/U2652A/U2653A Digital I/O device?
No, calibration is not required for the U2651A, U2652A and U2653A Digital I/O devices.

FAQ 2008-09-24

Why should I use the U2802A Thermocouple input device?
The U2802A Thermocouple input device offers you a complete temperature measurement solution when used with data acquisition (DAQ) devices….

FAQ 2008-09-24

Can the Measurement Manager (AMM) display multiple U2781A modular chassis on the same application window?
No, the Measurement Manager (AMM) can only display one U2781A modular chassis on one application window…

FAQ 2008-09-24

How do I connect external sensors to the U2300A Series Data Acquisition (DAQ) devices?
External sensors can be connected to the U2300A Series Data Acquisition (DAQ) devices through the U2901A or U2902A terminal block….

FAQ 2008-09-24

Where can I get the terminal pin configuration for each model of the U2300A Series USB Data Acquisition (DAQ) devices?
The terminal pin configuration for each model of the U2300A Series USB Data Acquisition (DAQ) devices can be found in the User’s Guide….

FAQ 2008-09-24

When using the U2300A Series DAQ devices, how many channels can the Measurement Manager (AMM) display?
The Measurement Manager (AMM) can display all 16 or 64 channels depending on the model of the U2300A Series DAQ device selected….

FAQ 2008-09-24

Can the U2531A/U2541A/U2542A Data Acquisiton device work in both Single-Ended and Differential mode?
No, the U2531A, U2541A and U2542A Data Acquisiton devices cannot work in both Single-Ended and Differential mode….

FAQ 2008-09-24

What is the expected transfer rate over the U2781A USB Modular Instrument Chassis?
The transfer rate of the U2781 is dependent on the type of USB Data Acquisition (DAQ) Modules installed and the number of channel counts….

FAQ 2008-09-24

Can the Measurement Manager (AMM) application software be used to control all six USB Data Acquisition (DAQ) devices in a modular chassis?
Yes, the Measurement Manager (AMM) can be configured to control all USB Data Acquisition (DAQ) devices in the chassis.

FAQ 2008-09-24

Are there any sample programs provided for the U2300A and U2500A Series Data Acquisition (DAQ) devices?
Yes, sample programs of VEE, LabView and Microsoft® Visual Studio® are available for the U2300A and U2500A Series Data Acquisition (DAQ)….

FAQ 2008-09-24

What is the maximum torque force allowable on the 82350B GPIB card connector?
The maximum torque force allowable when attaching a GPIB cable to the 82350B GPIB card connector is 8 in. lbs.

FAQ 2008-09-24

Can the Measurement Manager (AMM) display more than 10 channels for synchronization?
No, the Measurement Manager (AMM) cannot display more than 10 channels for synchronization….

FAQ 2008-09-22

Keysight IO Libraries Suite 14.2 외에 별도의 드라이버가 있어야 82357B가 작동합니까?
82357B는 Keysight IO Libraries Suite 14.2와 호환되나 외장형 드라이버를 설치해야 합니다. 사용자들은 82357B와 함께 들어있는 CD에서 드라이버를 설치하거나 웹사이트에서 드라이버를 다운로드할 수 있습니다.

FAQ 2008-09-22

How do I connect the 33210A or 33220A to a PC via the USB port?
Install IO Libraries. Connect instrument. When prompted select “display a list of known drivers…”

FAQ 2008-09-01

Can I Perform Open/Short Test Using 34980A?
Yes. There are two ways you can setup using the 34980A to perform this test.

FAQ 2008-06-25

Ca Keysight build my custom L4490A/L4491A solution?
Please visit "/find/AD-systems" or see Keysight’s Channel Partners and Solution Providers at "/find/channelpartner"

FAQ 2008-04-07

Can I assign names to switches when using the L4490A/L4491A?
Yes. At the web interface, right click on the switch to assign a name.

FAQ 2008-04-07

Can I record the L4490A/L4491A I/O traffic?
Yes, select the "System Overview" button in the web browser to "Generate Report".

FAQ 2008-04-07

34970A: 키사이트 34970A 모듈의 한 채널에 여러개의 알람을 설정할수있나요?
특정한 한채널에 1개이상의 알람을 설정할 수는 없습니다.

FAQ 2008-04-07

Does the L449XA have universal AC power input?
Yes, 100 Vac to 240 Vac +/- 10%, 50-60Hz.

FAQ 2008-04-07

이전 1 2 3 4 5 6 7 8 9 10 ... 다음