Here’s the page we think you wanted. See search results instead:

 

Parla con un Esperto

Technical Support

Data Acquisition – DAQ

Support by Product Model Number:

126-150 of 407

Sort:
How can I open a configuration from a different data logger application?
See “Import Data Logger 3 Configuration”, or “Import Data Logger for 34980A Configuration”, or “Packages” in the Help menu for detail.

FAQ 2010-05-05

How do I set channel limits?
On the “Configure Scan Lists” tab, after configuring a channel's measurement function, you can set limits by clicking in the channel's Limit Type column.

FAQ 2010-05-05

How do I acquire and install a license?
After the evaluation period, you must license BenchLink Data Logger Pro as described below.

FAQ 2010-05-05

Can I start a scan and then close Data Logger Pro and continue scanning?
Yes. However, there are some limitations.

FAQ 2010-05-05

How do multiple scan lists appear in a datalog?
Multiple scan lists are stored by Data Logger Pro in the same datalog.

FAQ 2010-05-05

How can I tell if my PC is licensed?
In Data Logger Pro, click Tools > Licensing > License Status... The “License Status” dialog box displays your PC's license status.

FAQ 2010-05-05

How do I start a scan when using multiple scan lists?
Scanning always starts with the Base scan list.

FAQ 2010-05-05

What is an Action Script and what can I do with it?
An Action Script contains one or more action steps that perform actions on modules in 34970A/34980A instruments, and other instrumentation connected to the PC.

FAQ 2010-05-05

Can I rename an instrument instead of using the default Instr1, Instr2... naming convention?
Yes. Click on InstrN in the Name column of the “Configure Instruments” tab and enter a new instrument name.

FAQ 2010-05-05

How do I branch from one scan to another?
The Stop the scan and start the scan on action on the “Configure Events” tab, allows you to branch to another scan list on the occurrence of the corresponding event.

FAQ 2010-05-05

What is the Base scan list?
The default scan list is named Scan List A and is the Base scan list.

FAQ 2010-05-05

I don't have channels wired-up yet. How can I experiment with Data Logger Pro?
You can view getting started “simulations” by clicking Help > Start Simulation Mode and selecting a simulation from the list.

FAQ 2010-05-05

Can I export data while scans are running?
Yes, select Automatically export to .csv during scan in the “Export Data Preferences” dialog box.

FAQ 2010-05-05

How is licensing implemented for Data Logger Pro?
To run the Data Logger Pro software after the evaluation period, you must have a license for each PC using the software.

FAQ 2010-05-05

Can I send an email following a scan or on some event?
Yes. You can use a notification to execute an external program or batch file in response to an event.

FAQ 2010-05-05

How do I control instruments using SCPI commands?
You can use Action Scripts and SCPI commands to control any instrument connected to the PC.

FAQ 2010-05-05

How do multiple instruments affect the scan list?
Multiple instruments are integrated seamlessly into a scan list.

FAQ 2010-05-05

Can I reduce data while scanning?
No. All scanned data is saved in the datalog.

FAQ 2010-05-05

How can I update the 34980A to Firmware Revision 2.19?

FAQ 2010-05-05

What are channel limits?
Limits can be set on multiplexer, totalizer and digital read channels (see the limit types question below).

FAQ 2010-05-05

Are there separate licenses for 34970A and 34980A instruments?
Yes. Each instrument uses a specific Data Logger Pro product number.

FAQ 2010-05-05

How can I move a complete configuration from one PC to another?
You can do this by creating a package, move the package to the new PC then read the package in.

FAQ 2010-05-05

Can I be scanning and run an Action Script at the same time (in parallel)?
No. Scan lists and Action Scripts are executed sequentially

FAQ 2010-05-05

Can I run two scan lists at the same time (in parallel)?
No. Scan lists can only be run sequentially

FAQ 2010-05-05

Is there a pictorial or tabular representation available for my scan lists, events, Action Scripts, and notifications?
Yes.

FAQ 2010-05-05

Previous 1 2 3 4 5 6 7 8 9 10 ... Next