Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-13 of 13

Sort:
Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

What is the best way to ensure simultaneous triggering of multiple units of modular products?
Using the cardcage, U2781A is the best way of ensuring simultaneous triggering of multiple units

FAQ 2010-12-20

How do I extract the 32Mpts from U270xA?
One way of “viewing” the full memory waveform is using the zoom function (that the red arrow...

FAQ 2010-09-14

Why is my acquired data for U2300A and U2500A shifted? eg. Column 2 data is in column 1, column 3 data is in column 2, and so on.
Install DAQ hardware driver version 1.05 and above.

FAQ 2010-08-09

When I sent commands using VISA (Both Keysight VISA and NI VISA), why must i put '\n' or '\r' after the commands for U2600A…
Please upgrade your U2600A firmware to version 1.05 or above

FAQ 2010-08-09

Matlab throw this error with U2300A/U2500A "??? Error using ==> daqhwinfo at 115 Failure to find requested data acquisition device: agilentu2500....
Please check whether your Matlab adaptor is installed at the following path:.....

FAQ 2010-08-09

Why do we see unused port in U2300A/U2500A with similar waveform and frequency but with lower amplitude to its adjacent or close by used port?
It is recommended to ground all the AI connection that is not being used. If you have multiples of AI channels to be used, one good way is to have…

FAQ 2010-08-09

No Title
Instead of the ("Counter value"/"48 x 10^6") as the duration in seconds taken to count, it is...

FAQ 2010-05-10

Is number of bits the only factor to look at if I'm measuring at very low voltage say 5mVpp?
No it is not. Often times, you will have to look at the Gain Error and Offset Error as well as...

FAQ 2010-05-10

Why USB modular instruments (U272XA, U2741A, U2751A and U2761A) is not detectable by E5813A?
PC is failed to enumerate the USB modular instrument.

FAQ 2010-04-09

Is there any special setting that I need to do in Keysight VEE before using the U2300A or U2500A DAQ with it?
Yes. In fact it is the most important thing you need to set before using the DAQ with Keysight VEE. As most instruments uses MSB byte ordering, DAQ...

FAQ 2009-12-15

What is the main difference between the digital output (DO) of the U2100A, U2600A, U2300A and U2500A?
The DO port of U2100A and U2600A requires external power supply to be pumped into the port...

FAQ 2009-10-20

Why do I receive an error message below ?
Generally, if you are sampling at 60kSa/s and above, you should use high sampling mode to acquire data. This is just a rough guideline. If you encountered this message even when....

FAQ 2009-08-06