Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

PXI / AXIe / DAQ & Modular Solutions

Support by Product Model Number:

Refine the List

remove all refinements

By Topic

By Type of Content

By Product Category

26-50 of 132

Sort:
If I set Channel 1 of U2300A/U2500A with voltage range of 5V, I get a reading of 4.99968 when nothing is connected to the DAQ.
If you don't have anything connected to the DAQ and you do an acquisition out of it, the result…

FAQ 2010-08-09

What is the clock rate for Digital Inputs(DI) and Digital Outputs(DO) of U23xxA and U25xxA USB Data Acquisition?
The DAQ DIO is not meant to measure DI with clock rate precision or to control frequency of digital output

FAQ 2010-07-18

I get error from the example "C:\Program Files\Keysight\RF Switch Driver\Examples\VS.NET\CSharp\Example1".
The temporary solution to this is to load the U2931A .dll file that was not loaded with the...

FAQ 2010-07-18

Transferring Data and Configurations to a new version or to a new computer
Moving between computers with same version or moving configurations and data to a new version on the same computer...

FAQ 2010-05-07

How can I move a complete configuration from one PC to another?
You can do this by creating a package, move the package to the new PC then read the package in.

FAQ 2010-05-05

How many instruments can I have in a configuration?
You can have up to two 34980As or four 34970As in a configuration

FAQ 2010-05-05

Can I rename an instrument instead of using the default Instr1, Instr2... naming convention?
Yes. Click on InstrN in the Name column of the “Configure Instruments” tab and enter a new instrument name.

FAQ 2010-05-05

How do multiple instruments affect the scan list?
Multiple instruments are integrated seamlessly into a scan list.

FAQ 2010-05-05

Why USB modular instruments (U272XA, U2741A, U2751A and U2761A) is not detectable by E5813A?
PC is failed to enumerate the USB modular instrument.

FAQ 2010-04-09

Transferring Data and Configurations to a new version or to a new computer
Moving between computers with same version or moving configurations and data to a new version on the same computer:

FAQ 2010-03-30

Is U2722A compatible with E5813A?
No

FAQ 2010-03-22

Is U2723A compatible with E5813A?
No

FAQ 2010-03-22

Is there any special setting that I need to do in Keysight VEE before using the U2300A or U2500A DAQ with it?
Yes. In fact it is the most important thing you need to set before using the DAQ with Keysight VEE. As most instruments uses MSB byte ordering, DAQ...

FAQ 2009-12-15

I've written my own text format for SCPI in *.txt. How do I use these for SCPI completion within VEE 9.0. What tool should I use?
You can use the tool found within Keysight.com. Just search using the keyword "Keysight VEE SCPI...

FAQ 2009-11-12

VEE 9.0 has SCPI completion. How do I make my own SCPI command built-in with VEE?
Please refer to the attached Microsoft Word document for a step by step explanation...

FAQ 2009-11-12

What is the main difference between the digital output (DO) of the U2100A, U2600A, U2300A and U2500A?
The DO port of U2100A and U2600A requires external power supply to be pumped into the port...

FAQ 2009-10-20

IO Libraries Suite: Can software written from other vendors specific to their devices that utilize NI-488.2 as an I/O Library work with a Keysight ...
Yes, it is possible with Keysight IO Library version 14.1 and greater.

FAQ 2009-08-25

How can I remotely connect to all my USB DAQ devices, Digital IOs, and card cage?
Please make sure that your remote PC (which is connected to all your USB instruments) is connected to the same network as yourself. However, your remote PC cannot be connected...

FAQ 2009-08-06

Can I save on the 34970A data synchronously during a scan?
Yes.

FAQ 2009-03-12

Can the U2802A Thermocouple input device work with all the USB Data Acquisition (DAQ) models?
No. The U2802A Thermocouple input device can only be used with the U2355A or U2356A USB data acqusition (DAQ) model.

FAQ 2008-09-25

How many U2781A modular chassis can be connected via USB at the same time?
USB has a limit of 127 device connections. Theoretically, about 18 chassis can be connected at a time.

FAQ 2008-09-24

Where can I get the terminal pin configuration for each model of the U2300A Series USB Data Acquisition (DAQ) devices?
The terminal pin configuration for each model of the U2300A Series USB Data Acquisition (DAQ) devices can be found in the User’s Guide….

FAQ 2008-09-24

Can the U2531A/U2541A/U2542A Data Acquisiton device work in both Single-Ended and Differential mode?
No, the U2531A, U2541A and U2542A Data Acquisiton devices cannot work in both Single-Ended and Differential mode….

FAQ 2008-09-24

What is the maximum torque force allowable on the 82350B GPIB card connector?
The maximum torque force allowable when attaching a GPIB cable to the 82350B GPIB card connector is 8 in. lbs.

FAQ 2008-09-24

Which thermocouple types are compatible with the U2802A Thermocouple input device?
Eight standard thermocouple types defined in the NIST ITS-90 Thermocouple Database are compatible with the U2802A input device….

FAQ 2008-09-24

Previous 1 2 3 4 5 6 Next