이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

상세 분류

상세분류 제거

주제별

분야별 검색결과

제품 카테고리별

1-23 / 23

정렬방식:
When automating markers on the ENA is it possible to programmatically query the indicated inductance or capacitance on a Smith Chart?
The inductance / capacitance information cannot be directly queried via the automation interfaces. The inductance (positive reactance, top half of the Smith Chart) or capacitance (negative reactance, lower half of the Smith Chart) is not available as an automation query.

FAQ 2014-08-11

ENA 6 시리즈는 주파수 스윕할 때 swept sweep 모드를 지원합니까?
아니요..

FAQ 2013-04-25

What is the difference between an "ECal Confidence Check" and a Network Analyzer "System Verification" test?
The ECal Confidence Check is a method to check the accuracy of a calibration performed with either a mechanical cal kit or an ECal module. System verification testing provides network analyzer users a method to verify that the network analyzer is ...

FAQ 2012-12-18

Is it possible on the Keysight ENA series Network Analyzers to over-ride the output source blanking at every sweep end?
Yes, the output source blanking on sweep retrace can be prevented by turning off the Initial Source Port Control function.

FAQ 2012-12-18

What are the implications of swapping test heads between different Keysight 4287A Impedance Analyzers?
The Keysight 4287A Impedance Analyzer must be used with the furnished test head as a set because it is an indivisible portion of the calibrated 4287A.

FAQ 2012-01-16

How is trace math implemented within the Keysight Technologies Vector Network Analyzers?

FAQ 2012-01-11

키사이트 ENA-시리즈 E5071C 네트워크 분석기에서 글자 크기를 바꿀 수 있는가?
예, E5071C 네트워크 분석기에서는 디스플레이 주석 글자 크기를 바꿀 수 있습니다.

FAQ 2011-10-07

Does the touchstone file generated by the ENA / ENA-L include the electrical delay?
The touchstone files do not include electrical delay. Please use port extension.

FAQ 2011-10-07

키사이트 네트워크 분석기에서 둔화(Smoothing)와 평균화의 차이는 무엇입니까?

FAQ 2011-10-07

On the ENA, how can I make CW sweep (Fixed frequency) without turning off the ENA's output signal each time a sweep finishes?
Turn off the "Init Src Ctrl" feature, then hold trigger.

FAQ 2011-10-07

When I save a Touchstone file with the ENA / ENA-L, which calculation will be reflected in the Touchstone file?
All calculations are reflected in the Touchstone file except for the mixed-mode conversion.

FAQ 2011-10-07

벡터 네트워크 분석기와 관련하여 “스위프 속도”, “cycle time”과 “time per data point” 간의 차이점은 무엇입니까?

FAQ 2011-10-07

How can I calculate the equivalent phase delay, as a function of frequency, for a given electrical delay as set on Vector Network Analyzer?
Equivalent phase delay, based upon electrical delay is computed as: θ˚ = Ftest * Delay * 360

FAQ 2011-10-07

“set Zo” 함수는 네트워크 분석기의 표시된S-파라미터에 영향을 미치지 않는 것처럼 보입니다.이 함수를 작동시키는 방법은 무엇입니까?

FAQ 2011-10-07

실수와 허수 데이터 쌍(디스크 저장, GPIB 인터페이스 또는 디스플레이 마커에서 읽어 들인 값)을 로그 크기, 극상, 위상 및 Smith 차트 형식과 관련시키는 방정식은 무엇입니까?

FAQ 2011-10-07

On the ENA / ENA-L, what occurs if I select "order-based display" in sweep mode?
Measurement points of different segments are plotted in constant intervals.

FAQ 2011-10-07

Using the VBA program, can the ENA / ENA-L control the handler interface to control other peripherals?
Yes.

FAQ 2011-10-07

For Cable Testing should I use a TDR, a network analyzer, or both?
The cable specifications will determine the test equipment requirements...

FAQ 2011-10-07

키사이트 LCR 미터를 통한 캐패시터 측정 시 Cs 혹은 Cp 중 최상의 회로 모드는 어느 것입니까?

FAQ 2010-09-30

키사이트 4395A/4396B 결합 분석기를 노이즈 형식의 스펙트럼 분석기 모드에서 사용하고 있습니다. 단위는 V(전압)으로 설정되어 있는데 마커는 ‘nV / Hz’로 표시되어 있습니다. 표시된 단위는 이 모드에서 오류가 발생한 것입니까?

FAQ 2010-07-02

Our 4395A displays "Caution: CONT switching may damage Mech switch.". How should I repair?
The 4395A does not need repair.

FAQ 2008-06-27

키사이트 임피던스 분석기로 캐패시터를 측정하는 중에 Q와 D가 음수 값임을 알게 되었습니다. 어떻게 해야 하나요?
손실률이 낮은 디바이스(Q는 높음, D는 낮음)에서는 LCR 미터/임피던스 분석기에서 음의 값을 판독하는 일은 특별한 것이 아닙니다. 음의 값은 물리적으로 불가능하며(수동 소자일 경우) 이와 관련한 설명은 다음과 같습니다.

FAQ 2007-11-18

임피던스 Tangent Delta 측정에 어떤 절차를 권장합니까?

FAQ 2005-06-07