您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

縮小範圍

移除所有細分

依主題

依內容類型

依產品分類

1-25 / 164

排序:
How do I get replacement parts for individual items in the training kit?
Here are the parts that need to be purchased from Keysight at www.keysight.com/find/parts

FAQ 2017-02-26

Firmware update error with "Cannot Open another Window"
I cannot update the firmware with the error message; "Cannot Open another Window"

FAQ 2016-08-04

Does 34450A supports multiple measurements per trigger event?
No.

FAQ 2016-02-29

How do I find the calibration code and security code for my DMM?
The factory set security code is 'AT3446XA'. This is sometimes referred to as the calibration code.

FAQ 2015-11-21

Is DCV ratio measurement for 34401A and 34461A identical?
Yes. 34461A is intended as direct replacement for 34401A. Hence, the ratio measurement...

FAQ 2015-09-21

Can I enable 34450A data logger feature with programming command?
No. To enable data logging, execute "Enable log" at front panel...

FAQ 2015-09-21

How to enable 34410A/34411A/L4411A browser web control work in Java 8?
To enable browser web control to work in Java 8, update instrument to firmware version 2.41...

FAQ 2015-09-21

Why 34405A can't be detected in Windows 7?
There are two posibilities causing 34405A couldn't be detected. 1. IO Libraries Suit 15.1 or below...

FAQ 2015-09-21

Can 34460 & 34461A measure capacitance?
Yes. This feature is available when the DMM is upgrade to firmware revision 2.08 and above....

FAQ 2015-09-21

What is the calibration password to unlock the instrument?
The security code is "AT3446XA"...

FAQ 2015-09-21

What is the operating temperature range for 34138A test lead set?
The operating temperature range is limited to the DMM model with which it is used....

FAQ 2015-08-21

Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

What specification adder should be applied when performing Ohms measurements with OCOMP off?
Information on applying the Ohms specification with OCOMP OFF and OCOMP ON.

FAQ 2014-04-27

Why are USB modular instruments (U2700 Series) and USB DAQ modules (U2300, U2500, U2600 Series) not detectable by the E5810B?
Establish the connection between the USB modular Instrument and the PC directly, and then disconnect the device from the PC (while it’s still powered-on), and connect to E5810B.

FAQ 2014-04-17

Can I have multiple math functions (Null, Min-Max, dB, dBm, Limit) on at the same time on the 34401A?
No, the 34401A only allows one math function to be used at a time.

FAQ 2014-04-15

Can I set a measurement interval on the U1251A and U1252A Handheld Digital Multimeters?
Yes, you can set a measurement interval on the U1251A and U1252A Handheld Digital Multimeters….

FAQ 2013-11-17

Can I use a normal USB cable for datalogging with the U1250A Series Handheld Digital Multimeters?
No, you cannot use a normal USB cable for datalogging with the U1250A Series Handheld Digital Multimeters…..

FAQ 2013-11-17

Can I measure temperature with the 34405A Digital Multimeter using a thermocouple probe?
No, you cannot use a thermocouple probe to measure temperature with the 34405A Digital Multimeter….

FAQ 2013-11-17

Can HyperTerminal be used with the U1251A/U1252A Handheld Digital Multimeter?
No, HyperTerminal cannot be used with the U1251A and U1252A Digital Multimeter….

FAQ 2013-11-17

Can I have multiple math functions (Null, Min-Max, dB, dBm, Limit) turned on at the same time on the 34405A Digital Multimeter?
No, you cannot have multiple math functions (Null, Min-Max, dB, dBm, Limit) turned on at the same time on the 34405A Digital Multimeter….

FAQ 2013-11-17

Can I measure temperature with the 34405A Digital Multimeter?
Yes, you can measure temperature with the 34405A Digital Multimeter….

FAQ 2013-11-17

How do I view min-max values with the 34405A Digital Multimeter?
To view min-max values with the 34405A Digital Multimeter, press the ‘MnMx’ button….

FAQ 2013-11-17

Can I select the 34405A Digital Multimeter's front/rear terminals using a software command?
No, the 34405A Digital Multimeter only provides front terminal.

FAQ 2013-11-17

How do I start using the software provided with the 34405A Digital Multimeter for datalogging?
Follow the steps given here to begin datalogging using the software provided with the 34405A Digital Multimeter:….

FAQ 2013-11-17

Can I use the test probe leads marked with CAT III 1000V rating come together with the U1241A/U1242A/U1251A/U1252A/U1253A handheld Multimeter…
The test lead kit which currently marked with CAT III 1000V rating can be used with the multimeter at CAT IV 600V measurement environment...

FAQ 2013-11-17

1 2 3 4 5 6 7 下一頁