与专家交流

技术支持

已停产的频谱分析仪产品 [已停产]

按产品型号查找: 示例:34401A,E4440A

1-25 / 58

排序:
How can I get correct Log Frequency Scale Trace Data Using IntuiLink or BenchVue with my ESA Series Spectrum Analyzer?
Save the trace as a .csv file

FAQ 2014-03-13

How do I use the Service Request method (SRQ) to determine if the X-Series, ESA and PSA Signal Analyzers measurement is complete or has an error me...
Click here for information on the Service Request query to determine when a measurement is complete.

FAQ 2013-06-25

如何对频谱或矢量信号分析仪进行远程编程?
下面的信息可能会给您对是德频谱分析仪进行远程编程提供有益的帮助。

FAQ 2013-05-16

How do I remotely program my PSA Series Spectrum Analyzer or E4406A VSA Series Analyzer to transfer Raw I/Q trace data using the IVI-COM driver in...
Click here for information on transfering Raw I/Q trace data using IVI-COM and .NET.

FAQ 2012-05-29

How do I remotely program my PSA Series Spectrum Analyzer or E4406A VSA Series Analyzer to read ASCII trace points without using an instrument driv...
Click here for an example demonstrating how to over LAN read ASCII trace points of an entire EDGE waveform in the GSM w/ EDGE personality Power Vs. Time measurement.

FAQ 2012-05-29

How do I remotely make an Adjacent Channel Power (ACP) measurement with the 89601A VSA software using Microsoft Excel?
Click here for information on controlling the 89601A software using Excel to make an ACP measurement.

FAQ 2012-05-29

How do I remotely read demodulated symbols from the 89601A VSA software using Microsoft Excel?
Click here for information on reading demod symbols from the 89601A software using Excel.

FAQ 2012-05-29

How do I remotely read status bits and set interrupts for the 89601A VSA software using Microsoft Excel?
Save the self-extracting archive to disk, open it and click unzip to extract the 89600_Status_Bits.xls and ACP.sdf files to your C:\temp directory.

FAQ 2012-05-29

How do I remotely read the summary table for a demodulated Wireless LAN signal from the 89601A VSA software using Microsoft Excel?
Open the Excel file provided, select "Enable Macros" and follow procedure documented inside spreadsheet.

FAQ 2012-05-29

How do I remotely program my E4406A VSA Series Analyzer to transfer binary block data in Visual Basic 6?
Click here for information on transfering binary block trace data.

FAQ 2012-05-28

For my ESA/PSA/EMC Series Spectrum Analyzer or E4406A VSA Series Analyzer how do I serial poll to determine when an auto-alignment is complete usin...
Click here for information on performing an alignment and using serial polling to determine when it is complete.

FAQ 2012-05-28

What file formats does the 89601A VSA software support for signal waveforms?
Recorded data from the following files can be interpreted by the 89600: ASCII (.txt and .csv), Binary (89600 SDF .sdf, .dat), Binary (E3238 .cap), Binary (N5510A .bin), MATLAB 7 (or earlier, .mat)

FAQ 2012-05-28

How do I remotely transfer screen images from my E4406A VSA Series Analyzer using Visual Basic 6?
Click here for information on transfering screen images.

FAQ 2012-05-28

如何使用电脑上的VEE软件远程操作ESA、EMC或者PSA系列频谱分析仪将屏幕图像导入文件?
如欲了解详情,请参见上下文……

FAQ 2012-03-16

How can I transfer trace data from the 89400 VSA to my PC?
The VSA always saves data in standard data format; the utility is run from the DOS prompt.

FAQ 2012-02-25

What is the correct cable to use with the ESA Series for RS-232 communication?
Part number RS232-61601

FAQ 2012-02-25

有没有一种取样程序,捕获Keysight 8560系列频谱分析仪HPGL绘图仪输出,并通过GPIB总线传送到个人电脑的文件中?
有。所附文件“HPGL绘图仪输出保存至文件(vee, 4.03Kb)”是一个简单的VEE程序,它把Keysight 8560系列分析仪的HPGL绘图仪输出命令通过GPIB保存至PC机。

FAQ 2011-06-27

能否在长扫描时间配置中,作为单个数据点采集8590或8560系列频谱分析仪曲线数据?
8590系列和8560系列频谱分析仪家族不提供采集单点迹线数据的默认机制(程序命令)8590系列迹线传输由401个数据点组成。

FAQ 2011-06-27

How do I extract information from the 89601A VSA software's Error Summary trace through automation? I want to use a routine in my ActiveX program ...
Different modulation analysis modes feature different COM properties. This link describes the property for each demodulator.

FAQ 2010-11-22

How do I control instruments such as 82357A, E5810A, and 82350B using the GPIB interface?
There are several approaches to control instruments via the GPIB interface...

FAQ 2010-10-04

VEE Pro: Why can't I talk to an instrument at GPIB address 21?
The reason is that each device on the GPIB has to have a unique address, including the computer's GPIB card.

FAQ 2010-09-09

In the ESA Series, how can I save the results of a Channel Power, ACP, OBW, Emission Bandwidth, or Harmonic Distortion measurement?
Save a screen image to the floppy disk drive.

FAQ 2010-06-14

Can I program a waveform captured by my oscilloscope into a Keysight arbitrary waveform generator?
Yes. The free IntuiLink Waveform Editor software will download waveform data from Keysight Infiniium, 6000 series, and 54600 series oscilloscopes and send the data to the a Keysight 33120A, 33210A, 33220A, or 33250A generator.

FAQ 2010-05-14

How do I remotely program my X-Series, ESA, PSA Signal Analyzer to Transfer Trace data using VEE?
The attached program demonstrates how to transfer trace in in several formats including ASCII, REAL and Integer.

FAQ 2009-11-11

How do I remotely program my Keysight X-Series, ESA/PSA Series Signal Analyzer to transfer binary block trace data in Visual Basic 6?
Click here for information on transfering binary block trace data.

FAQ 2009-11-11

1 2 3 下一页