1-12 of 12

Sort:
Overcoming LTE-Advanced Test Challenges - Inter-Band Carrier Aggregation
This video will explain one of the major test challenges of demodulating the multiple component carriers simultaneously since the frequency band separation in inter-band aggregation is wider than the IF BW of any commercially available signal analyzer. Watch how Keysight addresses this test challenge with the 89600 VSA software along with dual X-Series signal analyzers or N7109A multi-channel signal analyzer.

How-To Video 2012-07-15

LTE Digital and Analog Vector Modulation Debug
Watch this video to learn how to debug and validate the vector signal path in an LTE radio. A common analysis environment allows for both digital and analog/RF teams to evaluate the quality of key LTE signals. Both digital and analog signals are processed by the 89600 Vector Signal Analyzer (VSA) software where the constellation diagram, spectral content, and error vector magnitude can be observed and compared to SystemVue simulation results.

Demo 2012-03-27

42 Mbps DC-HSDPA Throughput with the 8960
This video is a demonstration of the new E5515E measuring the maximum 42 Mbps throughput of a DC-HSDPA device in an environment that closely simulates real-world conditions

Demo 2012-03-05

MIMO OTA Two-Stage Method Using PXT and PXB
This video is a demonstration of testing the MIMO OTA performance of an LTE device using the two-stage method with Keysight Technologies' N5106A PXB and E6621A PXT. This method is efficient and cost-effective and can be used for multiple stages of test including design verification testing of antennas or devices on a lab bench. 3GPP and CTIA are currently evaluating this method to be added to LTE conformance testing.

Demo 2012-03-05

MIPI M-PHY Automated Tx Test Demo
Watch a Keysight engineering expert demonstrate the new MIPI transmitter solution that is designed to perform MIPI M-Phy measurements automatically to help save you time. This demo uses a M-Phy Gear2 devices from Cosmic Circuits.

Demo 2012-02-21

Anticipate Multi-Standard Radio (MSR) Performance with Keysight SystemVue
As mobility carriers embrace 4G LTE technology, new equipment must co-exist with older 2G/3G standards. Multi-Standard Radio (MSR) testing characterizes these interactions, and is supported by a variety of Keysight test products. Keysight SystemVue, a system-level modeling environment for communications physical layer, enables R&D engineers to anticipate these interactions, achieve more robust system designs, then connect to Test to validate simulated performance using real hardware.

Demo 2012-02-18

802.11ac System Design and Verification Using the W1917 SystemVue WLAN library
Keysight SystemVue and the W1917 WLAN library are used for communications system design and verification of a 5GHz 802.11ac WLAN physical layer.

Demo 2011-11-18

Demonstration of Handovers between LTE and eHRPD Cells (Inter-RAT)
This video demonstrates how to accelerate time-to-market for LTE UE designs with handovers between LTE and eHRPD Cells (Inter-RAT) using the Keysight E6621 PXT.

Demo 2011-05-02

Demonstration of Simultaneous Video Streaming and VoIP with a 4G LTE USB Modem
Using the Keysight E6621 PXT, this video demonstrates simultaneous video streaming and VoIP with a 4G LTE (LTE-Advanced) USB modem.

Demo 2011-05-02

Demonstration of VoIP with a 4G LTE USB Modem
This video demonstrates the use of the Keysight E6621 PXT Wireless Communications Test Set with VoIP with a 4G LTE (LTE-Advanced) USB modem.

Demo 2011-05-02

Demonstration of Streaming Video to a 4G LTE USB Modem
This video demonstrates streaming video to a 4G LTE (LTE-Advanced) USB modem using a Keysight E6621 PXT.

Demo 2011-05-02

Gain greater confidence in your DigRF designs
This video will demonstrate how the integrated test environment from Keysight Technologies will assist you through the different phases of the development process of both your digital and RF subsystems.

Demo 2011-04-11