Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 44

Sort:
Can I measure VSWR, return loss and DTF with my handheld spectrum analyzer?
Yes, the HSA N9342C handheld spectrum analyzer with option CA7 and TG7 support to read VSWR.

FAQ 2015-03-17

Will the handheld spectrum analyzers have an LXI C class (web server)?
No, there is no plan for an LXI C class (web server).

FAQ 2014-04-07

Can I switch off the U1602A/U1604A Handheld Oscilloscope's audible key sound?
Yes, you have the option to switch on or off the audible key sound of the U1602A/U1604A Handheld Oscilloscope….

FAQ 2013-11-17

Can I save the image of Meter or Logger mode to the internal memory of my U1602A/U1604A Handheld Oscilloscope?
No, you cannot save your Meter or Logger data to the internal memory nor the USB Flash Memory (for option-001) of your U1602A/U1604A....

FAQ 2013-11-17

Can I use a normal USB cable for datalogging with the U1250A Series Handheld Digital Multimeters?
No, you cannot use a normal USB cable for datalogging with the U1250A Series Handheld Digital Multimeters…..

FAQ 2013-11-17

Can I measure temperature with the U1251A/U1252A Handheld Digital Multimeter?
Yes, you can measure temperature with the U1251A and U1252A Handheld Digital Multimeter…

FAQ 2013-11-17

Can I measure duty cycle or pulse width with the U1251A/U1252A Handheld Digital Multimeter?
Yes, you can measure duty cycle or pulse width with the U1251A and U1252A Handheld Digital Multimeter.

FAQ 2013-11-17

Can HyperTerminal be used with the U1251A/U1252A Handheld Digital Multimeter?
No, HyperTerminal cannot be used with the U1251A and U1252A Digital Multimeter….

FAQ 2013-11-17

Can I change the amplitude level for the squarewave output function?
No, you cannot change the amplitude level …

FAQ 2013-11-17

Are the input channels on the U1602A and U1604A Handheld Oscilloscopes isolated?
No, the scope channels 1 and 2 on the U1602A and U1604A Handheld Oscilloscopes are not isolated. They share the same ground.

FAQ 2013-11-17

What are the conditions that will cause the U1270 series handheld multimeter to display Incorrect DC Voltage values at DC measurement mode when signal
The error value may occur if the Filter is not enabled...

FAQ 2013-11-10

Is it possible to modify the scale on the return loss plot when the measurement is configured for Return Loss & DTF on a FieldFox instrument?
There is no method to change the scale on the upper Return Loss (top) plot.

FAQ 2012-08-20

How can I make field strength measurements on my handheld spectrum analyzer?
Each of the HSA products supports field strength measurements.

FAQ 2012-03-02

Are the remote control commands of the handheld spectrum analyzers compatible with any other instrument?
The remote control command set of the handheld spectrum analyzers is compatible with the command sets of other spectrum analyzers.

FAQ 2012-03-02

Do the handheld spectrum analyzers offer a tracking generator?
Yes, all HSA models have a tracking generator option.

FAQ 2012-03-01

What is the Task Planner Trial program?
A program offered by Keysight that allows customers to obtain a 90-day trial license.

FAQ 2012-02-22

How long will a handheld spectrum analyzer powered by battery continuously work?
A battery-powered HSA can continuously work for a minimum of 3 hours.

FAQ 2012-02-20

How do I enable the GPS information on the handheld spectrum analyzer?
The steps to enable GPS on the N9342C, N9343C or N9344C are: Press[Shift] -> [System Mode] -> {More 1 of 2} -> {GPS} -> {GPS on} and {GPS Info on}.

FAQ 2012-02-20

Do the handheld spectrum analyzers have a keystroke recorder?
No, the HSAs do not have a keystroke recorder.

FAQ 2012-02-20

Do the handheld spectrum analyzers have AM/FM demodulation?
Yes

FAQ 2012-02-20

Does the user interface of the handheld spectrum analyzer support multiple languages?
Yes, the user interface for each of the HSA models supports eleven languages.

FAQ 2012-02-20

Is it possible to load built-in cellular frequency channels onto the handheld spectrum analyzer?
Yes, each HSA model allows the user to load standard frequency channels, like GSM or W-CDMA.

FAQ 2012-02-20

Is it possible to operate the power meter option (PWM) remotely using a SCPI command?
No, the power meter option on the HSAs cannot be controlled remotely.

FAQ 2012-02-20

Can the handheld spectrum analyzers be turned on or off remotely?
There is no SCPI command to turn the HSA on or off remotely.

FAQ 2012-02-20

Do the handheld spectrum analyzers have record/playback features in the spectrogram and the spectrum mode? Can the signal be recorded on a USB drive?
Option SIM for the HSAs provides record and playback features in the spectrogram and the spectrum mode.

FAQ 2012-02-20

1 2 Next