Contact an Expert

Technical Support

Electronic Measurement

Find by Product Model Number: Examples: 34401A, E4440A

126-142 of 142

Sort:
What is the relationship between the “No. of Least Significant Digit” and the accuracy of a handheld meter?
The “No. of Least Significant Digit” affects the accuracy of a handheld meter....

FAQ 2010-02-21

What are the differences between the N9340A and N9340B?
Please click the link to see the table showing the differences.

FAQ 2010-01-21

What is the relationship between the “No. of Least Significant Digit” and the accuracy of a handheld multimeter?
The “No. of Least Significant Digit” affects the accuracy of a handheld multimeter....

FAQ 2010-01-07

Are there any programming commands for the U1731A/U1732A Handheld Capacitance and LCR Meter?
No, it only offers datalogging with Keysight U173xA GUI Data Logger Software.

FAQ 2009-10-26

Are there any programming commands for the U1701A Handheld Capacitance Meter?
No, it only offers datalogging with Keysight U1701A GUI Data Logger Software…

FAQ 2009-10-22

What should I consider when charging my U1252A/ U1253A Handheld Digital Multimeter with the DC power adaptor?
Please ensure the following precautions is observed during the charging process ...

FAQ 2009-10-01

How to measure temperature with the AUXILIARY METER function of the U1602A/U1604A handheld Oscilloscope?
The humidity can be measured with U1586A Temperature Adaptor connected to the U1602A/U1604A handheld Oscilloscope

FAQ 2009-09-29

What is the update rate for U1600A series handheld scope?
update rate is 14 waveforms per second

FAQ 2009-08-06

What is the recommended battery type for the U1251A, U1252A and U1253A Handheld Digital Multimeters (DMM)?
The recommended battery type for the U1251A, U1252A and U1253A Handheld Digital Multimeters (DMM) are described on the table below……

FAQ 2009-06-10

How to measure current with the AUXILIARY METER function of the U1602A/U1604A handheld Oscilloscope?
The current can be measured with connect a current adaptor (current probe) to the U1602A/U1604A handheld Oscilloscope...

FAQ 2009-06-10

What does option 001 for the U1602A and U1604A Handheld Oscilloscopes consist of?
A U1602A or U1604A Handheld Oscilloscope with option 001 will have a USB 2.0 host port….

FAQ 2009-05-03

Will the "Auto Power Off" function work when the U1602A/U1604A Handheld Oscilloscope is connected to the AC adaptor?
No, the "Auto Power Off" function only works when the U1602A/U1604A Handheld Oscilloscope is operating with the battery pack....

FAQ 2009-05-03

What type of USB cable do the U1602A and U1604A Handheld Oscilloscopes use?
The U1602A and U1604A Handheld Oscilloscopes use the USB type-A to mini-B cable….

FAQ 2009-05-03

How do I download my preferred Quick Help language for my U1602A/U1604A Handheld Oscilloscope?
Download your preferred Quick Help language for the U1602A and U1604A Handheld Oscilloscope from the Product Reference CD……

FAQ 2009-05-03

Must I charge up my new U1602A/U1604A Handheld Oscilloscope before putting it to use for the first time?
Yes, you must fully charge your new U1602A/U1604A Handheld Oscilloscope for approximately 25 hours....

FAQ 2009-05-03

What is the length of the thermocouple cable for the U1186A Thermocouple (K-type) and Temperature Adapter?
The length of the K-type thermocouple bead is approximately 1m....

FAQ 2009-01-12

Why is the battery life of the U1253A Handheld Digital Multimeter (DMM) typically shorter than the battery life of the U1251A/U1252A?
The battery life of the U1253A Handheld Digital Multimeter (DMM) is typically shorter because its display brightness is set to the highest….

FAQ 2008-10-09

Previous 1 2 3 4 5 6