이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-25 / 101

정렬방식:
SD 카드에 얼마나 많은 이미지를 저장할 수 있습니까?
그것은 IR 과 실제 이미지를 저장하거나 실제이미지만 저장하거나에 따라서 달라집니다.

FAQ 2016-04-25

Can I save the image file into different format?
No.

FAQ 2015-11-21

Can I control my thermal imager through the software?
No.

FAQ 2015-11-21

Do U5855A, U5856A and U5857A have video recording capability?
No.

FAQ 2015-11-21

Do U5855A, U5856A and U5857A have wifi capability?
No.

FAQ 2015-11-21

트리거된 로깅 데이터를 GUI DATA LOGGER로 전송할 수 있나요?
아니요

FAQ 2015-04-22

저의 핸드형 스펙트럼 분석기로 VSWR, 반사 손실, DTF를 측정할 수 있습니까?
그렇습니다, 옵션 CA7과 TG7 지원이 추가된 HSA N9342C 핸드형 스펙트럼 분석기만 있다면 VSWR을 판독할 수 있습니다.

FAQ 2015-03-17

N9342C 스펙트럼 분석기(HSA)를 어떻게 업그레이드합니까?
N9342C 핸드형 스펙트럼 분석기 업그레이드

FAQ 2013-11-20

Do the U1251A and U1252A Digital Multimeters come with connectivity cables?
No, the U1251A and U1252A Digital Multimeters do not come with connectivity cables. The cable is an optional accessory…..

FAQ 2013-11-17

Can I change the amplitude level for the squarewave output function?
No, you cannot change the amplitude level …

FAQ 2013-11-17

Can I measure duty cycle or pulse width with the U1251A/U1252A Handheld Digital Multimeter?
Yes, you can measure duty cycle or pulse width with the U1251A and U1252A Handheld Digital Multimeter.

FAQ 2013-11-17

Can I upgrade to option 001(Host USB interface) for the U1600A Series Handheld Oscilloscopes after purchase?
No, you cannot upgrade to option 001 for the U1600A Series Handheld Oscilloscopes after purchase….

FAQ 2013-11-17

Can HyperTerminal be used with the U1251A/U1252A Handheld Digital Multimeter?
No, HyperTerminal cannot be used with the U1251A and U1252A Digital Multimeter….

FAQ 2013-11-17

Can I use a normal USB cable for datalogging with the U1250A Series Handheld Digital Multimeters?
No, you cannot use a normal USB cable for datalogging with the U1250A Series Handheld Digital Multimeters…..

FAQ 2013-11-17

Are the input channels on the U1602A and U1604A Handheld Oscilloscopes isolated?
No, the scope channels 1 and 2 on the U1602A and U1604A Handheld Oscilloscopes are not isolated. They share the same ground.

FAQ 2013-11-17

Can I use the test probe leads marked with CAT III 1000V rating come together with the U1241A/U1242A/U1251A/U1252A/U1253A handheld Multimeter…
The test lead kit which currently marked with CAT III 1000V rating can be used with the multimeter at CAT IV 600V measurement environment...

FAQ 2013-11-17

Can I export the interval logging data saved in the internal memory of my U1253A Handheld Multimeter?
Yes, you can export the interval logging data saved by upgrade your U1253A Firmware revision to V1.20…..

FAQ 2013-11-17

Can I save the image of Meter or Logger mode to the internal memory of my U1602A/U1604A Handheld Oscilloscope?
No, you cannot save your Meter or Logger data to the internal memory nor the USB Flash Memory (for option-001) of your U1602A/U1604A....

FAQ 2013-11-17

Can I export the data saved in the U1602A/U1604A Handheld Oscilloscope's internal memory to my PC?
No, you cannot export the data saved in the U1602A/U1604A Handheld Oscilloscope's internal memory to your PC....

FAQ 2013-11-17

Are there any calibration options available for the U1251A/U1252A Handheld Digital Multimeter?
Yes, there are a variety of calibration options available for the U1251A and U1252A Handheld Digital Multimeter…

FAQ 2013-11-17

What are the conditions that will cause the U1270 series handheld multimeter to display Incorrect DC Voltage values at DC measurement mode when signal
The error value may occur if the Filter is not enabled...

FAQ 2013-11-10

핸드형 스펙트럼분석기 peak table은 얼마나 많은 peak점을 보여줄 수 있나요?
N9342C, N9343C 그리고 N9344C에서...

FAQ 2013-10-10

How do I upgrade my N9343C Handheld Spectrum Analyzer?
Find Information on Hardware Upgrades, Instrument Software, Measurement Applications, etc...

FAQ 2012-12-17

How do I upgrade my N9344C Handheld Spectrum Analyzer?
Find Information on Hardware Upgrades, Instrument Software, Measurement Applications, etc…

FAQ 2012-12-17

왜 U1253B의 Battery수명이 U1251B/U1252B 보다 짧나요?
U1253B의 Battery 수명은 U1251B/U1252B보나 짧습니다.

FAQ 2012-10-31

1 2 3 4 5 다음