Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

51-75 of 102

Sort:
How do I enable the GPS information on the handheld spectrum analyzer?
The steps to enable GPS on the N9342C, N9343C or N9344C are: Press[Shift] -> [System Mode] -> {More 1 of 2} -> {GPS} -> {GPS on} and {GPS Info on}.

FAQ 2012-02-20

Do the handheld spectrum analyzers have record/playback features in the spectrogram and the spectrum mode? Can the signal be recorded on a USB drive?
Option SIM for the HSAs provides record and playback features in the spectrogram and the spectrum mode.

FAQ 2012-02-20

What is the size of the internal user memory on the handheld spectrum analyzer? How many trace files or pictures can be saved?
The internal user memory of the HSA holds up to 60 MB.

FAQ 2012-02-20

Do the handheld spectrum analyzers have a fan or vent?
No, the HSAs have design that is fanless and has no vent.

FAQ 2012-02-20

What is the operating system used by the handheld spectrum analyzers?
The HSAs use the VxWorks operating system.

FAQ 2012-02-20

How long will a handheld spectrum analyzer powered by battery continuously work?
A battery-powered HSA can continuously work for a minimum of 3 hours.

FAQ 2012-02-20

Do the handheld spectrum analyzers provide a continuous waveform generator option?
No, the HSAs do not have a CW (continuous waveform) generator function.

FAQ 2012-02-20

How many peaks can be displayed in the handheld spectrum analyzer’s peak table?
On the N9342C, N9343C and N9344C, there may be 10 peaks.

FAQ 2011-11-07

Does Keysight U1271A/U1272A Handheld Digital Multimeter comes with a power adapter?
No, U1271A/U1272A is powered by four 1.5V AAA alkaline batteries.

FAQ 2011-05-05

Can event (trigger) logged data be transferred to the GUI DATA LOGGER?
No, data can only be transferred for manual logged data and interval logged data.

FAQ 2011-05-05

Under the unit function’s ACV and DCV, the display rate of U1271/2A indicates 7 times per second, can GUI DATA LOGGER capture all 7 readings?
No, the GUI DATA LOGGER is running on different acquisition method than the unit’s display rate, therefore the fastest update rate is 1 sample per second.

FAQ 2011-05-05

When I press the Power On button on my U1602A/U1604A Handheld Oscilloscope, it does not boot up. Instead, the screen just flashes …
To turn on your U1602A/U1604A Handheld Oscilloscope, you will need to press and hold the Power On button for approximately 3 seconds….

FAQ 2010-08-09

When using the U1602A/U1604A Handheld Oscilloscope, I can see an offset value at the vertical axis although there is no connection…
When you see an offset value at the vertical axis although there is no connection at the test probe, try running the self-calibration….

FAQ 2010-08-09

Why am I getting a reading instead of zero when using U1252A/U1253A frequency counter measurement function although no measurement was done…
After the probes are connected to the U1252A/U1253A, the measured value will be automatically zeroed.

FAQ 2010-08-09

Why does the pulse shape of my scope probe compensation look different from the pulse shape shown…
The compensation signal (square wave) that you see is different from the pulse shape shown in the U1602A/U1604A's user’s manual because….

FAQ 2010-08-09

Can I measure coil resistance with the U1241B/U1242B Handheld Digital Multimeter (DMM)?
Yes, you can measure coil resistance with the U1241B/U1242B Handheld Digital Multimeter (DMM)

FAQ 2010-08-08

Can I measure AC voltage with the U1241B/U1242B Handheld Digital Multimeter (DMM) if there is a DC offset?
Yes, you can measure AC voltage with the U1241B/U1242B Handheld Digital Multimeter (DMM), even if there is a DC offset

FAQ 2010-08-08

Why does the new U1571A battery pack for my U1602/4A Handheld Oscilloscope last less than the stipulated 4 hours…
The new U1571A battery pack of the U1602A or U1604A Handheld Oscilloscope lasts less than 4 hours because….

FAQ 2010-08-08

Can I control the beeper sound volume for the audible continuity measurement?
No, you can't….

FAQ 2010-07-18

What is the different between Frequency Function and Frequency Counter Function at U1252B/U1253B Series handheld Digital Multimeter?
The Frequency function measures up to 600kHz 1000V … Frequency Counter function measures upto 20 MHz at <30Vpp…

FAQ 2010-05-10

Can I perform measurement with my U1252A/U1253A Handheld Multimeter while charging the unit?
No, U1252A/U1253A Handheld Multimeter does not allow to perform measurement while charging…

FAQ 2010-05-05

How to check the condition of the fuses in U1253A/U1253B before you use it?
To test the fuses inside the U1253A/U1253B OLED display DMM, just follow the instructions as follows…

FAQ 2010-03-22

Can I program to control U1401B?
No...

FAQ 2010-03-22

What should I consider when charging my U1252B/U1253B Handheld Digital Multimeter with the DC power adaptor?
Please ensure the following precautions is observed during the charging process ...

FAQ 2010-02-23

What is the recommended battery type for the U1251B, U1252B and U1253B Handheld Digital Multimeters (DMM)?
The recommended battery type for the U1251B, U1252B and U1253B Handheld Digital Multimeters (DMM) are described on the table below……

FAQ 2010-02-21

Previous 1 2 3 4 5 Next