이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

76-100 / 407

정렬방식:
How can I input 28V digital signal to U2651A/U2652A when it support digital input voltage < 24V?
You can connect a voltage divider in front of the digital input to reduce the voltage to <24V

FAQ 2010-10-07

What drivers will be provided with modular products?
IVI-COM, IVI-C and LabVIEW (G), are provided with all Keysight modular products...

FAQ 2010-10-06

Can I run a program that is controlling my PXI instrument while using its soft front panel (SFP)?
Not at this time...

FAQ 2010-10-06

Can I use SCPI to communicate with my Keysight modules?
No. Connectivity is provided through Drivers.

FAQ 2010-10-06

Where can customers download instrument drivers? (LabVIEW, Visual-studio.net,…)
The instrument drivers are provided with each instrument on a CD...

FAQ 2010-10-06

How do I find a partner to help develop my modular solution?
Keysight has a number of solution partners that can help define and create your modular solution...

FAQ 2010-10-06

What is the compatibility between PXIe chassis and Keysight new PXI/PXIe modules?
Keysight modules come in several varieties, so inspection is required to determine compatibility...

FAQ 2010-10-06

Does Keysight have mass interconnect solutions?
There are mass interconnect solutions from MAC panel....

FAQ 2010-10-06

Will ExpressVIs work with Keysight hardware?
No. Keysight has VIs available to use with LabView but not ExpressVIs.

FAQ 2010-10-06

Where can customers find user manuals and example programs for AXIe & PXIe products?
Datasheets of modular products will be included on the CD shipped with every product and will be available on Keysight.com from the product page...

FAQ 2010-10-06

Can I use PXI-1 existing cards in the Keysight Card cages and are there any that will no longer work?
Older PXI (PXI-1) modules (which have a J2 present) will not work in Keysight 18-slot PXIe chassis...

FAQ 2010-10-06

What is the difference between PXIe and AXIe?
The AXIe standard provides the maximum scalability to address a range of platforms...

FAQ 2010-10-06

Can I replace other vendors' module (for example a digitizer) with a Keysight one?
There are two aspects to consider...

FAQ 2010-10-06

GPIB 인터페이스를 이용해서, 82357A, E5810A 및 82350B 등의 계측기를 제어하는 방법이 궁금합니까?
GPIB 인터페이스를 통해 계측기를 제어하는 데는 몇 가지 방식이 있습니다.

FAQ 2010-10-04

Transferring the license from an older version to version 3.00
Before updating to a new revision of Data Logger on the SAME computer, be certain to save all data and configuration files that you wish to keep.

FAQ 2010-09-19

34980A 메인프레임의 일련 번호는 어디에 있습니까?
일련 번호는 34980A 후면 패널의 LAN 및 USB 커넥터 왼쪽에 있습니다.

FAQ 2010-09-15

BenchLink는 키사이트 3499A/B/C를 지원합니까?
BenchLink는 3499A/B/C를 지원하지 않는 제품별 소프트웨어입니다.

FAQ 2010-09-15

Can I retrieve data from the 34970A while it is scanning?
No. You can collect data during a scan, stop the scan and then transfer the data.

FAQ 2010-09-09

VEE : 왜 GPIB Address가 21번으로 설정된 장비와 통신할 수 없습니까?

FAQ 2010-09-09

IO Libraries Suite: What are the differences between Keysight IO Libraries Suite versions 14.0 and 14.1?
The major enhancement that has been added to version 14.1 is compatibility with National Instruments NI-488.2 API or I/O Library.

FAQ 2010-09-08

How can I copy Channels to Other Channels in BenchLink 3?
Select the channel(s) to be copied, right-click and select copy, select the channel(s) to be pasted, right click and select paste.

FAQ 2010-09-08

BenchLink 3에서 "Object reference not set to an instance of an object" 오류가 발생하는 이유는?
이 오류는 .NET Framework의 손상으로 인해 발생합니다.

FAQ 2010-09-08

Where can I get the Programming Guide for the U2300A Series USB Data Acquisition (DAQ) devices?
You can download the Programming Guide for the U2300A Series USB Data Acquisition (DAQ) devices from the Product Reference CD….

FAQ 2010-09-08

A Windows® Logo warning message appears during the U2300A Series driver installation. What does this mean?
The Windows® Logo warning message appears if the U2300A Series driver does not have Microsoft® Windows® Logo certification...

FAQ 2010-09-08

NI GPIB 카드와 키사이트 GPIB 카드 및 컨버터는 같은 시스템에서 작동 가능 합니까? 같이 작동하기 위해서는 어떤 구성이 필요한가요?
예. 원하는 셋업에 따라 VISA나 Keysight 488 설정을 구성해야 할 수도 있습니다.

FAQ 2010-09-08

이전 1 2 3 4 5 6 7 8 9 10 ... 다음