Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 29

Sort:
Multi-channel signals with the Keysight E1440A
The attached Application Note is an example describing the test of vehicle receivers used in Decca-type location systems that require a number of synthesizers to simulate the signals from a number of fixed transmitters. The frequencies, which are multiples of the master transmitter frequency...

Application Note 2004-02-20

PDF PDF 17 KB
IO Libraries support of IEEE 1394 CardBus/PCMCIA Cards
Windows 98 SE/Me/2000/XP have built-in support for IEEE 1394, enabling us to support several IEEE 1394 CardBus/PCMCIA Cards.

Application Note 2002-09-11

Understanding FireWire
New Serial Interface Promises Easier, Faster, and Cheaper Instrument Control Scaleable, flexible, and plug-and-play, FireWire (aka IEEE specification 1394.1995) is an ideal interface to connect...

Application Note 2002-06-27

VXI System Helps IC Package Company Test ICs
In recent years IC density have been increasing. Read how VXI Systems can help solve these test issues.

Application Note 2001-12-20

I/O Libraries Supported Interfaces - Application Note
IO Library

Application Note 2001-12-12

Functional Test & Data Acquisition I/O Benchmarks
The following benchmarks compare computer I/O performance in functional test and data acquisition applications.

Application Note 2001-12-04

VXI-Based Test Station Reduces Development Cost and Cycle Time
This article describes a system called the Hellfire II Common Core Test Station which can be used for both military and commerical uses.

Application Note 2001-04-13

VXI I/O Using the IEEE 1394 Serial Bus (FireWire)
FireWire, IEEE 1394, IEC 1883. These titles refer to a high-speed serial bus that is literally a new standard for transmitting data between PCs and consumer electronics.

Application Note 2001-04-13

Firewire for VXIbus, The Keysight E8491B
IEEE 488, known also as HP-IB or GPIB, started out as one of the first ways to connect a computer to external instrumentation.

Application Note 2001-04-10

Using VXI to Reduce Test-System Size and Cost
describes how how VXI hardware and updated software can simplify the redesign of older test systems

Application Note 2001-04-10

Design Verification for Mobile Phones
A European manufacturer of mobile phones is using HP VEE to dial-up higher profits and greater market share.

Application Note 2001-04-09

Increasing Test System Throughput with IEEE 1394: Keysight E8491B
The Measure of a System No matter how sophisticated or complete a test system, the ultimate measure of its worth is the rate at which it can turn out tested (good) products - in a word, throughput. Throughput is affected by a variety of factors, important among which is the choice of slot...

Application Note 2000-04-01

PDF PDF 478 KB
Canning Process Characterization
Following the description of the canning process application, measurement and control requirements for characterizing the process are discussed, then in this Application Note, Keysight data acquisition equipment suitable for such an application is listed. Description In the canning industry...

Application Note 1997-11-01

PDF PDF 94 KB
Pharmaceutical Process Control
In this Application Note following the description of the pharmaceutical process control, application measurement and control requirements for characterizing the process are discussed. Then, Keysight VXI-Based data acquisition equipment suitable for such an application is listed. Description...

Application Note 1997-11-01

PDF PDF 113 KB
Environmental/Autoclave Testing
In this Application Note following the description of the environmental/autoclave testing application, measurement and control requirements for characterizing the process are discussed. Then, Keysight VXI-based data acquisition equipment suitable for such an application is listed. Description...

Application Note 1997-11-01

PDF PDF 92 KB
Pilot Plant Monitoring
In this Application Note following the description of the pilot plant monitoring application, measurement and control requirements for characterizing the process are discussed. Then, Keysight VXI-based data acquisition equipment suitable for such an application is listed. Description Pilot plants...

Application Note 1997-11-01

PDF PDF 120 KB
Rolling Mill
In this Application Note following the description of the rolling mill application, measurement and control requirements for characterizing the process are discussed. Then, Keysight VXI-based data acquisition suitable for such an application is listed. Description Steel, aluminum, fiberglass...

Application Note 1997-11-01

PDF PDF 82 KB
Facility Management
In this Application Note following the description of the facility management application, measurement and control requirements for characterizing the process are discussed. Then, Keysight VXI-based data acquisition equipment suitable for such an application is listed. Description Large...

Application Note 1997-11-01

PDF PDF 121 KB
Appliance Testing
In this Application Note following the description of the appliance testing application, measurement and control requirements for characterizing devices are discussed. Then, Keysight VXI-based data acquisition suitable for such an application is listed. Description Household and commercial...

Application Note 1997-11-01

PDF PDF 110 KB
Wastewater Treatment
In this Application Note following the description of the wastewater treatment application, measurement and control requirements for characterizing the process are discussed. Then, Keysight VXI-based data acquisition equipment suitable for such an application is listed. Description...

Application Note 1997-11-01

PDF PDF 104 KB
Commercial Energy Conservation
In this Application Note following the description of the commercial energy conservation application measurement and control requirements for characterizing the process are discussed. Then, Keysight VXI-based data acquisition equipment suitable for such an application is listed. Description...

Application Note 1997-11-01

PDF PDF 106 KB
Pumping Station Control
In this Application Note following the description of the pumping station control application, measurement and control requirements for characterizing the process are discussed. Then, Keysight VXI-based data acquisition equipment suitable for such an application is listed. Description...

Application Note 1997-11-01

PDF PDF 110 KB
Parallel Cell/Traffic Generator and Analyzer System: Keysight E4829B and E4821A
The Keysight E4829B Parallel Cell/Traffic Generator and Analyzer System is used in research and development to verify the correct functional operation and performance of ATM designs from parallel interfaces. See the attached Product Overview for more information.

Application Note 1996-08-01

PDF PDF 103 KB
Environmental Test of Automotive Radio and Engine Controllers (AN 1270-11)
Automotive components such as radios and engine controllers are tested to environmental limits using HP Automatic Test Systems to control the environmental chamber and test the components therein. See Application Note 1270-11 attached to this page for more information.

Application Note 1995-06-01

PDF PDF 108 KB
Vehicle Body Testing (AN 1270-5)
Application Note 1270-5 describes how an HP System submits a vehicle to a variey of test track stress conditions and measures the resulting performance on material fatigue and stress.

Application Note 1995-06-01

PDF PDF 44 KB

1 2 Next