1-25 of 166

Sort:
MATLAB IQtools
Example MATLAB IQtools scripts to generate multi-tone signals, pulsed radar signals and multi-carrier modulated waveforms using AWG - standalone or in conjunction with a Vector PSG.

Programming Example 2016-11-28

I/O Libraries Example Programs
Examples to get you started with instrument programming...

Programming Example 2016-10-19

MIMO Config Utility 1.1.6.msi
This utility assists new users in making their first measurements when using the M9381A PXIe VSG and M9391A PXIe VSA in a MIMO environment.

Programming Example 2014-05-15

FILE FILE 737 KB
MIMO Demo Tool Install 1.2.1.msi
This demo tool provides the capability to generate multi-channel waveforms from the M9381A PXIe VSG, including waveforms and sequences of waveforms for WLAN, LTE MIMO, and Carrier Aggregation signals. This demo tool includes source code and a programming guide that can be leveraged when writing your own test code.

Programming Example 2014-05-15

FILE FILE 128.52 MB
Keysight 34970A Example Programs
More than 100 examples and programming questions for 34970A data acquisition/switch unit.

Programming Example 2013-01-17

M9392A Multichannel Streaming Example Program
Sample program, created using Microsoft Visual Studio C#, allows you to begin making multichannel streaming measurements immediately. The source code shows which IVI COM command sequences are required and which test techniques are recommended. The solution can be built on a 32-bit operating system (OS); however, a 64-bit OS is recommended. For details about the program, read the included MCStreamingHelp.pdf file.

Programming Example 2012-04-26

ZIP ZIP 806 KB
M9392A Example Programs
Example programs for the M9392A PXI Vector Signal Analyzer. These programs are also provided in the general software installer. Includes sample programs in Visual Studio.net, LabVIEW, MATLAB, LabWindows, and Keysight VEE Pro.

Programming Example 2011-05-19

ZIP ZIP 530 KB
MATLAB Programming Example for U2500A USB Modular Data Acquisition module’s Analog Input
The document shows how a user can set the USB Data Acquisition module to sample immediately without waiting for a trigger signal.

Programming Example 2010-04-12

TXT TXT 1 KB
MATLAB Programming Example for U2300A USB Modular Data Acquisition module’s Analog Input
The document shows how a user can set the USB Data Acquisition module to sample immediately without waiting for a trigger signal.

Programming Example 2010-04-12

TXT TXT 1 KB
34980A Programmer's Reference Version 1.2

Programming Example 2010-02-17

ZIP ZIP 4.54 MB
34970A/34972A LabView Programming Examples

Programming Example 2010-01-29

34970A/34972A VEE Programming Examples

Programming Example 2010-01-29

34970A/34972A C/C++ Programming Examples

Programming Example 2010-01-29

34970A/34972A VB.NET Programming Examples

Programming Example 2010-01-29

34970A/34972A Code Wizard Programming Examples

Programming Example 2010-01-29

34970A/34972A C# Programming Examples

Programming Example 2010-01-29

34970A/34972A VB 6.0 Programming Examples

Programming Example 2010-01-29

34970A Excel Programming Examples

Programming Example 2010-01-29

MATLAB Programming Example for U2300A Modular USB Data Acquisition module’s Analog Output
This program sets the USB Data Acquisition module to output a continuous sine wave.

Programming Example 2009-11-18

ZIP ZIP 1 KB
USB DAQ Audio VEE Sample Software
A programming example to show how the USB DAQ can be used to make audio measurements.

Programming Example 2009-09-03

ZIP ZIP 202 KB
Sample Program for Binary Data Conversion
This sample program will help you convert the binary data (*.bin file) extracted from USB modular oscilloscope, to actual amplitude values.

Programming Example 2009-07-27

ZIP ZIP 5 KB
MATLAB Programming Example for U2500A USB Modular Data Acquisition module’s Analog Output
This program sets the module to send out discrete values out of the analog output and the analog input will be used to measure the value.

Programming Example 2009-04-29

ZIP ZIP 1 KB
MATLAB Programming Example for U2500A USB Modular Data Acquisition module’s Digital IO
This program sets the USB Data Acquisition module’s first 8 Digital IO ports to be digital outputs.

Programming Example 2009-04-29

ZIP ZIP 1 KB
MATLAB Programming Example for U2600A USB Modular Digital IO module
The U2651A module is slotted into the U2781A USB Chassis. This program sets all the ports as digital inputs and trigger type initially as “Star Trigger” followed by “No trigger” and captures the digital input values.

Programming Example 2009-04-29

ZIP ZIP 1 KB
MATLAB Programming Example for U2300A USB Modular Data Acquisition module’s Digital IO
This program sets the USB Data Acquisition module’s first 16 Digital IO ports to be digital inputs.

Programming Example 2009-04-29

ZIP ZIP 1 KB

1 2 3 4 5 6 7 Next