Here’s the page we think you wanted. See search results instead:

 

Parla con un Esperto

Technical Support

Electronic Measurement

Support by Product Model Number:

226-250 of 651

Sort:
What is the clock rate for Digital Inputs(DI) and Digital Outputs(DO) of U23xxA and U25xxA USB Data Acquisition?
The DAQ DIO is not meant to measure DI with clock rate precision or to control frequency of digital output

FAQ 2010-07-18

Why do I get verification error upon reset with single channel pulsed switches and Y1151A distribution board?
On this particular distribution board...

FAQ 2010-06-30

Keysight 34970A FAQ archive
More than 100 FAQs regarding the 34970A data acquisition/switch unit

FAQ 2010-06-07

How can I remotely view what modules are installed in the 34970A?
Use the SYSTem:CTYPe? {100|200|300} SCPI command or System.CardType( ) IVI COM object.

FAQ 2010-05-16

What is the temperature coefficient supported by the 34970A for RTD temperature measurements?
The 34970A supports PT100 RTD's with an alpha=0.00385, RTD's with alpha=0.00385, or alpha=0.00391.

FAQ 2010-05-16

Can the measurements taken be read from the 34980 Data Acquisition Front Panel?
No

FAQ 2010-05-14

Is number of bits the only factor to look at if I'm measuring at very low voltage say 5mVpp?
No it is not. Often times, you will have to look at the Gain Error and Offset Error as well as...

FAQ 2010-05-10

No Title
Instead of the ("Counter value"/"48 x 10^6") as the duration in seconds taken to count, it is...

FAQ 2010-05-10

Transferring Data and Configurations to a new version or to a new computer
Moving between computers with same version or moving configurations and data to a new version on the same computer...

FAQ 2010-05-07

Can I run two scan lists at the same time (in parallel)?
No. Scan lists can only be run sequentially

FAQ 2010-05-05

Can I send an email following a scan or on some event?
Yes. You can use a notification to execute an external program or batch file in response to an event.

FAQ 2010-05-05

Can I set a limit on multiple channels?
Yes. After configuring more than one channel limit on the “Configure Scan Lists” tab, you can configure the On Multiple Channel Limits event on the “Configure Events” tab.

FAQ 2010-05-05

Is there a pictorial or tabular representation available for my scan lists, events, Action Scripts, and notifications?
Yes.

FAQ 2010-05-05

What is an Action Script and what can I do with it?
An Action Script contains one or more action steps that perform actions on modules in 34970A/34980A instruments, and other instrumentation connected to the PC.

FAQ 2010-05-05

How are multiple scan lists graphed?
The starting point for each scan list is indicated by a vertical bar on the graph and the label Started.

FAQ 2010-05-05

Can I start a scan and then close Data Logger Pro and continue scanning?
Yes. However, there are some limitations.

FAQ 2010-05-05

Where can I export the data?
You can save data to files on any disk drive or storage media connected to your PC.

FAQ 2010-05-05

What are channel limits?
Limits can be set on multiplexer, totalizer and digital read channels (see the limit types question below).

FAQ 2010-05-05

What is the Base scan list?
The default scan list is named Scan List A and is the Base scan list.

FAQ 2010-05-05

How can I get started using multiple scan lists?
Please refer to the “Getting Started with Multiple Scan Lists, Limits, Events and Action Scripts” in the Help menu.

FAQ 2010-05-05

How can I update the 34980A to Firmware Revision 2.19?

FAQ 2010-05-05

How can I Locate Exported Data on the Hard Disk?
You can control where files are stored using either the automatic or manual methods discussed above.

FAQ 2010-05-05

How do multiple instruments affect the scan list?
Multiple instruments are integrated seamlessly into a scan list.

FAQ 2010-05-05

How do I control instruments using SCPI commands?
You can use Action Scripts and SCPI commands to control any instrument connected to the PC.

FAQ 2010-05-05

Can I export data while scans are running?
Yes, select Automatically export to .csv during scan in the “Export Data Preferences” dialog box.

FAQ 2010-05-05

Previous 1 2 3 4 5 6 7 8 9 10 ... Next