이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-25 / 635

정렬방식:
What is the current rating of the Y113xA cables?
The Y1135A and Y1136A cables are 50 conductor, 24 AWG cables with 25 shielded twisted pairs with PVC insulation. They can be used with the 34921A, 23A, 25A, 31A, 32A, 33A, 37A, 38A, 51A, and 52A plug-in modules for the 34980A. However, they do not support the full rated total current of the 34937A and 34938A. The Y1137A and Y1138A cables are 78 conductor cables 28 AWG conductors with 39 shielded twisted pairs. They can be used with the 34922A, 24A, 34A, 39A, and 34950A plug-in modules.

FAQ 2016-12-13

AXIe 모듈과 컨트롤러 사이에 빈 슬롯이 있을 때 AXIe 모듈을 표시하려면 어떻게 해야 합니까?
M9537A 컨트롤러와 AXIe 모듈 사이의 슬롯이 비어 있으면 AXIe 모듈을 사용할 수 없게 되고 Windows Device Manager에 에러 메시지가 표시됩니다. 이 문제를 해결하는 방법은 아래와 같습니다.

FAQ 2016-11-21

DisplayPort 핫 스왑 기능은 어떻게 설정합니까?
M9537A는 부팅할 때 활성화되는 3개의 DisplayPort가 있습니다. 하나의 DisplayPort에서 다른 DisplayPort로 케이블을 이동시키는 경우 새 구성을 활성화하려면 재부팅이 필요합니다.

FAQ 2016-11-21

M9537A에 대한 기계 도해는 어디에서 다운로드할 수 있습니까?
파일을 모델링 어플리케이션으로 가져올 수 있습니다.

FAQ 2016-11-21

M9019A에 대한 기계 도해는 어디에서 다운로드할 수 있습니까?
파일을 모델링 어플리케이션으로 가져올 수 있습니다.

FAQ 2016-11-21

M9502A에 대한 기계 도해는 어디에서 다운로드할 수 있습니까?
파일을 모델링 어플리케이션으로 가져올 수 있습니다.

FAQ 2016-11-16

34972A may freeze when LAN connection is under control after power-up
Yes. The first thing to remember is that the 34972A freeze because the user is trying to communicate with the instrument right after power-up. During that time, the instrument is not yet in ready mode. To prevent the problem, please set a delay (approximately 20s or more time until the instrument boot up completely) after power-up before attempting the LAN communication.

FAQ 2016-11-01

IO Libraries Suite: What is the latest version of the IO Libraries Suite?
IO Libraries Suite 17.3, available online.

FAQ 2016-10-26

IO Libraries Suite: What has changed in IO Libraries Suite 17.0, 17.1, 17.2, 17.2 Update 1, 17.2 Update 2, 17.3?
Keysight IO Libraries Suite 17 marks a significant update in the architecture of the IO Libraries Suite infrastructure, as well as an all-new Connection Expert...

FAQ 2016-10-26

34972A with USB data logging may eventually freeze. How to prevent?
Yes, experience has shown that using a powered USB 2.0 Hub between the 34972A and the PC usually eliminates the problem.Using LAN instead of USB is the recommended solution if possible.

FAQ 2016-10-26

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2016-10-21

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2016-10-21

How do I create a Mono FM Signal using N5182B MXG ARB?
You can configure N7611B Signal Studio Broadcast Radio to play a mono/FM signal.

FAQ 2016-10-21

How many carriers can the MXG support in Carrier Aggregation mode?
One MXG can support one instance of the Carrier Aggregation mode. One instance of the Carrier Aggregation mode supports 5 component carriers.

FAQ 2016-10-11

How do I fix: unable to change GPIB settings on an M9037A or M9537A Embedded Controller?
Make the following changes...

FAQ 2016-08-27

All M9300A Frequency Reference Instrument Drivers
Supported models: M9300A

FAQ 2016-08-02

What termination model (Balanced vs. Unbalanced) should I use for my M8000 BERT?
For M8000 (M8041A/51A/61A/62A) BERT data outputs, a Termination Model must be selected in the Amplifier section of the Parameters window, Balanced or Unbalanced.

FAQ 2016-07-08

Can the U4431A MIPI M-PHY protocol analyzer be controlled from an external PC via the AXIe mainframe's USB port?
Yes, the USB connected chassis option (M9502A-U20/M9505A-U20) is a viable connection strategy when using the U4431A M-PHY Protocol Analyzer instrument.

FAQ 2016-07-08

Does the L449XA have USB? What interfaces are built in?
LAN and GPIB are included. The 82357B USB/GPIB converter is available if you require USB.

FAQ 2016-07-05

Does the M9290A CXA-m PXIe signal analyzer offer a tracking generator?
Yes, M9290A CXA-m has optional tracking generator function. Order option T03/T07/T13/T26 according to the frequency range.

FAQ 2016-07-05

Signal Analyzer IVI and MATLAB Instrument Drivers
Supported models: N9000A, N9010A, N9020A, N9030A, N9038A, E4406A, E4440A, E4443A, E4445A, E4446A, E4448A, N8201A, E4447A, E4401B, E4402B, E4403B, E4404B, E4405B, E4407B, E4408B, E4411B, E7401A, E7402A, E7403A, E7404A, E7405A, M9290A, N9040B, N9038A, M9420A, N9000B, N9010B, N9020B, N9030B, N9040B, M9290A, M9420A, M9421A, SPN9026A, SPN9003A

FAQ 2016-07-02

Y1226A에 대한 기계 도해는 어디에서 다운로드할 수 있습니까?
파일을 모델링 어플리케이션으로 가져올 수 있습니다.

FAQ 2016-05-31

Y1234A에 대한 기계 도해는 어디에서 다운로드할 수 있습니까?
파일을 모델링 어플리케이션으로 가져올 수 있습니다.

FAQ 2016-05-31

Y1221A에 대한 기계 도해는 어디에서 다운로드할 수 있습니까?
파일을 모델링 어플리케이션으로 가져올 수 있습니다.

FAQ 2016-05-31

M9505A에 대한 기계 도해는 어디에서 다운로드할 수 있습니까?
파일을 모델링 어플리케이션으로 가져올 수 있습니다.

FAQ 2016-05-31

1 2 3 4 5 6 7 8 9 10 ... 다음