Contact an Expert

Technical Support

Spectrum Analyzers (Signal Analyzers)

Find by Product Model Number: Examples: 34401A, E4440A

Refine the List

remove all refinements

By Topic

By Type of Content

By Product Category

1-15 of 15

Sort:
Can I measure VSWR, return loss and DTF with my handheld spectrum analyzer?
Yes, the HSA N9342C handheld spectrum analyzer with option CA7 and TG7 support to read VSWR.

FAQ 2015-03-17

Will the handheld spectrum analyzers have an LXI C class (web server)?
No, there is no plan for an LXI C class (web server).

FAQ 2014-04-07

Are the remote control commands of the handheld spectrum analyzers compatible with any other instrument?
The remote control command set of the handheld spectrum analyzers is compatible with the command sets of other spectrum analyzers.

FAQ 2012-03-02

How can I make field strength measurements on my handheld spectrum analyzer?
Each of the HSA products supports field strength measurements.

FAQ 2012-03-02

Do the handheld spectrum analyzers offer a tracking generator?
Yes, all HSA models have a tracking generator option.

FAQ 2012-03-01

What is the Task Planner Trial program?
A program offered by Keysight that allows customers to obtain a 90-day trial license.

FAQ 2012-02-22

Do the handheld spectrum analyzers have a keystroke recorder?
No, the HSAs do not have a keystroke recorder.

FAQ 2012-02-20

Is it possible to load built-in cellular frequency channels onto the handheld spectrum analyzer?
Yes, each HSA model allows the user to load standard frequency channels, like GSM or W-CDMA.

FAQ 2012-02-20

Do the handheld spectrum analyzers have AM/FM demodulation?
Yes

FAQ 2012-02-20

Does the user interface of the handheld spectrum analyzer support multiple languages?
Yes, the user interface for each of the HSA models supports eleven languages.

FAQ 2012-02-20

Do the handheld spectrum analyzers have record/playback features in the spectrogram and the spectrum mode? Can the signal be recorded on a USB drive?
Option SIM for the HSAs provides record and playback features in the spectrogram and the spectrum mode.

FAQ 2012-02-20

Is it possible to operate the power meter option (PWM) remotely using a SCPI command?
No, the power meter option on the HSAs cannot be controlled remotely.

FAQ 2012-02-20

How long will a handheld spectrum analyzer powered by battery continuously work?
A battery-powered HSA can continuously work for a minimum of 3 hours.

FAQ 2012-02-20

How do I enable the GPS information on the handheld spectrum analyzer?
The steps to enable GPS on the N9342C, N9343C or N9344C are: Press[Shift] -> [System Mode] -> {More 1 of 2} -> {GPS} -> {GPS on} and {GPS Info on}.

FAQ 2012-02-20

Can the handheld spectrum analyzers be turned on or off remotely?
There is no SCPI command to turn the HSA on or off remotely.

FAQ 2012-02-20