이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-25 / 145

정렬방식:
Firmware update error with "Cannot Open another Window"
I cannot update the firmware with the error message; "Cannot Open another Window"

FAQ 2016-08-04

B2900A 제어를 위해 사용 가능한 인터페이스에는 어떠한 종류가 있나요?
GPIB,LAN,USB

FAQ 2016-07-05

1채널 SMU B2900A에 2nd SMU 채널 추가가 가능한가요?
불가능 합니다.

FAQ 2016-07-05

B2901A/02A/11A/12A SMU에 N1294A-021/022 저잡음필터를 사용할 수 있습니까?
아니요...

FAQ 2015-10-28

B29000A 시리즈 SMU에 소스메모리 스윕 기능이 있나요?
아니요...

FAQ 2015-10-28

Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

How does the Microsoft end of support for Windows XP affect my B1500A and B1505A Device Analyzer?
As of April 8, 2014 Microsoft has ceased supporting the Windows XP operating system. This document will provide the information about the migration from Window XP to Windows 7.

FAQ 2014-04-30

Why are USB modular instruments (U2700 Series) and USB DAQ modules (U2300, U2500, U2600 Series) not detectable by the E5810B?
Establish the connection between the USB modular Instrument and the PC directly, and then disconnect the device from the PC (while it’s still powered-on), and connect to E5810B.

FAQ 2014-04-17

계측기 Host 정보 확인 방법
계측기 Host 정보 확인하는 방법

FAQ 2013-10-17

How to use the interlock to output more than ±42V?
B2900A has interlock detection with the digital I/O on the rear pannel. Click the link for details.

FAQ 2013-09-16

How can the B2900A Series of SMU source pulses whenever it receives an external trigger signal?
It can do it by configuring a digital I/O pin to be used for an external trigger signal. Click the above link for details.

FAQ 2013-09-16

What is the difference among data query commands such as ":FETCh?", ":MEASure?", ":READ?", :SENSe:DATA?"?
They have the function to query data similarly but there is some difference among them. Click the above link for details.

FAQ 2013-09-16

Can the B2900A Series of SMU sweep voltage source by the know on the front panel?
Yes, it's possible by enabiling Immediate V/I Update function. Click the above link for details.

FAQ 2013-09-16

What is the difference among Trigger Types on Single View?
Click the above link for details.

FAQ 2013-09-16

What is the equivalent command to "Output after Sweep" parameter on "Sweep" dialog?
It should be [:SOURce]:FUNCtion:TRIGgered:CONTinuous. Once you send it with the parameter "ON", the parameter is set to "END VALUE".

FAQ 2013-09-16

How can I set up Power-on State of the B2901/02/11/12A?
It is possible to store the desired instrument condition as Power-on State. Click the above link for details.

FAQ 2012-11-21

Can I use the triaxial cable with B2900A?
Yes. You can use the triaxial cable by using the N1294A adaptor.

FAQ 2012-11-20

프로그램 메모리에 얼마나 저장이 가능한가요?
B2900 series의 프로그램 메모리는 100Kbyte입니다.

FAQ 2012-10-31

B2901/02/11/12A용 Labview Plag&Play 장비 드라이버를 어디서 받을 수 있나요?
NI 홈페이지에서 받을 수 있습니다.

FAQ 2012-10-31

Keysight B2900A Quick I/V software가 Floating low terminal을 지원 하나요?
지원 하지 않습니다.

FAQ 2012-10-31

B2901/02/11/12A에서 6-Wire 저항측정이 가능한가요?
아니요. 안됩니다.

FAQ 2012-10-31

B2901/02/11/12A에 '찾기' 기능이 제공됩니까?
B2900 series에는 찾기 기능이 없습니다.

FAQ 2012-10-26

B2902A와 B2912A의 채널 2번이 SCPI 명령어를 인식하지 못합니다.
B2902A와 B2912A의 채널 2번이 SCPI 명령어를 인식하지 못하고 error를 발생합니다.

FAQ 2012-10-26

I cannot store the channel 2 measurement condition to USB memory stick, why not?
The instrument may be configured to use the conventional command set. Click the above link for details.

FAQ 2012-10-09

The password is required to access the instrument.
The password is required to access the instrument compliant with the LXI specification. Click the above link for details.

FAQ 2012-10-09

1 2 3 4 5 6 다음