Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

LTE-Advanced (LTE-A)

Support by Product Model Number:

Refine the List

remove all refinements

By Industry/Technology

By Type of Content

1-20 of 20

Sort:
Keysight Expands UXM Wireless Test Set LTE-A Capabilities with 4CC, 256 QAM, LTE-U, Cat 0 Support
Keysight announced verification of end-to-end IP data throughput for downlink rates of 587.5 Mbps with the E7515A UXM wireless test set. Using three component carriers (3CC) and 256 QAM in the downlink, Keysight achieved sustained bi-directional 3GPP UE category 11 data rates.

Press Materials 2015-05-21

Keysight Demonstrates LTE-Advanced Category 11 IP Data Throughput with UXM Wireless Test Set
Keysight announced verification of end-to-end IP data throughput for downlink rates of 587.5 Mbps with the E7515A UXM wireless test set. Using three component carriers (3CC) and 256 QAM in the downlink, Keysight achieved sustained bi-directional 3GPP UE category 11 data rates.

Press Materials 2015-05-06

Keysight to Demonstrate New UXM Wireless Test Set Features at Mobile World Congress
The E7515A UXM wireless test set is the industry’s leading UE test platform ready for 3CC/4CC, 256 QAM, UE categories 11-14. Visit us at Hall 2, Booth 212.

Press Materials 2015-02-12

Keysight Extends UXM Wireless Test Set LTE-A Carrier Aggregation Support with 3CC, TDD, Uplink
The E7515A UXM wireless test set adds features to address the rapidly evolving 3GPP LTE-Advanced carrier aggregation advancements.

Press Materials 2015-01-21

Keysight Demonstrates LTE-A 450 Mbps End-to-End IP Data Throughput with UXM
The E7515A UXM wireless test set provides verification of three component carrier (3CC) end-to-end IP data throughput.

Press Materials 2014-11-18

Keysight Technologies announces expanded TRX module and EXM wireless test set enhancements
Keysight Technologies Announces Expanded TRX Module and EXM Wireless Test Set Enhancements

Press Materials 2014-10-01

Keysight Expands Functional Test Capabilities, Delivers Greater RF Design Confidence
The E7515A UXM wireless test set includes support for LTE-A category 7 data throughput, expanded functional test capabilities, and in-depth RF performance verification using the X-Series measurement applications.

Press Materials 2014-09-18

Agilent's UXM Wireless Test Set Accelerates Marvell's LTE-Advanced Category 7 Chipset Development
Agilent and Marvell worked in concert to achieve sustained bidirectional 300 Mbps downlink/100 Mbps uplink data throughput using 3GPP release 10 downlink and uplink carrier aggregation.

Press Materials 2014-05-06

Agilent’s UXM Wireless Test Set Enables New Insights into LTE-Advanced Category 6 Chipsets, Devices
Introducing the E7515A UXM wireless test set, the most highly integrated signaling test set created for functional and RF design validation in the 4G era and beyond.

Press Materials 2014-02-13

E6640A EXM Wireless Test Set Ready for Volume Production of LTE-A, 802.11ac WLAN Devices
Agilent Technologies today announced the E6640A EXM wireless test set, which offers breakthrough manufacturing-test scalability in technology coverage, performance and capacity to test up to 32 cellular and wireless-connectivity devices in parallel.

Press Materials 2014-02-13

Agilent Technologies Introduces Industry's First LTE-Advanced 8x8 MIMO Signal-Generation and Analysi
Agilent Technologies Introduces Industry's First LTE-Advanced 8x8 MIMO Signal-Generation and Analysis Solutions

Press Materials 2013-01-03

Agilent Technologies Accelerates Early Wireless Design Verification with New Release of SystemVue
Agilent will demonstrate SystemVue 2012.06 along with a range of solutions for everything from circuit-level modeling through system verification for general RF, microwave, 4G communications, and aerospace/defense applications at DAC2012 (Booth 313), June 3-7, in San Francisco. SystemVue 2012.06 will also be demonstrated at IMS 2012/IEEE MTT-S (Booth 1015), June 19-21, in Montr al, Canada. A range of premier partner solutions will be available on Agilent Avenue and throughout the event area.

Press Materials 2012-06-05

Agilent Technologies Introduces 6-GHz Signal Generators with Industry-Best Performance
Today's aerospace/defense environment requires enhanced radar performance to detect weak signals at long distances. To provide the pure and precise signals needed to test these designs, the MXG uses an innovative triple-loop synthesizer to deliver phase noise performance of -146 dBc/Hz at 1 GHz and 20 kHz offset. For developers of radar components such as mixers and analog-to-digital converters, the MXG also features industry-leading spurious performance of -96 dBc at 1 GHz.

Press Materials 2012-05-01

Agilent Technologies Named Oscilloscope Company of the Year
The award is based on Frost & Sullivan's recent analysis of the oscilloscope market. Frost & Sullivan ranked Agilent as the No. 2 company in 2009, but its rapid revenue growth since then has made it the leader in market penetration.

Press Materials 2012-04-25

Agilent Technologies Introduces Wideband DPD Modeling Platform for LTE-Advanced, 802.11ac
Agilent Technologies Inc. (NYSE: A) today announced the newest release of its W1716 Digital Pre-Distortion Builder (DPD) software, designed to enable the high levels of wireless performance necessary for emerging wideband standards such as LTE-Advanced and IEEE 802.11ac.

Press Materials 2011-08-31

Agilent to Demonstrate Industry-First Solutions for 3G/4G and LTE-Advanced at Mobile World Congress
Agilent Technologies to Demonstrate Industry-First Design and Test Solutions for 3G/4G and LTE-Advanced at Mobile World Congress

Press Materials 2011-02-07

Agilent Technologies Introduces Industry's First LTE-Advanced Signal Generation, Analysis
Agilent Technologies Inc. (NYSE: A) today extended its leadership in LTE test with the introduction of dedicated LTE-Advanced signal generation and signal analysis solutions. Both solutions will be showcased at the upcoming Mobile World Congress in Barcelona, Feb. 14-17 (Hall 1, Stand A46).

Press Materials 2011-02-02

Agilent Technologies Introduces Industry’s First Design and Test Solution for 3GPP LTE-Advanced
Agilent announces the first commercially available 4G system design library for 3GPP Release 10 - the W1918 LTE-Advanced Library for SystemVue.

Press Materials 2011-01-05

Agilent Technologies Wins Informa LTE North America Award
Moray Rumney, the lead technologist specializing in LTE at Agilent, has won the Informa LTE North America 2010 award for individual contribution to LTE development.

Press Materials 2010-11-17

Agilent Technologies’ New LTE Applications Target 4G System-Level Designers

Press Materials 2010-02-16