Contact an Expert

Technical Support

Electronic Measurement

Find by Product Model Number: Examples: 34401A, E4440A

1-25 of 51

Sort:
Signal & Spectrum Analyzer Benchtop/Handheld Firmware Update Center
To access the most recent version of firmware or software for signal and spectrum analyzer - benchtop and handheld models.

FAQ 2015-04-08

Signal Analyzer IVI and MATLAB Instrument Drivers
Supported models: N9000A, N9010A, N9020A, N9030A, N9038A, E4406A, E4440A, E4443A, E4445A, E4446A, E4448A, N8201A, E4447A, E4401B, E4402B, E4403B, E4404B, E4405B, E4407B, E4408B, E4411B, E7401A, E7402A, E7403A, E7404A, E7405A, M9290A, N9040B

FAQ 2015-02-06

Where can I find manuals for discontinued and obsolete Hewlett-Packard, Agilent and Keysight test equipment?
Most Keysight products have PDF manuals that can be found on product pages. Other vendors also supply old manuals.

FAQ 2014-08-01

How can I get correct Log Frequency Scale Trace Data Using IntuiLink or BenchVue with my ESA Series Spectrum Analyzer?
Save the trace as a .csv file

FAQ 2014-03-13

What is included with Option UK6?
Beginning December 19, 2013, the list below describes what will be included with Option UK6:

FAQ 2014-02-27

What Printers can be used for my Network and Spectrum Analyzer products?
Printer Compatibility Information for your specific model of Network and/or Spectrum Analyzer can be found here.

FAQ 2014-01-31

What is the RF Test Blog?
RF engineers know that making good measurements is a challenge. The RF Test Blog was created as a resource for RF engineers to find ways to make better RF measurements.

FAQ 2013-12-17

What calibrations are available on X-Series, PSA, ESA analyzers and X-Series, ESG-C, PSG Signal Generators at time of initial sale from the factory?
Details regarding time of sale calibrations can be found here...

FAQ 2013-10-15

How do I use the Service Request method (SRQ) to determine if the X-Series, ESA and PSA Signal Analyzers measurement is complete or has an error me...
Click here for information on the Service Request query to determine when a measurement is complete.

FAQ 2013-06-25

How do I remotely program my spectrum or vector signal analyzer?
Instructions, examples, and references for remotely programming your spectrum analyzer

FAQ 2013-05-16

What is a Spectrum Analyzer?
"What is a spectrum analyzer?” You asked and we answered.

FAQ 2013-03-28

How do I upgrade my ESA-L Series Spectrum Analyzer?
Find information on Hardware Options, Measurement Personalities, Connectivity Methods, Firmware Upgrades, etc...

FAQ 2013-02-07

For my Spectrum Analyzer, where can I find a conversion guide between IVI-COM and SCPI?
The linked spreadsheet provides a mapping between IVI-COM and SCPI

FAQ 2012-05-26

What type of cabinets can the ESA Rackmount Kit (Option 1CP) be installed into?
The ESA Rackmount Kit (Option 1CP) was designed to mount into an System II Rack.

FAQ 2012-03-16

How do I transfer the screen image on my PSA, ESA, or EMC analyzer to a PC using Keysight VEE?
See content for complete details and an example program...

FAQ 2012-03-16

How do I erase/clear the user data in an ESA or EMC series spectrum analyzer for security reasons?
Follow this link for further information....

FAQ 2012-03-16

What is the fastest pulse risetime that I can measure with my spectrum analyzer in zero span?
The measurement risetime may not be faster that the best risetime of the spectrum analyzer

FAQ 2012-03-02

Why do spurious signals appear in my spectrum analyzer span when I apply a clean signal to the RF input?
Overdriving the input mixer of the analyzer may cause the spurs.

FAQ 2012-02-26

Why do performance verification tests 55, 56 and 57 in the ESA Calibration Guide say "This test has been deleted"?
These tests were put in the manual as placeholders...

FAQ 2012-02-25

What is the correct cable to use with the ESA Series for RS-232 communication?
Part number RS232-61601

FAQ 2012-02-25

How do I save my trace data in a comma-separated variable (.csv) file format on an ESA, PSA or EMC spectrum analyzer?
On the front panel of the analyzer, press [File]{Save} and select either the A: (floppy) or C: (internal) drive...

FAQ 2012-02-24

Why is there a "chirping" noise coming out of my ESA Series Spectrum Analyzer?
This is caused by the alignment routine and is normal.

FAQ 2012-01-24

Is a viewing hood available for the ESA Series Spectrum Analyzer?
No, the display which is used in the ESA has a large viewing angle and the contrast can be adjusted to compensate for direct sunlight.

FAQ 2012-01-11

How can I find accessories for a Keysight product?
For instrument-specific accessories (such as probes for an oscilloscope), first go to the product page and then see the related accessories. For general-purpose accessories (such as rf & microwave test accessories, carts, and racks), go to the ...

FAQ 2011-10-07

Can I convert my 1.5 GHz ESA Spectrum Analyzer input impedance from 50-ohm to 75-ohm or vice versa from 75-ohms to 50-ohms?
Keysight does not supply a specific upgrade kit to change the input impedance of the Spectrum Analyzer. It is not a simple connector change, rather an entire R.F. assembly, model ID label, and connector label.

FAQ 2010-10-01

1 2 3 Next