Contact an Expert

Technical Support

Spectrum Analyzers (Signal Analyzers)

Find by Product Model Number: Examples: 34401A, E4440A

1-25 of 174

Sort:
Signal Analyzer IVI and MATLAB Instrument Drivers
Supported models: N9000A, N9010A, N9020A, N9030A, N9038A, E4406A, E4440A, E4443A, E4445A, E4446A, E4448A, N8201A, E4447A, E4401B, E4402B, E4403B, E4404B, E4405B, E4407B, E4408B, E4411B, E7401A, E7402A, E7403A, E7404A, E7405A, M9290A, N9040B

FAQ 2015-01-17

What are the login and passwords that are used on the X-Series Signal Analyzers?
There are two different login accounts: User account and Administrator account

FAQ 2015-01-13

89600 VSA software and X-Series signal analyzer software compatibility matrix
Supported versions listed here

FAQ 2014-12-16

Signal & Spectrum Analyzer Benchtop/Handheld Firmware Update Center
To access the most recent version of firmware or software for signal and spectrum analyzer - benchtop and handheld models.

FAQ 2014-12-08

How do I upgrade my M9290A CXA-m PXIe Signal Analyzer?
Find Information on Hardware Options, Measurement Applications, etc....

FAQ 2014-11-17

How can I determine what CPU shipped with my PXA, MXA, or EXA?
CPU install details can be found here...

FAQ 2014-10-13

What N9030A PXA signal analyzer options will be included in the N9040B UXA signal analyzer?
See the list of included options in the base product

FAQ 2014-10-06

With the new N9040B, UXA signal analyzer user interface how can I record signals?
The 89600 VSA software may be used to record signals, but users may also do their own I/Q time captures using IQ Analyzer mode over the remote interface.

FAQ 2014-10-06

What are the dimensions and weight of the N9040B UXA signal analyzer?
Dimensions and weight information can be found here.

FAQ 2014-10-06

What is the bandwidth of the wideband I.F. output of the N9040B UXA signal analyzer?
Same as the N9030A PXA signal analyzer with Option CR3, wideband I.F. output.

FAQ 2014-10-06

What will the sweep rates of the N9040B UXA signal analyzer be?
Similar to the N9030A PXA signal analyzer with Option FS1.

FAQ 2014-10-06

What are the similarities and differences in the N9040B UXA Signal Analyzer when it comes to Real-Time Spectrum Analysis?
Specific items listed here...

FAQ 2014-10-06

Is the N9040B UXA signal analyzer SCPI compatible with other X-Series signal analyzers?
Yes, it is SCPI compatible

FAQ 2014-10-06

Which external mixers are compatible with the N9040B UXA signal analyzer?
The same external mixers as the other X-Series signal analyzers.

FAQ 2014-10-06

What is the size, resolution, and aspect ratio of the N9040B UXA signal analyzer's display?
Details can be found here.

FAQ 2014-10-06

What are the frequency range options on the N9040B UXA signal analyzer?
Initially Options 508 (8.4 GHz) , 513 (13.6 GHz) and 526 (26.5 GHz). More details found here.

FAQ 2014-10-06

What will be the maximum SA-mode RBW setting in the N9040B UXA signal analyzer?
The maximum RBW setting in SA-mode will be 8 MHz, the same as the other X-Series signal analyzers. When using the 89600 VSA software, it will still be possible to select wider RBW settings. Additionally, real-time spectrum analysis has >8 MHz depending on span.

FAQ 2014-10-06

How do I upgrade my N9040B UXA Signal Analyzer?
Find Information on Hardware Upgrades, Instrument Software and Measurement Applications, etc....

FAQ 2014-10-06

What interfaces does the N9040B UXA signal analyzer have?
Front and Rear Panel interfaces are listed.

FAQ 2014-10-06

Are there plans to have the Pulse Measurement software available for the N9040B UXA signal analyzer?
Yes, in the near future.

FAQ 2014-10-06

How do I upgrade my N9038A MXE EMI Receiver?
Find Information on Hardware Upgrades, Instrument Software and Measurement Applications, etc...

FAQ 2014-09-29

Does the M9290A CXA-m PXIe signal analyzer offer a tracking generator?
Currently, there is no tracking generator function for the M9020A.

FAQ 2014-09-11

How many slots does the M9290A CXA-m PXIe signal analyzer have?
There are four slots in the PXIe-based modular instruments.

FAQ 2014-09-11

Can I upgrade the frequency range of my M9290A CXA-m PXIe signal analyzer?
No, the frequency range of the M9290A is not upgradable.

FAQ 2014-09-11

Does M9290A CXA-m PXIe Signal Analyzer support sweep mode for spectrum analysis?
Yes, the M9290A supports both sweep and FFT mode for spectrum analysis.

FAQ 2014-09-11

1 2 3 4 5 6 7 Next