이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

상세 분류

상세분류 제거

주제별

분야별 검색결과

제품 카테고리별

1-13 / 13

정렬방식:
How does the Microsoft end of support for Windows XP affect my Keysight AFM or NanoIndenter?

FAQ 2014-05-13

How do I implement the correction of Pharr, Strader, and Oliver in an older test method?
In a recent special-focus issue of the Journal of Materials Research, Pharr, Strader, and Oliver demonstrated that in some circumstances, the oscillation amplitudes of the CSM option have non-negligible effects on the semi-static measurements of f...

FAQ 2009-10-11

What is the positional accuracy when moving between the XP and DCM heads? For example, say you need to make an indent with the XP and then scan wit...
The quoted accuracy for the XP stage (High Precision) is 1 micron within the field of view at a point that has been calibrated in Microscope to Indenter distance...

FAQ 2009-10-11

Why did beta change?
Historically, a “fudge-factor” beta has appeared in the equation that relates stiffness to reduced modulus...

FAQ 2009-10-11

When I change grips on the Nano UTM, must I re-determine the mass for dynamic analysis?
No...

FAQ 2009-10-11

What is the nominal area function for a cone?
Given a cone with a half-included angle of...

FAQ 2009-10-11

My frame stiffness changed from 8.5e+6 N/m to 6.5e+6N/m. Is this a problem?
Because the contact and the frame are springs in series, this is not as big of a change as it seems. Let us consider the effect of this change on fused silica when the applied force is 400mN...

FAQ 2009-10-11

What is the area function for a spherical tip? How do I enter this into TestWorks.
The spherical tip function is the lead term, a0 is 0. The 2nd term, a1 is 2R, where R is tip radius in nm. The remaining terms are 0...

FAQ 2009-10-11

How is displacement range affected when changing gain value?
NanoSuite Explorer gives the user the ability to change gain settings to fit specific testing needs. Each gain setting, 0-7, has a corresponding displacement range...

FAQ 2009-10-11

What is an appropriate flat punch diameter for my material?
The flat punch diameter used to test a material should generate a contact stiffness much greater then the stiffness of the springs in the indenter head. The standard stiffness of the springs in the XP indentation head is approximately 80N/m...

FAQ 2009-10-11

Can you please explain to me the Strain Rate Target input in determining the rate at which the indenter penetrates the surface? I am using the XP ...
The Strain Rate Target input is used so that the indenter loads at a rate that is equivalent to the user’s desired target strain rate for their material. This is an important parameter for time-dependent materials since their mechanical properties...

FAQ 2009-10-11

Unloading properties don’t calculate
The test seems to run fine, but none of the properties from the unload are calculated...

FAQ 2009-10-11

What is the noise floor for force and displacement?
The noise-floor values for displacement and force in our laboratory for the DCM head are <0.1nm and <10nN, respectively. For the XP head, these values are <1.0nm and <100nN. We do not quote values for noise floor, because they are not concrete val...

FAQ 2009-10-11