이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-25 / 31

정렬방식:
Keysight 5G Trial System Design and Validation Solution Demo
This video demonstrates Verizon’s early 5G trial system modeling connected to the latest 3GPP TR 38.900 mmWave channel model. These specifications facilitate early 5G trial system deployments and provide the wireless industry with the ability to test and validate key 5G technical components.

기본 데모 2016-12-19

Transform 5G Concepts into “This Changes Everything” Reality
Evolve existing technologies. Invent new ones. Go from 5G waveform concept to “this changes everything" reality – while saving time, money and silicon. It starts with Keysight’s testbed for 5G waveform generation and analysis.

기본 데모 2016-10-19

Unlocking Millimeter Wave Insights
It is easy to underestimate the challenges at millimeter-wave frequencies, and this amplifies the importance of integrated tools for design, simulation, measurement, and analysis. Learn more about how Keysight is taking the mystique out of millimeter waves and unlocking new insights.

기본 데모 2016-09-30

유튜브의 SystemVue 동영상
유튜브 키사이트 EEsof EDA 채널의 SystemVue 동영상 라이브러리 재생 목록

기본 데모 2016-09-16

Introducing SystemVue 2016
See a live demo of SystemVue 2016. The new capabilities enable researchers and system architects working on platforms using beamforming algorithms for 5G, satellite, NewSpace, radar and EW applications, to reduce interference and power consumption, while increasing physical range.

기본 데모 2016-06-27

IMS-MTT 2016 from Keysight EEsof EDA
Highlights from Keysight EEsof EDA on the show floor at IMS-MTT 2016 in San Francisco, CA on May 22-26, 2016.

기본 데모 2016-06-05

IMS 2015 Demos from Keysight EEsof EDA
YouTube video playlist containing International Microwave Symposium (IMS) 2015 demo videos from Keysight EEsof EDA MicroApps.

기본 데모 2015-06-19

Microwave Journal - Keysight 5G Design and Verification
Microwave Journal video: 5G Applications Development Engineer Greg Jue demonstrates one of Keysight's latest innovations.

기본 데모 2015-06-02

Microwave Journal - Keysight Interview with Todd Cutler
Microwave Journal Editor Pat Hindle interviews Todd Cutler, General Manager of Keysight EEsof EDA.

기본 데모 2015-05-31

How to Understand 5G: Waveforms
This video will provide you with good guidance for understanding what kinds of new waveforms are being researched for the next generation standard. The example with end-to-end link level simulation will demonstrate waveform quality issues of a multi-carrier system and the nonlinearity from the RF chain.

사용방법 동영상 2015-05-01

Discovering SystemVue - MATLAB Script Modeling
Keysight SystemVue now includes MATLAB Script, an equation and modeling engine from MathWorks. This product tutorial shows communications system designers how to create and debug MATLAB models from inside the SystemVue user interface.

기본 데모 2015-04-15

5G Channel Sounding
This video discusses Keysight's This video discusses Keysight's mmWave MIMO channel sounding solution for 5G. 5G is aiming to achieve gigabytes per second data rate anywhere, anytime, and to get there, we need to use new technologies such as massive MIMO and millimeter wave broadband. solution for 5G. 5G is aiming to achieve gigabytes per second data rate anywhere, anytime, and to get there, we need to use new technologies such as massive MIMO and millimeter wave broadband.

기본 데모 2015-03-19

Keysight 5G signal generation and analysis demonstration at Mobile World Congress
Keysight demonstrates candidate 5G FBMC waveform co-existence with 4G LTE, and up to 2GHz wideband FBMC signal generation and analysis using SystemVue W1906 5G library, N7608B Signal Studio for custom modulation, and 89600 VSA software applications with Keysight wideband test equipment.

기본 데모 2015-03-09

Keysight 5G Millimeter-Wave Channel Sounding demonstration at Mobile World Congress
Keysight demonstrates a multi-channel Channel Sounding system at milimeter-wave frequencies, to enable 5G research and system validation

기본 데모 2015-03-09

Keysight EEsof EDA Electronic System Level Design Flow with SystemVue
In this video we show the Electronic System Level, or ESL, design flow from Keysight based on SystemVue -- the fastest way to design and validate challenging physical layer communications systems, where baseband and RF must work together.

기본 데모 2014-12-12

Design Challenges in DDR4 - The Keysight DDR Bus Simulator
This video is about design challenges in DDR4 and in particular the DDR Bus Simulator, which is a new Keysight EEsof EDA simulation tool for DDR4 and beyond.

기본 데모 2014-10-16

Introducing Wireless Verification Test Benches in ADS 2014 at IMS 2014
ADS verification test benches, or VTBs, provide easy-to-use Wireless Standards for RF Verification. Now in ADS 2014 you have the flexibility to create custom VTBs or customize a current VTB product with SystemVue.

기본 데모 2014-08-01

Flexible RF Stimulus Response Validation of Emerging Communications Standards
IMS 2014 - Commercially available flexible simulation tools and flexible instruments can be readily used to create appropriate waveforms by specifying the top level parameters in the time or frequency domains. These can be used to test the emerging and existing RF/MW components and infrastructure and derive the required enhancements to the standards and infrastructure performance.

기본 데모 2014-08-01

Breaking the RF Carrier Barrier: 0-200 in Under a Second
Simulating nonlinear responses to hundreds of RF carriers is now practical with an innovative simulation technique.

기본 데모 2014-08-01

Simulation of Airborne, Space Borne and Ship Based Radar Systems with Complex Environment
The presentation reviews several simulation techniques for accurately evaluating radar system performance and may reduce system deployment risks and costs. Handling moving Tx/Rx platforms for Airborne, Space-Borne and Ship based radars is key in determining system performance. It is important to include radar environmental scenarios for interference, clutter, jamming/deception, and radar cross section (RCS). These simulation techniques can be used to analyze advanced radar systems such as phased array, Multiple-Input Multiple-Output (MIMO), active/passive, and multi-static radar systems. Application examples will be demonstrated.

기본 데모 2014-08-01

Simulation of Phased Array Radar Systems
This video presents a new method of simulating large‐scale, phased‐array networks.

기본 데모 2013-07-24

Creating and Analyzing Multi Emitter Environment Test Signals with COTS Equipment
This presentation shows how wide‐bandwidth, multi‐channel digitizers can be used to capture and analyze signals.

기본 데모 2013-07-24

Virtual Development and Flight Testing of Radar and EW Systems
Learn how SystemVue and Radar Model Library, when combined with STK from Analytical Graphics, Inc (AGI), can be used to create realistic, "RF-aware" Radar/EW signals in algorithm simulations.

기본 데모 2013-07-09

Realistic Ultra-Wideband Radar Signal Generation Using Keysight SystemVue
To lower test costs SystemVue can be used with Keysight test equipment to model realistic environment and jamming scenarios, which often involve costly outdoor ranges, chambers, and real-time hardware simulators. Watch the YouTube video to see how.

기본 데모 2012-08-23

Explore YouTube Videos - Keysight Tube (Cellular)
A collection of Keysight Cellular video demonstrations and tutorials.

기본 데모 2012-05-28

1 2 다음