이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-25 / 324

정렬방식:
BenchVue 2017 소프트웨어란 무엇입니까?
BenchVue 2017 소프트웨어에 대한 추가 정보.

FAQ 2017-04-25

How do I contact Keysight EEsof EDA Sales Support for help?
Use the form provided in this FAQ to submit your contact information.

FAQ 2017-04-24

Where can I find system requirements and supported platform information for GoldenGate?
For GoldenGate system requirements and supported platform information, refer to the Prerequisites section for your platform at http://www.keysight.comfind/eesof-goldengate-latest-downloads

FAQ 2017-04-06

GoldenGate의 최신 릴리즈 및 기타 정보 소개
GoldenGate용 제품별 릴리즈 정보 등록

FAQ 2017-04-06

Where can I find product documentation for MBP and MQA?
Product documentation for Model Builder Program (MBP) and/or Model Quality Assurance (MQA) can be found in the Knowledge Center.

FAQ 2017-04-03

Where can I get current and previous software versions as well as updates of MBP and/or MQA?
Current and previous software versions of Model Builder Program (MBP) and/or Model Quality Assurance (MQA) can be found in the Knowledge Center.

FAQ 2017-04-03

How do I renew an expired MBP or MQA license?
General information on renewing an expired Model Builder Program (MBP) or Model Quality Assurance (MQA) license.

FAQ 2017-04-03

IO Libraries Suite: What is the latest version of the IO Libraries Suite?
IO Libraries Suite 2017, available online.

FAQ 2017-03-22

Keysight Software Licenses
Keysight software node-locked/fixed, transportable, floating/network/enterprise licenses provide flexibility. Whether you have a short term need or require software for years, for a single user or multiple users, Keysight licenses put you in charge.

FAQ 2017-03-09

Can I use Command Expert with non-Keysight instruments?
Yes, you can use Command Expert with any SCPI instrument that follows the SCPI-99 standard, or has an IVI-COM, IVI-C, or IVI.NET driver

FAQ 2017-03-08

Why does the FPGA Configuration Window appear upon boot up?
Information on why the FPGA Configuration Window appears...

FAQ 2017-02-02

CalPod system을 N1500A 소프트웨어와 함께 사용 할 수 있습니까?
아니요. CalPod와 N1500A 소프트웨어는 호환되지 않습니다.

FAQ 2017-01-24

Keysight EEsof EDA Distinguished Authors
Keysight EEsof EDA Distinguished Author program.

FAQ 2017-01-20

Why has Keysight changed the N9069C licensing structure model?
The N9069C licensing structure model has been collapsed as a customer ordering convenience. Click on the question for additional information.

FAQ 2016-12-07

What are the new Wave 2 features for Mobile WiMAX™ 802.16 system profiles?
Read about IO-MIMO and IO-BF (beamforming) profiles...

FAQ 2016-12-02

How do I create a Mono FM Signal using N5182B MXG ARB?
You can configure N7611B Signal Studio Broadcast Radio to play a mono/FM signal.

FAQ 2016-10-21

How do I use myKeysight Keysight Software Manager
Depending on what you want to do, the myKeysight/KSM can help you perform actions such as redeeming an order, resetting your password, viewing, renewing, upgrading or re-hosting a license.

FAQ 2016-10-12

How many carriers can the MXG support in Carrier Aggregation mode?
One MXG can support one instance of the Carrier Aggregation mode. One instance of the Carrier Aggregation mode supports 5 component carriers.

FAQ 2016-10-11

When using OFDM mode in N7610B Signal Studio for Short Range Communications, is User File data supplied by an external file started with MSB or LSB?
The first bit in the file is used first. So this can be thought of as the MSB is used first.

FAQ 2016-10-11

For my UXA Signal Analyzer, what applications support option H1G (1 GHz Analysis Bandwidth) and what additional functionality does it provide?
Option H1G also includes the B2X digitizer. Therefore, option H1G is supported by all applications that support B2X up to at least 255 MHz bandwidth. Option H1G additionally provides 1 GHz analysis bandwidth for some other measurement applications.

FAQ 2016-10-07

Why is Option DP2 or B40 recommended on the spectrum analyzer (EXA, MXA, PXA) with the EMI Measurement Application(N6141A)?
Time Domain Scan (TDS), Monitor Spectrum, and Amplitude Probability Distribution (APD) all require 2 GB of Capture memory (option DP2). Option B40 includes DP2, so having either option B40 or DP2 will work equally as well for N6141A.

FAQ 2016-10-07

Explore the Newest Release of HeatWave and More
List of product-specific release information for HeatWave.

FAQ 2016-09-23

SystemVue의 최신 릴리즈 및 기타 정보 탐색
SystemVue용 제품별 릴리즈 정보 목록

FAQ 2016-09-16

How do I get started with ADS?
Watch this short video and you will learn how to navigate through the ADS environment to create a new workspace, build a new schematic, and run a simulation. To watch the video, go to http://www.keysight.com/find/starting-ads

FAQ 2016-09-11

ADS의 최신 릴리즈 및 기타 정보 소개
ADS용 제품별 릴리즈 정보 목록

FAQ 2016-09-09

1 2 3 4 5 6 7 8 9 10 ... 다음