1-15 of 15

Sort:
How to Simplify Device Model Extraction using an Open Source User Interface
This video shows an example of an IC-CAP custom user interface (UI) for device modeling. In the selected modeling application, the DC modeling of a Zener diode is intentionally kept simple in order to demonstrate the features of the UI.

How-To Video 2017-06-26

Static Random Access Memory (SRAM) Cell Modeling in MBP 2017
This video introduces a new turnkey solution for SRAM modeling now available in Keysight’s Model Builder Program 2017. The video describes the concept of SRAM cell modeling and highlights the major challenges of that process.

Demo 2017-06-12

How to Extract a BSIM4 DC Model
This video introduces a general DC modeling and characterization flow for the BSIM4 model, which is one of the most popular models used by the industry today for bulk CMOS.

How-To Video 2017-05-24

The High-Frequency, High Speed Design Revolution: Why Your Design & Test Flow Will Soon Be Obsolete
In this keynote from EDI CON USA 2016, Todd Cutler, vice president and general manager of Keysight Design & Test Software, discusses these trends and explains how, when coupled with market pressures, they are driving a revolution in the design and measurement industry.

Demo 2016-10-11

Unlocking Millimeter Wave Insights
It is easy to underestimate the challenges at millimeter-wave frequencies, and this amplifies the importance of integrated tools for design, simulation, measurement, and analysis. Learn more about how Keysight is taking the mystique out of millimeter waves and unlocking new insights.

Demo 2016-09-30

Advanced Low-Frequency Noise Analyzer Overview
This video will provide a brief overview of Keysight E4727A Advanced Low-Frequency Noise Analyzer (ALFNA), the next-generation system for measurement of 1/f noise and random telegraph noise. It will describe ALFNA’s innovative modular design and its technical advantages. It will also touch on wide-range applications and how they are enabled by ALFNA’s industry-leading technical specifications and rich feature set.

Product Tour 2016-08-29

Low Frequency Noise Analyzer Technical Demo
A more technical dive on the new Advanced Low-Frequency Noise Analyzer with WaferPro Express, which offers the unique ability to measure and model device noise across wafers. This release features a new user interface and tight integration with Keysight's WaferPro Express software, a platform that performs automated wafer-level measurements of semiconductor devices.

Demo 2016-07-20

Introducing the 2016 Advanced Low-Frequency Noise Analyzer
The new Advanced Low-Frequency Noise Analyzer Offers Unique Ability to Measure and Model Device Noise Across Wafers. This release features a new user interface and tight integration with Keysight's WaferPro Express software, a platform that performs automated wafer-level measurements of semiconductor devices.

Demo 2016-07-18

How to Accurately Measure and Validate S-Parameters for Transistor Modeling
This video explains and demonstrates a method to develop accurate Spice models based on verified S-parameter measurements. The video walks you through the entire modeling flow for two RF spiral inductors using IC-CAP.

How-To Video 2016-04-04

How to Model RF Passive Devices: Spiral Inductors
This video explains and demonstrates a method to develop accurate Spice models based on verified S-parameter measurements. The video walks you through the entire modeling flow for two RF spiral inductors using IC-CAP.

How-To Video 2016-02-11

How to Model RF Passive Devices: Capacitors and Resistors
This video explains and demonstrates a method to develop accurate Spice models from verified S-parameter measurements. The video walks you through the entire modeling flow for an on-wafer capacitor using IC-CAP.

How-To Video 2015-10-27

How to Model a BJT Bipolar Junction Transistor
This video covers the basics of bipolar junction transistor (BJT) modeling and illustrates an easy step-by-step procedure to extract the model parameters of the popular Gummel-Poon (GP) model. While the GP model was introduced in the early 1970’s, it still enjoys a wide popularity in electronic device modeling and many modeling engineers consider it a classic and an excellent starting point for getting familiar with modeling in general.

How-To Video 2015-08-28

Keysight WaferPro Express
The Keysight WaferPro Express software performs automated wafer-level measurements of semiconductor devices such as transistors and circuit components. It provides turnkey drivers and test routines for a variety of instruments and wafer probers. Its user interface makes it easy to setup and run complex wafer-level test plans, while powerful customization capabilities are enabled by the new Python programming environment.

Product Tour 2015-03-24

How to Make Accurate, Automated RF Wafer-level Measurements
The video introduces automation as a way to increase productivity and efficiency. Keysight WaferPro Express measurement software is used to illustrate the various steps in combination with Cascade Microtech Velox software for prober control and Cascade WinCalXE software for automated calibration.

How-To Video 2015-01-27

How to Extract SRAM Models
This video shows how to extract SRAM device models efficiently on Keysight's device modeling platform.

How-To Video 2015-01-14