Here’s the page we think you wanted. See search results instead:

 

Sprechen Sie mit einem Experten

Technischer Support

Electronic Measurement

Support by Product Model Number:

26-40 of 40

Sort:
Can I measure temperature with the U1241B/U1242B Handheld Digital Multimeter?
Yes, you can measure temperature with the U1241B/U1242B Handheld Digital Multimeter using a thermocouple adaptor and thermocouple tip….

FAQ 2010-02-21

Can I use a normal USB cable for datalogging with the U1250B Series Handheld Digital Multimeters?
No, you cannot use a normal USB cable for datalogging with the U1250B Series Handheld Digital Multimeters…..

FAQ 2010-02-21

How long can the batteries of the U1241B or U1242B Handheld Digital Multimeter last?
The batteries that are supplied with the U1241B or U1242B Handheld Digital Multimeter can last for more than 200 hours under normal use.

FAQ 2010-02-21

Can I set a measurement interval on the U1251B, U1252B and U1253B Handheld Digital Multimeters?
Yes, you can set a measurement interval on the U1251B, U1252B and U1253B Handheld Digital Multimeters….

FAQ 2010-02-21

Can I perform measurement with my U1252B/U1253B Handheld Multimeter while charging the unit?
No, U1252B/U1253B Handheld Multimeter does not allow to perform measurement while charging…

FAQ 2010-02-21

Can I save measurements with the U1241B or U1242B Handheld Digital Multimeter?
You can save measurements with the U1242B Handheld Digital Multimeter but not with the U1241B….

FAQ 2010-02-21

What is the length of the thermocouple cable for the U1186A Thermocouple (K-type) and Temperature Adapter?
The length of the K-type thermocouple bead is approximately 1m....

FAQ 2010-02-21

Why is the battery life of the U1253B Handheld Digital Multimeter (DMM) typically shorter than the battery life of the U1251B/U1252B?
The battery life of the U1253B Handheld Digital Multimeter (DMM) is typically shorter because its display brightness is set to the highest….

FAQ 2010-02-21

What is the relationship between the “No. of Least Significant Digit” and the accuracy of a handheld meter?
The “No. of Least Significant Digit” affects the accuracy of a handheld meter....

FAQ 2010-02-21

Can I use regular AAA batteries in the U1241B and U1242B Handheld Digital Multimeters?
Yes, you may use regular AAA batteries for the U1241B and U1242B Handheld Digital Multimeters….

FAQ 2010-02-21

What is the relationship between the “No. of Least Significant Digit” and the accuracy of a handheld multimeter?
The “No. of Least Significant Digit” affects the accuracy of a handheld multimeter....

FAQ 2010-01-07

What should I consider when charging my U1252A/ U1253A Handheld Digital Multimeter with the DC power adaptor?
Please ensure the following precautions is observed during the charging process ...

FAQ 2009-10-01

What is the recommended battery type for the U1251A, U1252A and U1253A Handheld Digital Multimeters (DMM)?
The recommended battery type for the U1251A, U1252A and U1253A Handheld Digital Multimeters (DMM) are described on the table below……

FAQ 2009-06-10

What is the length of the thermocouple cable for the U1186A Thermocouple (K-type) and Temperature Adapter?
The length of the K-type thermocouple bead is approximately 1m....

FAQ 2009-01-12

Why is the battery life of the U1253A Handheld Digital Multimeter (DMM) typically shorter than the battery life of the U1251A/U1252A?
The battery life of the U1253A Handheld Digital Multimeter (DMM) is typically shorter because its display brightness is set to the highest….

FAQ 2008-10-09

Previous 1 2