이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-25 / 48

정렬방식:
Integrating Multiple Technology Devices onto Laminate-Based Multi-Chip-Modules
Microwave Product Digest (MPD) featured article on "Integrating Multiple Technology Devices onto Laminate-Based Multi-Chip-Modules Using an Integrated Design Flow", written by Keefe Bohanan, Applications Engineer District Manager for Keysight EEsof EDA.

기사 2016-11-29

PDF PDF 3.90 MB
Direct-Synthesis Software Approach Facilitates Filter Design
This Microwaves & RF article discusses how Genesys software can be used to design filters with the direct-synthesis technique. A lowpass filter example is presented to illustrate the software’s capabilities.

기사 2016-11-28

Using DSP and RF circuit co-design to reduce risk and cost
For modern design organizations, it’s now more imperative than ever that they simulate both Digital Signal Processor (DSP) and RF circuits together at the system level using mixed signals.

기사 2016-10-11

Software plus signal generators and analyzers support IEEE 802.11p design and test
Jungik Suh, marketing program manager, Automotive & Energy Solutions, Keysight Technologies, provides input on several Keysight solutions for the connected-car arena for Evaluation Engineering's October print special report on automotive test.

기사 2016-10-05

Phased array beamforming software design, test, and measurement kit introduced by Keysight
Military & Aerospace Electronics article introduces the W1720EP phased array radar beamforming kit add-on software simulation personality for the SystemVue 2016.08 design and test and measurement environment.

기사 2016-06-13

Solving Mobile Radar Measurement Challenges
This Microwave Journal article examines an alternative simulation method that allows for better cross-domain modeling in a single framework, to capture the complete effects of modern radar system performance.

기사 2016-06-13

Keysight EEsof EDA makes it easy to get back to school—at least virtually
Rick Nelson, executive editor of Evaluation Engineering, visited Keysight Technologies and had this to say about Keysight EEsof EDA.

기사 2015-09-11

Determining the Best RF Simulation Tools as an RF Consulting Engineer
Independent consulting in RF and microwave engineering is a growing trend and many engineers are delivering their highly sought after RF expertise back to the industry.

기사 2015-06-08

PDF PDF 2.64 MB
Digital Predistortion Linearizes Wireless Power Amplifiers
This Article by Wan-Jong Kim, Shawn P. Stapleton, Jong Heon Kim, and Cory Edelman focuses on how digital predistortion linearizes wireless power amplifiers.

기사 2014-07-31

PDF PDF 1.81 MB
Using S-Parameter Data Effectively
This Article by Wilfredo Rivas-Torres focuses on how to incorporate Sparameters in the design process using a CAD approach.

기사 2014-07-31

PDF PDF 248 KB
Designing RFID Tags Using Direct Antenna Matching
This Article by Cory Edelman and Murthy Upmaka describes the design challenges involved in RFID design and also focuses on the use of integrated EDA tools to optimally address the challenges.

기사 2014-07-31

PDF PDF 1.09 MB
New LDMOS Model Delivers Powerful Transistor Library - Part 1
This Article presents a new CMC LDMOS model that can accurately predicts both small-signal and nonlinear performance, and is scalable for devices of different sizes and power output capabilities.

기사 2014-07-31

PDF PDF 544 KB
Design and Characterization of Discontinuous RF/Microwave Passive Components
This Article by Dean Nicholson presents a design methodology proposed for designing and building RF circuits likely to contain discontinuous regions.

기사 2014-07-31

PDF PDF 1.43 MB
Symmetric and Asymmetric - Coupled Lines Band-Stop Filters at Ku/Ka Bands
This Article presents theory and design of coupled-line spur line band-stop filters, which are quite compact structures, lower radiation loss than conventional shunt stub and coupled-line filters.

기사 2014-07-31

PDF PDF 1.38 MB
New LDMOS Model Delivers Powerful Transistor Library - Part 2
This article reprint presents that the CMC (LDMOS FET) model can be scaled for a larger device, with a good fit for signal, power and distortion performance as illustrated by a 60W Doherty PA design example.

기사 2014-07-31

PDF PDF 699 KB
RF SiP Design Verification Flow with Quadruple LO Down Converter SiP
This article reprint by HeeSoo Lee and Dean Nicholson outlines the design flow used for a System-in-Package component, using multiple die integrated into a single packaged device.

기사 2014-07-31

PDF PDF 505 KB
Accurate Simulation Models Yield High-Efficiency Power Amplifier Design
This Article by Sonoko Akamatsu, Charles Baylis, and Larry Dunleavy details the design goals and simulation- based processes for Power Amplifier Design.

기사 2014-07-31

PDF PDF 592 KB
System-Level Modelers Race The Design Cycle
Microwaves & RF article by Jean-Jacques DeLisle describes how effective system-level modeling and analysis is becoming more critical in virtually every RF system.

기사 2014-04-02

Overcoming the Challenges of Designing and Testing Phased-Array Radar Systems
Microwave Product Digest (MPD) featured article for January 2014 written by Dingqing Lu of Agilent Technologies.

기사 2014-01-27

Using Channel Coding to Verify and Increase the Performance of Channel-Coding Algorithms
An advanced simulation methodology and environment can now be used to verify and measure the efficiency of algorithms under real-world communication scenarios, saving engineers both significant time and cost.

기사 2013-12-09

A New Approach for Multi-Emitter Test Signal Generation
A new capture and playback approach generates multi-emitter test signals using a combination of COTS test equipment and simulation software.

기사 2013-11-14

Beyond CMOS Vs. GaAs: Picking The Right Technology
Design software can help evaluate the many different technology options for a high-frequency electronic circuit or system under a wide range of operating conditions.

기사 2013-10-24

Efficient Synthetic Aperture Radar Antenna Array Design Using Multiple Electromagnetic Solvers
Example of a synthetic aperture radar antenna array shows how applying the most efficient EM technology to each segment of the antenna system significantly improves design efficiency compared to traditional approaches.

기사 2013-10-11

Addressing the Challenges of Radar and EW System Design and Test using a Model-Based Platform
Article reprint, High Frequency Electronics, October 2013. Due to the challenges of Electronic Warfare (EW) environments, today’s designers require a solution for designing, verifying and testing their Radar and EW systems in an effective way.

기사 2013-10-10

PDF PDF 1.45 MB
Realization and Analysis of Electronically Steerable Phased Array using Scripting & Parameterization
With the advent of multi-core, high speed processors and abundant memory availability, complex designs using 3-D full-wave electromagnetic (EM) tools have become common choice for microwave and antenna engineers.

기사 2013-07-09

1 2 다음