这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-22 / 22

排序:
Early Design Review or Boundary Scan in Enhancing Testability and Optimazation of Test Strategy
With complexities of PCB design scaling and manufacturing processes adopting to environmentally friendly practices raise challenges in ensuring structural quality of PCBs.

文章 2017-05-08

PDF PDF 624 KB
Expanding IEEE Std 1149.1 Boundary-Scan Architecture Beyond Manufacturing Test of PCBA
This paper will discuss the expanded use of boundary-scan testing beyond the typical manufacturing test to capture structural defects on a components/devices in a Printed Circuit Board Assembly (PCBA)

文章 2017-04-01

PDF PDF 860 KB
Stay ALERT – Don’t Get Hurt

文章 2016-03-03

Testing a Network Communication PCBA from Prototype to Manufacturing - Article Reprint
Early implementation of BST can cut test costs and time.

文章 2016-02-17

PDF PDF 178 KB
The Boundary Scan Toolbox - Article Reprint
Find out how boundary scan can enable embedded and other value-added test in your toolbox.

文章 2016-02-16

PDF PDF 409 KB
New IEEE Standards for Board and System Tests - Article Reprint
This article highlights of changes to IEEE Std 1149.1, IEEE Std 1149.6, IEEE P1149.10 and IEEE P1838.

文章 2016-02-16

PDF PDF 190 KB
I'm a Board Test Engineer and I'm Loving It! - Article Reprint
Life on the road can be relentless, but it’s never boring. Find out why from this personal story of a test engineer.

文章 2016-02-12

PDF PDF 178 KB
Emulating Analog Input Sensors in Automotive Electronics Functional Test - Article Reprint
This article discusses guidelines for evaluating the digital-analog converters for your automotive electronics functional test needs.

文章 2016-02-09

PDF PDF 318 KB
Manufacturing Test Solutions for SSDS - Article Reprint
A new system performs both ICT and boundary scan in high-volume settings.

文章 2016-02-09

PDF PDF 222 KB
Testing the Internet of Things - Article Reprint
Connectivity is embedded in the electronics ecosystem. And test should be embedded in the devices that support it.

文章 2016-02-09

PDF PDF 79 KB
Tester for Hire - Article Reprint
This article explores the possibility of renting test equipment to help electronics manufacturers juggle capacity according to production demand and available resources.

文章 2016-02-09

PDF PDF 381 KB
Finding Fault - Article Reprint
testing mission-critical functions in automotive electronics.

文章 2016-02-05

PDF PDF 452 KB
Testing of Small Form-Factor Products - Article Reprint
Boundary scan and embedded test will need to make up for ICT gaps.

文章 2016-02-03

PDF PDF 546 KB
Making Boundary Scan Easy - Article Reprint
Testing boundary scan devices no longer need be a laborious task.

文章 2016-02-03

PDF PDF 217 KB
Testing New Grounds in Automotive Electronics - Article Reprint
Manufacturers are increasingly designing products for ease of test.

文章 2016-02-02

PDF PDF 279 KB
Automating In-Circuit Test - Article Reprint
Inline ICT is not as cumbersome as it used to be, and in the longer run, will help manufacturers save costs.

文章 2016-02-02

PDF PDF 87 KB
LXI Instrumentation applied to bioanalytical electrical characterization

文章 2014-04-07

ECN article: Remote Wireless Test With LXI
Article reprinted with approval from ECN magazine.

文章 2014-04-07

University of Hawaii using Keysight Equipment for Patient Monitoring Research

文章 2013-05-27

Artificial Retina Research at the University of Utah Provides Hope for the Blind

文章 2013-05-27

Electromagnetic Interference Meets Its Match
NVIDIA Summer 2010 article on how gaming-inspired 3D glasses and a GPU-accelerated simulation using Agilent's EMPro impact products we use every day.

期刊 2010-06-24

Positron Emission Tomography Imaging Using Agilent Acqiris U1067A High-Speed PCI

文章 2008-05-15

PDF PDF 73 KB