Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discutez avec un expert

Support technique

Mesure Electronique

Support by Product Model Number:

1-22 sur 22

Tri:
Expanding IEEE Std 1149.1 Boundary-Scan Architecture Beyond Manufacturing Test of PCBA
This paper will discuss the expanded use of boundary-scan testing beyond the typical manufacturing test to capture structural defects on a components/devices in a Printed Circuit Board Assembly (PCBA)

Article 2017-04-01

PDF PDF 860 KB
Early Design Review or Boundary Scan in Enhancing Testability and Optimazation of Test Strategy
With complexities of PCB design scaling and manufacturing processes adopting to environmentally friendly practices raise challenges in ensuring structural quality of PCBs.

Article 2017-04-01

PDF PDF 417 KB
Stay ALERT – Don’t Get Hurt

Article 2016-03-03

Testing a Network Communication PCBA from Prototype to Manufacturing - Article Reprint
Early implementation of BST can cut test costs and time.

Article 2016-02-17

PDF PDF 178 KB
New IEEE Standards for Board and System Tests - Article Reprint
This article highlights of changes to IEEE Std 1149.1, IEEE Std 1149.6, IEEE P1149.10 and IEEE P1838.

Article 2016-02-16

PDF PDF 190 KB
The Boundary Scan Toolbox - Article Reprint
Find out how boundary scan can enable embedded and other value-added test in your toolbox.

Article 2016-02-16

PDF PDF 409 KB
I'm a Board Test Engineer and I'm Loving It! - Article Reprint
Life on the road can be relentless, but it’s never boring. Find out why from this personal story of a test engineer.

Article 2016-02-12

PDF PDF 178 KB
Manufacturing Test Solutions for SSDS - Article Reprint
A new system performs both ICT and boundary scan in high-volume settings.

Article 2016-02-09

PDF PDF 222 KB
Tester for Hire - Article Reprint
This article explores the possibility of renting test equipment to help electronics manufacturers juggle capacity according to production demand and available resources.

Article 2016-02-09

PDF PDF 381 KB
Emulating Analog Input Sensors in Automotive Electronics Functional Test - Article Reprint
This article discusses guidelines for evaluating the digital-analog converters for your automotive electronics functional test needs.

Article 2016-02-09

PDF PDF 318 KB
Testing the Internet of Things - Article Reprint
Connectivity is embedded in the electronics ecosystem. And test should be embedded in the devices that support it.

Article 2016-02-09

PDF PDF 79 KB
Finding Fault - Article Reprint
testing mission-critical functions in automotive electronics.

Article 2016-02-05

PDF PDF 452 KB
Testing of Small Form-Factor Products - Article Reprint
Boundary scan and embedded test will need to make up for ICT gaps.

Article 2016-02-03

PDF PDF 546 KB
Making Boundary Scan Easy - Article Reprint
Testing boundary scan devices no longer need be a laborious task.

Article 2016-02-03

PDF PDF 217 KB
Testing New Grounds in Automotive Electronics - Article Reprint
Manufacturers are increasingly designing products for ease of test.

Article 2016-02-02

PDF PDF 279 KB
Automating In-Circuit Test - Article Reprint
Inline ICT is not as cumbersome as it used to be, and in the longer run, will help manufacturers save costs.

Article 2016-02-02

PDF PDF 87 KB
LXI Instrumentation applied to bioanalytical electrical characterization

Article 2014-04-07

ECN article: Remote Wireless Test With LXI
Article reprinted with approval from ECN magazine.

Article 2014-04-07

University of Hawaii using Keysight Equipment for Patient Monitoring Research

Article 2013-05-27

Artificial Retina Research at the University of Utah Provides Hope for the Blind

Article 2013-05-27

Electromagnetic Interference Meets Its Match
NVIDIA Summer 2010 article on how gaming-inspired 3D glasses and a GPU-accelerated simulation using Agilent's EMPro impact products we use every day.

Journal 2010-06-24

Positron Emission Tomography Imaging Using Agilent Acqiris U1067A High-Speed PCI

Article 2008-05-15

PDF PDF 73 KB