您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

1-25 / 35

排序:
Industry Primary Impedance Measurement System (iPIMMS) – What is it?
In 2005 Keysight Technologies' facility at South Queensferry in the United Kingdom was the first calibration laboratory to be granted ISO/IEC 17025 accreditation for an internet-enabled technology to make measurements of complex reflection and transmission coefficient parameters.

FAQ 2015-03-16

Keysight Accreditation Milestones: Australia and Great Britain
Keysight’s Melbourne service center was first accredited by NATA in August 1974; the Winnersh service center was accredited by the BCS in August 1984.

FAQ 2014-02-14

How can the memory in a 438A Power Meter be erased for security purposes?
This can be done by a sequence of keypresses, or by a sequence of remote commands.

FAQ 2013-11-22

How can the E4416A/E4417A/E4418A (EPM441A)/E4418B/E4419A (EPM442A)/E4419B memory be erased for security purposes?
There is a power-on keypress combination that can be used to erase the power meter's memory.

FAQ 2013-10-10

何謂 ISO 17025?為何如此重要?
是德提供符合 ISO 17025 標準的服務。取得更多資訊並瞭解電子測試設備如何滿足 ISO 17025 的要求。

FAQ 2013-07-10

「最佳量測能力」一詞改為「校驗與量測能力」
經過國際協商,校驗實驗室用來描述在量測中所能達到之準確度的慣用語已在 2010 年進行變更。

FAQ 2013-03-14

向量網路分析儀量測不確定性計算軟體
無論是經驗豐富的使用者或是初學者,面對向量自動網路分析儀,都可能會問:它可提供多準確的量測?」

FAQ 2013-03-14

Uncertainty Calculators. What is the Accuracy of My Measurements?
Whether you are a novice or experienced user of Keysight test equipment, you may sometimes need more details to answer the question “How accurate are these measurements?” Learn more important details and download the following uncertainty calculators.

FAQ 2013-02-28

Acceptability of Foreign Calibration Certificates
Keysight offers an ISO/IEC 17025 accredited calibration service for many products. The calibration certificate bears the logo of the national accreditation organization.

FAQ 2013-01-16

Accreditation Details for the United Kingdom
Answers to your questions

FAQ 2013-01-13

Accreditation Details for Germany
Answers to questions about calibration cerificiation

FAQ 2013-01-13

Can I Use a USB External Storage Devices?
Yes. It is recommended to use FAT32 formatted drive.

FAQ 2012-08-17

How do you clear the M9045A, M9045B, M9047A and M9048A memory?
Please refer to the link below for the procedure on how to clear the memory for the M9045B and M9048A adapters.

FAQ 2012-05-01

為了安全起見,該如何清除ENA記憶體中的資料?

FAQ 2012-04-18

How do I erase/clear the user data in an ESA or EMC series spectrum analyzer for security reasons?
Follow this link for further information....

FAQ 2012-03-16

How do I recover my PSA Spectrum Analyzer after a secure erase memory sanitization?
A secure erase memory sanitization clears all of the user writable instrument memory. Firmware and measurement personalities must be reinstalled.

FAQ 2012-02-26

是德手持式頻譜分析儀是否有清除記憶體資料的安全功能?
是的,配備選項 SEC 之是德手持式頻譜分析儀提供清除記憶體資料的保護功能。

FAQ 2012-02-20

How can I securely erase the non-volatile memory?
Click on the question for more information

FAQ 2012-02-17

How do I erase or sanitize the memory on my MXG?
When moving the signal generator from a secure development environment, there are several security functions you can use to remove classified proprietary information from the instrument.

FAQ 2010-09-08

I need information on Keysight Instrument Security and memory sanitization.
Use the Keysight Instrument Security page to look up the security and memory sanitization procedures for your instrument. Use this link view security information by model number or product type.

FAQ 2008-11-20

How do I erase 33220A memory?
The 33220A contains memory locations that retain user values and settings. This document describes the method for clearing the memory to default values, or to an empty condition.

FAQ 2008-02-11

How do I sanitize / erase / clear the memory on a 34401A digital multimeter for security reasons?
Information on memory types and clearing procedures.

FAQ 2007-10-17

How do I erase or sanitize the memory on my PSG signal generator?
Please refer to the following document, ESG/PSG Security Features.

FAQ 2005-12-05

How do I sanitize / erase / clear the memory on a 53150A CW Microwave Frequency Counter for security reasons?
Information on memory types and clearing procedures.

FAQ 2005-11-11

How do I sanitize / erase / clear the memory on a 34970A data acquisition mainframe for security reasons?
Information on memory types and clearing procedures.

FAQ 2005-11-11

1 2 下一頁