Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 35

Sort:
Industry Primary Impedance Measurement System (iPIMMS) – What is it?
In 2005 Keysight Technologies' facility at South Queensferry in the United Kingdom was the first calibration laboratory to be granted ISO/IEC 17025 accreditation for an internet-enabled technology to make measurements of complex reflection and transmission coefficient parameters.

FAQ 2015-03-16

Keysight Accreditation Milestones: Australia and Great Britain
Keysight’s Melbourne service center was first accredited by NATA in August 1974; the Winnersh service center was accredited by the BCS in August 1984.

FAQ 2014-02-14

How can the memory in a 438A Power Meter be erased for security purposes?
This can be done by a sequence of keypresses, or by a sequence of remote commands.

FAQ 2013-11-22

How can the E4416A/E4417A/E4418A (EPM441A)/E4418B/E4419A (EPM442A)/E4419B memory be erased for security purposes?
There is a power-on keypress combination that can be used to erase the power meter's memory.

FAQ 2013-10-10

ISO 17025 and Accreditation
Keysight provides ISO 17025 compliant services. Get more information and learn how to meet ISO 17025 requirements for electronic test equipment.

FAQ 2013-07-10

Best Measurement Capability (BMC) Ousted in Favor of Calibration & Measurement Capability (CMC)
By international agreement, the phrase traditionally used by calibration labs to describe the accuracy which they can achieve in their measurements was replaced during 2010.

FAQ 2013-03-14

Uncertainty Calculators. What is the Accuracy of My Measurements?
Whether you are a novice or experienced user of Keysight test equipment, you may sometimes need more details to answer the question “How accurate are these measurements?” Learn more important details and download the following uncertainty calculators.

FAQ 2013-02-28

Acceptability of Foreign Calibration Certificates
Keysight offers an ISO/IEC 17025 accredited calibration service for many products. The calibration certificate bears the logo of the national accreditation organization.

FAQ 2013-01-16

Accreditation Details for Germany
Answers to questions about calibration cerificiation

FAQ 2013-01-13

Accreditation Details for the United Kingdom
Answers to your questions

FAQ 2013-01-13

Vector Network Analyzer Uncertainty Calculator, What is the Accuracy of My Measurements?
No matter whether you are an experienced or novice user of vector automatic network analyzers, you may have asked "How accurate are these measurements?"

FAQ 2013-01-13

Can I Use a USB External Storage Devices?
Yes. It is recommended to use FAT32 formatted drive.

FAQ 2012-08-17

How do you clear the M9045A, M9045B, M9047A and M9048A memory?
Please refer to the link below for the procedure on how to clear the memory for the M9045B and M9048A adapters.

FAQ 2012-05-01

How can the memory in the ENA be erased for security purposes?

FAQ 2012-04-17

How do I erase/clear the user data in an ESA or EMC series spectrum analyzer for security reasons?
Follow this link for further information....

FAQ 2012-03-16

Do the handheld spectrum analyzers have a memory clearing (security) feature?
Yes, the HSAs offer an optional security feature for memory sanitization, Option SEC.

FAQ 2012-03-02

How do I recover my PSA Spectrum Analyzer after a secure erase memory sanitization?
A secure erase memory sanitization clears all of the user writable instrument memory. Firmware and measurement personalities must be reinstalled.

FAQ 2012-02-26

How can I securely erase the non-volatile memory?
Click on the question for more information

FAQ 2012-02-17

How do I erase or sanitize the memory on my MXG?
When moving the signal generator from a secure development environment, there are several security functions you can use to remove classified proprietary information from the instrument.

FAQ 2010-09-08

I need information on Keysight Instrument Security and memory sanitization.
Use the Keysight Instrument Security page to look up the security and memory sanitization procedures for your instrument. Use this link view security information by model number or product type.

FAQ 2008-11-20

How do I erase 33220A memory?
The 33220A contains memory locations that retain user values and settings. This document describes the method for clearing the memory to default values, or to an empty condition.

FAQ 2008-02-11

How do I sanitize / erase / clear the memory on a 34401A digital multimeter for security reasons?
Information on memory types and clearing procedures.

FAQ 2007-10-17

How do I erase or sanitize the memory on my PSG signal generator?
Please refer to the following document, ESG/PSG Security Features.

FAQ 2005-12-05

How do I sanitize / erase / clear the memory on a 53151A CW microwave frequency counter for security reasons?
Information on memory types and clearing procedures.

FAQ 2005-11-11

How do I sanitize / erase / clear the memory on a 34970A data acquisition mainframe for security reasons?
Information on memory types and clearing procedures.

FAQ 2005-11-11

1 2 Next