Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 45

Sort:
“Shotgunning”, a Bad Fit for Lead-Free Test
Shotgunning, a common repair technique in functional test, will be negatively affected by lead-free processes. This article explores the technique and draws broad conclusions regarding the impact of lead-free on electronics manufacturing test

Application Note 2015-07-14

PDF PDF 99 KB
Enhanced Log Records for the Keysight Medalist In-Circuit Test System
Track changes made to your i3070 test programs to improve success.

Application Note 2009-03-04

PDF PDF 801 KB
Medalist i3070 Test Throughput Optimization
This application note explores some factors which cause test time to increase on the Medalist i3070 In-Circuit Test system, and methods which users can employ to reduce the test time and increase throughput on the Medalist i3070 ICT system.

Application Note 2008-11-24

IEEE 1149.6 Standard Boundary Scan Testing on Keysight Medalist i3070 ICT Systems
This paper introduces the latest advancements in Boundary Scan test capabilities on the Keysight Medalist i3070 In-Circuit Test platform that supports the testing of IEEE 1149.6-compliant devices.

Application Note 2008-11-24

PDF PDF 297 KB
First pass Yield (FPY) and Alarm Triggers on the Keysight Medalist i3070 In-circuit Test System
This application note will explain some customizations and how to create alarm triggers.

Application Note 2008-09-26

PDF PDF 131 KB
Procedure to backup ITF3.1.1 Database and DataStore and Restore Them in a New ITF Server with SQL200
This document is targeted at users who are archiving historical data or migrating to a more powerful server utilized to run Keysight’s ITF.

Application Note 2008-07-28

PDF PDF 512 KB
Troubleshooting Medalist Intelligent Test Framework Port Problems
This document serves as a guide/reference to do preliminary analysis and troubleshooting when network/communication problems occur with the ITF server of the tester agent.

Application Note 2008-05-22

PDF PDF 813 KB
Using the Auto Optimizer on the Keysight Medalist In-Circuit Test Systems
Learn how to optimize throughput by using the auto optimizer tool.

Application Note 2008-05-03

PDF PDF 237 KB
Using the Graphical Pin Locator on Keysight Medalist In-Circuit Test Systems
Enhancing productivity is the end result when the graphical version of "find pins" is utilized. This tool is called pin locator and is part of the Operator GUI Browser in version 7.0.

Application Note 2008-05-03

PDF PDF 203 KB
The Future of In-Circuit Testing in the High-speed, Complex Electronics Environment
As board complexity and node counts continue to rise and high speed differential signaling continues to grow in popularity, In-Circuit Test needs to move quickly beyond the traditional realms. This article explores this in detail.

Application Note 2007-10-31

Making the Most of Keysight Throughput Multiplier on Medalist In-Circuit Test Systems
Keysight Throughput Multiplier reduces test time on in-circuit test systems by testing up to four boards of a single-board-type panel simultaneously. The tips in this application note will help users make the most of this valuable tool.

Application Note 2007-10-12

Medalist 3070 and Medalist i5000 System Recovery using Retrospect Express
This app note describes how to perform backups of the system hard disk for the Keysight Medalist 3070 and Keysight Medalist i5000 In-circuit Test systems that have been shipped with Retrospect Express 7.0 and Roxio Digital Media Plus 7.2 software.

Application Note 2007-07-10

PDF PDF 628 KB
Maximising Test Coverage with Keysight Medalist VTEP v2.0
This paper describes how to get the most from Keysight Technologies’ industry-leading vectorless test innovation, the Medalist VTEP v2.0 which is a suite of solution comprising VTEP, iVTEP and NPM.

Application Note 2007-04-17

Applying a New In-Circuit Probing Technique for High-Speed/High Density Printed Circuit Boards
Bead probes were used to obtain additional test access on a high-density production printed circuit board. This case study includes practical information and key bead-specific learnings discovered during the process of outsourcing.

Application Note 2006-10-24

In-circuit Testing of Low Voltage Devices
Core technical document summarizing issues regarding the testing of low voltage devices on the 3070 and i5000, including updated Safeguard information.

Application Note 2005-05-25

PDF PDF 172 KB
Test and Inspection as Part of the Lead-free Manufacturing Process
The paper addresses issues that will impact defect levels and defect spectrum during the transition to lead-free manufacturing. It also addresses different test and inspection systems’ readiness to test lead-free printed circuit board assemblies.

Application Note 2005-02-22

PDF PDF 421 KB
The Importance of Test and Inspection When Implementing Lead-Free Manufacturing
Many papers, articles, and studies have been written about process issues, reliability issues, repair issues, and the merits of different alloys. This paper addresses the impacts on test and inspection when going lead-free.

Application Note 2004-08-20

PDF PDF 260 KB
Using Lead-Free PCB Finishes at Manufacturing In-circuit Test Stage
The purpose of this document is to share experiences and educate engineers regarding different PCB surface finishes and the specific changes required in the PCB build process to allow for ICT.

Application Note 2004-08-08

PDF PDF 102 KB
Test Coverage: What Does It Mean when a Board Test Passes?
Originally presented at the 2002 International Test Conference -- Characterizing board test coverage as a percentage of devices or nodes having tests does not accurately portray coverage, especially in a limited access testing environment.

Application Note 2003-07-28

PDF PDF 266 KB
Testing Transformers on Unpowered Systems
This paper explains how to test basic analog parts, using unpowered systems.

Application Note 2003-03-21

PDF PDF 10 KB
Using Boundary Scan to Link Design and Manufacturing Test
By leveraging boundary-scan tests generated in Design and re-using them at Manufacturing Test, manufacturers can produce long-term benefits in terms of lower costs, greater efficiencies and higher quality products.

Application Note 2003-03-01

PDF PDF 502 KB
Boundary Scan Helps EMS Companies Cut Test Costs and Increase Revenues
Electronics Manufacturing Services (EMS) providers can utilize boundary-scan to reduce test cost expenses and also generate additional revenue opportunities.

Application Note 2003-03-01

PDF PDF 242 KB
What to Consider When Selecting the Optimal Test Strategy
This paper addresses several issues for selecting the optimal inspection strategy, presenting data from many studies that Keysight has performed in the quest to find the optimal test / inspection strategy.

Application Note 2003-03-01

PDF PDF 175 KB
New Features in Version 5.0 Software for 3070
Typically, when Keysight's Manufacturing Test Division introduces a new software revision for its flagship 3070 In-Circuit Tester, it only communicates with customers about the major new features.

Application Note 2003-01-28

PDF PDF 84 KB
System Issues in Boundary-Scan Board Test
While Boundary-Scan is a powerful test tool, test engineers are finding out that yesterday's DFT rules and test approaches may actually be detrimental to successfully testing systems on a board.

Application Note 2003-01-28

PDF PDF 37 KB

1 2 Next